Thursday, July 9, 2015

Python for LXI Instrument Control



Summary

LXI instruments often provide an interface to their parsers via telnet and/or sockets.  These connections do not require a VISA library as the communication layer.  On systems that don’t support VISA or users who just prefer to not use the VISA library, sockets is a good choice for connecting to and controlling instruments.  Python is a programming language that is easy to learn and is supported across many different operating systems.  Python is especially popular on UNIX-like OS’s like Linux and HP-UX.  This article will give a quick introduction on how to use Python for controlling your LXI instrument.

LXI Instruments

First let’s take a look at the LXI instrument.  There are two ports registered for SCPI services with the Internet Assigned Numbers Authority (IANA) for SCPI LAN services.   Those ports are 5024 for scpi-telnet and port 5025 for scpi-raw.   These are optional services that LXI instrument can implement.  The LXI Specification 1.4 has these services as a recommendation (See section 10.4.3.12).  Not all venders used the IANA reserved ports for these services, so you will need to review your specific instruments documentation to determine if these services are available and what port numbers to use.

What are these services?  Telnet is a simple protocol for connecting to a remote computer via a shell like a command prompt.  The default port for Telnet is 23 and typically does not need to be specified when starting a Telnet session.  The scpi-telnet port is 5024.  Scpi-telnet is a connection between a computer and a remote LXI instrument using a SCPI parser.   Scpi-telnet is useful for systems that don’t have any I/O Libraries installed, but have a LAN connection to their instrument.

Figure 1

Figure 1 is an example scpi-telnet session by using a command prompt.  The command used to start this session is ‘telnet 192.168.0.97 5024’.  Once there is an instrument prompt SCPI can be entered and responses display in the command window.

Scpi-raw is a connection between a computer and a LXI instrument using raw sockets.  This connection does not have the addition of the MEPE protocol that HiSlip or VXI-11 have.  If you desire or need MEPE you can use the PyVISA contribution for a Python application.

Python and Instruments

There is a PyVISA Python package and this enables the user to control instruments with any I/O that the instrument supports and is appropriate to use if you need to control an instrument over USB, VXI-11, HiSlip, or GPIB.  This package does require an installation of VISA exist on the controller to be able to open a session.  There is not a great deal of value in using the PyVISA package if using Sockets as your transport layer, plus you lose the  portability of moving to a system that does not have VISA.
Python has a low-level networking module that provides access to the BSD socket interface.   This article is not a tutorial assumes that the reader is familiar with sockets.  Here is a link to the Python documentation for socket programming.  Below is the code for starting the client side connects to an instrument:

def SocketConnect():
    try:
        #create an AF_INET, STREAM socket (TCP)
        s = socket.socket(socket.AF_INET, socket.SOCK_STREAM)
        #NODELAY turns off Nagle to improves chatty performance
        s.setsockopt(socket.IPPROTO_TCP, socket.TCP_NODELAY, 0)
        s.setsockopt(socket.SOL_SOCKET, socket.SO_LINGER, 0)
    except socket.error:
        print ('Failed to create socket.')
        sys.exit();
    try:
        #Connect to remote server
        s.connect((remote_ip, port))
        #print ('Socket Connected to ip ' + remote_ip)
    except socket.error:
        print ('failed to connect to ip ' + remote_ip)
    return s

The open is has two parts.  The first part is creating the socket.  After creating the socket I have set two options.  The first option is turning off NODELAY.  This turns off the Nagle algorithm which attempts to accumulate multiple send messages in a single packet.  This means with the Nagle ON a send will be scheduled to be sent a few milliseconds after the request waiting for other send requests that could be sent together saving some bandwidth.  Instrument SCPI tends to be chatty with lots of short strings waiting for responses, so with this ON it will increase the send latency adding time to the overall configuration of an instrument.  The second options is turning off LINGER.  When socket connections close they wait around for several minutes to process any stray packets that my still be in the system.  With LINGER off, it turns this wait time to 0 and so when the connection is closed it doesn’t wait around.  This really is not a good practice but I have seen many systems where they do a lot of open/closes which will result in the system eventually running out of resources and hanging on an open.  It’s better to re-architecture the system to reuse open sessions.
The second part connects to the remote instrument server.  This requires the IP Address or the hostname and the port number of the instrument service (default 5025).  Once the connection to the instrument service is successfully completed, we are ready to use the socket.
I have written a short script that open a socket, sends a query, and closes the socket.  It does this loop for 100 times.   Below is the core of this script:

def SocketQuery(Sock, cmd):
    try :
        #Send cmd string
        Sock.sendall(cmd)
    except socket.error:
        #Send failed
        print ('Send failed')
        sys.exit()
    reply = Sock.recv(4096)
    return reply

def SocketClose(Sock):
    Sock.close()
    #Sleep paces the rate of open/close.  Warning: This time worked for
    #the instrument I was using, mileage may vary.
    time.sleep(.300)
   
# Body
for i in range(100):
    s = SocketConnect()
    qStr = SocketQuery(s, b':DIAG:SYST:MEM?\n')
    SocketClose(s)
    print (str(count) + ":: " + str(qStr))
    count = count + 1

I wrote a function to return the response from a query.  It’s nice to have a set of functions like this so that your main control loop is a straight forward as possible.  I also wrote a close function.  This allows me to do any actions that might be needed to disconnect from the instrument service. 

Conclusion

Python is an interpreted programming language that lets you work quickly and is very portable.   LXI provides the transport and specifications for LXI instruments. Python scripts can be written for sockets to do a variety of test and measurements tasks.


---Full Source of Test Script ---
#!/usr/bin/env python
import socket   # for sockets
import sys  # for exit
import time # for sleep
import getopt

remote_ip = "156.140.113.41"
port = 5025
count = 0

def SocketConnect():
    try:
        #create an AF_INET, STREAM socket (TCP)
        s = socket.socket(socket.AF_INET, socket.SOCK_STREAM)
        #NODELAY turns of Nagle improves chatty performance
        s.setsockopt(socket.IPPROTO_TCP, socket.TCP_NODELAY, 0)
        s.setsockopt(socket.SOL_SOCKET, socket.SO_LINGER, 0)
    except socket.error:
        print ('Failed to create socket.')
        sys.exit();
    try:
        #Connect to remote server
        s.connect((remote_ip , port))
        #print ('Socket Connected to ip ' + remote_ip)
    except socket.error:
        print ('failed to connect to ip ' + remote_ip)
    return s

def SocketQuery(Sock, cmd):
    try :
        #Send cmd string
        Sock.sendall(cmd)
    except socket.error:
        #Send failed
        print ('Send failed')
        sys.exit()
    reply = Sock.recv(4096)
    return reply

def SocketClose(Sock):
    Sock.close()
    #Sleep paces the rate of open/close.  Warning: This time worked for 
    #the instrument I was using, milage may vary.
    time.sleep(.300)

def Usage():
    print('mySocket -a <ipaddress> -p <portnumber default=5025>')
    sys.exit();

def main(argv):
    global remote_ip
    global port
    global count
    try:
        opts, args = getopt.getopt(argv, "ha:p:",["address=","port="])
    except getopt.GetopError:
        Usage()
    for opt, arg in opts:
        if opt == '-h':
            Usage()
        elif opt in ("-a", "--addr"):
            remote_ip = arg
        elif opt in ("-p", "--port"):
            port = arg
    # Body
    for i in range(100):
        s = SocketConnect()
        qStr = SocketQuery(s, b':DIAG:SYST:MEM?\n')
        SocketClose(s)
        print (str(count) + ":: " + str(qStr))
        count = count + 1
main(sys.argv[1:])

192 comments:

  1. For anyone that is interested I do have an example of a script that works with telnet. It's a little trickier because you have to read off the welcome message and the prompt. It would have to be modified for each individual instruments welcome message and prompt, but it could be useful in the case of an instrument that implemented scpi-telnet but not scpi-sockets.

    ReplyDelete
  2. The python programming help is really helpful to us. I am sure that It can also helpful to the students. Very amazing post.

    ReplyDelete

  3. للحصول علي خدمة نظافة جيدة تاكد انك تتعامل مع شركة تنظيف بالرياض لديها باع طويل في مجال النظافة العامة فتعاملك مع شركة متميزة فانك ستحصل علي اد اء متميزة فشركات النظافة عديدة فمثلا عندما تبحث عن شركة تنظيف فلل بالرياض ستلاقيي شركة ركن البيت التي تمتلك امكانيات جيدة في اداء الخدمات المنزلية الجيدة بادوات حديثة ومواد مستوردة تقوم باستعمالها فمعك ايضا شركة تنظيف خزانات بالرياض اتي تقوم باداء جيدة لتسليمك خزان تمتلك به مياه نظيفة خالية من الرواسب والبكتريا كما سنمدك باعمال شركة تنظيف مسابح بالرياض التي تعطيك كل الامكانيات في امتلاك مسبح نظيف يحافظ علي اسرتك واطفالك بدون وجود اي اوساخ به ونقدم لكم الخدمة الخاصة بالمنازل والبيوت الصغيرة من خلال البحث عن شركة تنظيف منازل بالرياض التي تستطيع ان تحل لك كل مشاكل التنظيف المنزلي المتعبة التي تعاني منها واليكم خدمة القضاء علي الحشرات بواسطة مبيدات عالية الجودة تقوم بالقضاء علي جميع الحشرات الصغيرة والكبيرة بواسطة شركة رش مبيدات بالرياض التي تقضي علي جميع الحشرات

    ReplyDelete
  4. This article gives a definite clarification of can someone write my paper the LXI gauges utilized for attachments and telnet and a clarification of a case of a python script that controls an instrument.

    ReplyDelete
  5. Python or Jython both are best programming languages to learn.concept of java in Python making it really helpful for Automation . Want help in Jython assignment help or in Python homework https://codingzap.com/

    ReplyDelete
  6. I really like you post good blog,Thanks for your sharing.

    แตกใน xxx

    ReplyDelete
  7. This is very interesting, You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Regards - www.office.com/setup
    www.office.com/setup

    ReplyDelete
  8. Needed to compose you a very little word to thank you yet again regarding the nice suggestions you’ve contributed here.
    Python Training in Bangalore

    ReplyDelete
  9. I have read many other articles about the same topic, but your article convinced me! I hope you continue to have high quality articles like this to share with veryone!
    happy wheels

    ReplyDelete
  10. I am convinced that your website is convinced that weblog is very new. Probably I am going to bookmark your site. There are certainly impressive stories. Passion for sharing your website with us.
    Regards - www.office.com/setup
    www.office.com/setup
    www.office.com/setup

    ReplyDelete
  11. Some genuinely superb posts on this site, thanks for contribution.
    Regards - www.office.com/setup
    www.norton.com/setup

    ReplyDelete
  12. Some genuinely superb posts on this site, thanks for contribution.
    Regards - www.office.com/setup
    www.norton.com/setup

    ReplyDelete
  13. The blog has been extremely useful to keep I can share the your ideas in the future as this is really what I was looking for. I have subscribed to your blog. Are you looking for MIS research paper topics to write a quality research paper? Then link with us and we will serve you according to you specifications.

    ReplyDelete
  14. For the longest time, one of the things that I have been looking for is a way to always benefit from this kind of information. I have found a nice post, a page I can say is very interesting. Kindly keep on sharing. When you feel that you want to buy the most beautiful tempered glass wall cabinets, we are the best choice of sellers. If you need the most beautiful interior decoration items, we are the shop to visit.

    ReplyDelete
  15. Office Setup (post-acquisition installation)
    By purchasing one of these packages, you acquire a product key that can be used by one or more computers, depending on the item.

    • When downloading, discover the product key in your Amazon account to do office setup.

    • When purchased as a box, there is a PVC card with the product key inside the box
    .www.office.com/setup

    ReplyDelete
  16. Office Setup (post-acquisition installation)
    By purchasing one of these packages, you acquire a product key that can be used by one or more computers, depending on the item.

    • When downloading, discover the product key in your Amazon account to do office setup.

    • When purchased as a box, there is a PVC card with the product key inside the box
    .www.office.com/setup

    ReplyDelete
  17. I have a better understanding of the LXI, which makes my work quick and easy to use
    run 3

    ReplyDelete
  18. Thanks for sharing https://funnyguru.co/

    ReplyDelete
  19. I feel it interesting, your post gave me a new perspective! I have read many other articles about the same topic, but your article convinced me!
    devast io

    ReplyDelete
  20. http://gpete.blogs.keysight.com/2015/07/python-for-lxi-instrument-control.html?showComment=1534558891759#c6259786743041692171

    ReplyDelete
  21. http://yeswecandigital.blogspot.com/2018/01/yeswecandigital-australian-government.html

    http://www.hoobly.com/Yq4wH/yeswecan-digital-australian-govt-web-accessibility-development.htm
    https://worldradio.ch/classifieds/community/yeswecandigital-public-sector-web-development/
    https://profiles.wordpress.org/yeswecandigital/
    https://www.flickr.com/people/164614442@N02/
    https://www.pinterest.com.au/yeswecandigital/
    https://www.last.fm/user/Yeswecandigital
    https://www.quora.com/profile/Yeswecan-Digital

    ReplyDelete
  22. I feel it is interesting, I hope you continue to have good posts like this to share.
    wings io

    ReplyDelete
  23. Install Office Setup – Sign-in to you microsoft account and then Enter 25 digit alphanumeric office setup product key on country and language.click on next to start office installation.We are the best Office Setup in US, Canada and Australia. At Office Setup, we put high effort, moderate IT answers for organization's, and people.Whether set up or beginning, equipment or programming, system or electronic, we have something for each financial plan. officeplus.net is the exchanging name of Spacesolutions Pvt Ltd situated in California, USA. We are not Microsoft. However we are trained professionals to provide technical support for We are the world's biggest innovation wholesaler and a main innovation deals, showcasing and logistics organization for the IT business around the world. Our people group based ethos, focused costs and nature of administration settles on Office Setup the right decision for your IT needs .Whether you are a learner or experienced in IT our courses are altered to furnish you with the key achievement criteria to thrive in future attempts.
    www.office.com/setup

    ReplyDelete
  24. Excellent post!!!. The strategy you have posted on this technology helped me to get into the next level and had lot of information in it.
    SCCM Self Placed Videos

    Office 365 Self Placed Videos

    Exchange Server Self Placed Videos

    Sap Security Self Placed Videos

    ReplyDelete
  25. Hello fellow sufferer or companion,

    My name is Christian and I teach as a teacher in Hamburg at a district school. One of my great passions is to increase the topic of health.

    But that's not so easy, considering everything that comes together for me. For one thing, I have a very stressful job that costs me a lot of energy. Because of a diaphragmatic fracture and a lack of stomach acid, I tend to heartburn very easily.

    ReplyDelete
  26. Thank you much for this tutorial; this is an informative and valuable blog. Visit for
    Offshore Anonymous Hosting

    ReplyDelete
  27. I simply want to tell you that I am just beginner to blogs and absolutely enjoyed you’re website. More than likely I’m planning to bookmark your blog . You really come with awesome stories.

    DevOps Training
    RPA Training in Chennai
    Angular 6 Training in Chennai
    Dot Net Training in Chennai

    ReplyDelete
  28. Antika Eşya Alanlar Alım satım alanında 20 yıllık tecrübesi bulunan firmamız Hurda Gümüş , Plak Alanlar Firmasıdır.

    ReplyDelete
  29. This comment has been removed by the author.

    ReplyDelete
  30. This comment has been removed by the author.

    ReplyDelete
  31. [url=http://pacsuppliesusa.com/]Inventory app [/url]
    [url=http://pacsuppliesusa.com/]Rugged Tablet[/url]
    [url=http://pacsuppliesusa.com/]Weigand[/url]
    [url=https://pacsuppliesusa.com/rugged-tablets-phones-pda?pages=1-1#p1013]Rugged Tablet[/url]
    [url=https://pacsuppliesusa.com/handheld-computers-pda?pages=1-1#p1775
    ]Handheld Computer[/url]

    ReplyDelete
  32. Positive site, where did u come up with the information on this posting?I have read a few of the articles on your website now, and I really like your style. Thanks a million and please keep up the effective work. machine learning training in chennai

    artificial intelligence and machine learning course in chennai

    machine learning training in velachery

    ReplyDelete
  33. Such a Great Article!! I learned something new from your blog. Amazing stuff. I would like to follow your blog frequently. Keep Rocking!!
    Blue Prism training in chennai | Best Blue Prism Training Institute in Chennai

    ReplyDelete
  34. Thanks for your post. This is excellent information. The list of your blogs is very helpful for those who want to learn, It is amazing!!! You have been helping many application.
    best selenium training in chennai |

    ReplyDelete
  35. Thank you for sharing your article. Great efforts put it to find the list of articles which is very useful to know, Definitely will share the same to other forums.

    best openstack training in chennai | openstack course fees in chennai | openstack certification in chennai | openstack training in chennai velachery

    ReplyDelete
  36. Thank you so much for your information,its very useful and helful to me.Keep updating and sharing. Thank you.
    RPA training in chennai | UiPath training in chennai


    ReplyDelete
  37. Good job in presenting the correct content with the clear explanation. The content looks real with valid information. Good Work

    DevOps is currently a popular model currently organizations all over the world moving towards to it. Your post gave a clear idea about knowing the DevOps model and its importance.

    Good to learn about DevOps at this time.


    devops training in chennai | devops training in chennai with placement | devops training in chennai omr | devops training in velachery | devops training in chennai tambaram | devops institutes in chennai | devops certification in chennai | trending technologies list 2018

    ReplyDelete
  38. Hey, Wow all the posts are very informative for the people who visit this site. Good work! We also have a Website. Please feel free to visit our site. Thank you for sharing.AngularJS Training in Chennai | Best AngularJS Training Institute in Chennai

    ReplyDelete
  39. Hi, the post which you have provided is fantastic, I really enjoyed reading your post, and hope to read more. Thank you so much for sharing this post, I appreciate your work.
    norton.com/setup | office.com/setup | office.com/setup | mcafee.com/activate

    ReplyDelete
  40. It is very interesting post, the information is very useful. Thank you for sharing such a amazing post.

    www.office.com/setup

    ReplyDelete
  41. thanks for sharing the nice and useful updates, character count

    ReplyDelete
  42. Hi! The post you published is well-written and informative. It has more topic discussions which i want really. So helpful to me. Keep updating.
    German Training in Chennai
    german classes chennai
    Python Classes in Chennai
    R Programming Training in Chennai
    Angularjs Training in Chennai
    Angularjs course in Chennai

    ReplyDelete
  43. Wow!! Really a nice Article. Thank you so much for your efforts. Definitely, it will be helpful for others. I would like to follow your blog. Share more like this. Thanks Again.
    iot training in Chennai | Best iot Training Institute in Chennai

    ReplyDelete
  44. Infiltrate the gaming world with BGAOC online casino, win and get income by day. great game slot online Play at any time in an online casino.

    ReplyDelete
  45. Thanks for such a great article here. I was searching for something like this for quite a long time and at last, I’ve found it on your blog. It was definitely interesting for me to read about their market situation nowadays.React js training in Chennai | Best React js training institute in Chennai |

    ReplyDelete
  46. Geek Squad Tech Support is a group of tech expert. The experts of geek squad team are capable of resolving various tech issues. In case of any tech help contact Geek Squad Tech Support.

    ReplyDelete
  47. Brother Printer Support is team of well experienced experts who are capable to resolve your printer issue. If you face any problem with your printer like cable problem, blank screen issue, or your printer is not working properly then reach our experts by making a call at toll free number of Brother Support helpline and get instant help.

    ReplyDelete
  48. HP Printer Support is active helpline that is available round the clock to resolve Hp printer problems. If you face any problem with your printer like device is not working properly, paper jamming issue, cable wire problem and others then reach experts of HP Printer Support and get instant help.

    ReplyDelete
  49. AOL Tech Support Phone Number is a customer care helpline that is offered by one of world's best mail service provider. The experts at this toll-free helpline renders all your forget password, password recovery and other related issues. Reach them anytime of day or night at AOL Tech Support whenever you need their help.

    ReplyDelete
  50. Epson Printer Support is available whole day and night to resolve your printer problems. If you face any problem with your epson printer device like device is not working properly, cable problem, cartage problem, blank screen and others then contact at Epson Support and resolve your issue in no time.

    ReplyDelete
  51. Dell Printer Support is a team of well experienced experts who takes care of your dell device problems. If face any problem with your device like your device is crashed, device is not working properly, paper jamming or others then contact at Dell Support and get instant help.

    ReplyDelete
  52. Many students face the problem of stress in college. Whether it is because of social anxiety, or not being able to clear exam etc. Most of the times, students get stressed due to their piled up assignments. If it is with you also then you might seek for Online Assignment Help.

    ReplyDelete
  53. Acer Support is a team of well experienced experts who takes care of your Acer devices. If you are facing any problem with your Acer device like your device is crashed, device is not working properly or any other problem then contact toll free number of Acer Tech Support and get instant help.

    ReplyDelete
  54. Preparing a thorough and precise literature review is crucial when you present your academic paper. It is a general aspect of the assignment to be followed when you are writing your dissertation or thesis. When you have a literature review rightly in place, your readers will know that you have not ignored the basics of conducting research. If you are not entirely adept at writing one, then hire the research paper writing service as per your convenience.
    A literature review assists you to develop a connection with your readers so they can understand that you’ve gone through the research process thoroughly. In return, you earn their trust and appreciation since you've done your share of research. If the research process seems too tiresome, then look for online College Paper Writing Services.

    ReplyDelete
  55. This comment has been removed by the author.

    ReplyDelete
  56. Canon Printer Support is a team of experts who takes care of your canon device issue. If face any problem with your device like your device is crashed , device is not working properly or others then contact Canon Support and get instant help.

    ReplyDelete
  57. Best Buy Geek Squad is a repair service that is meant to fix your broken gadgets. We advise you to simply call the Best Buy Geek Squad experts at their toll-free number and you would be helped instantly.

    ReplyDelete
  58. Such a Great Article!! I learned something new from your blog. Amazing stuff. I would like to follow your blog frequently. Keep Rocking!!

    Dot Net Training in Chennai
    Full Stack Training
    MEAN Stack Training

    ReplyDelete
  59. HP Support is a group of experts who deals with every issue with your HP devices. These experts are proficient enough to give you the best of services.HP Support experts are quite efficient in giving repair services.

    ReplyDelete
  60. Dell Support is a team of experts who take care of your dell device issue. If face any problem with your device like your device is crashed , device is not working properly or others then contact Dell Tech Support and get instant help.

    ReplyDelete
  61. Brother Printer Support team handles all the tech issues like paper jamming, improper cable connection, ink issues etc. perfectly. Brother Support team is active 24/7 for customer satisfaction, In case of any Printer issues contact Brother Printer Support.

    ReplyDelete


  62. Geek Squad Tech Support group is accessible 24/7 across the globe. These experts are trained to resolve various tech issues. Call the experts at Geek Squad Tech Support for 24/7 help and avail best help on device repair.

    ReplyDelete

  63. Geek Squad Online Support provides online support for your damaged devices. The team of online support is experienced in dealing with tech issues online. In case you're facing issue with your device contact Geek Squad Online Support

    ReplyDelete

  64. Trend Micro Geek Squad is the answer to each one of your queries with respect to antivirus. Trend micro provides the best antivirus support. Dial Geek Squad Phone Number for more information.

    ReplyDelete
  65. Thanks for such a great article here. I was searching for something like this for quite a long time and at last, I’ve found it on your blog. It was definitely interesting for me to read about their market situation nowadays.angularjs best training center in chennai | angularjs training in velachery | angularjs training in chennai | angularjs training in omr |

    ReplyDelete
  66. Resources like the one you mentioned here will be very useful to me ! I will post to this page on my blog. I am sure my visitors will find that very useful

    href="https://www.mytrainingbangalore.com/seo-training-in-bangalore/" rel="nofollow"SEO Training in Bangalore
    href="https://www.mytrainingbangalore.com/" rel="nofollow"Best Training in Bangalore

    ReplyDelete
  67. Packers and Movers Bangalore as a Services providing company can make all the difference to your ###Home Relocation experience. Bangalore based Company which offers versatile solutions, Right team that easily reduce the stress associated with a ✔✔✔Household Shifting, ***Vehicle Transportation. we help things run smoothly and reduce breakages and offer you seamless, Affordable, Reliable Shifting Services, Compare Shifting Charges @
    Packers And Movers Bangalore

    ReplyDelete
  68. Hey Nice Blog!! Thanks For Sharing!!!Wonderful blog & good post.Its really helpful for me, waiting for a more new post. Keep Blogging!
    SEO company in coimbatore
    Digital Marketing Company in Coimbatore
    web design in coimbatore

    ReplyDelete
  69. studentsassignmenthelp.com offers assignment writing service in the UK with on-time delivery, 100% plagiarism free, and unique work with the help of UK Assignment Writer on a very cheap price. Assignment written by UK assignment writers will help you to improve your academic profile.

    ReplyDelete
  70. Is Essay help is also a very complex task for you, and you want that somebody solve some of your assignment problem, at a very low cost . you can take help of our Experienced Assignment Writer to solve your difficult assignment problems.

    ReplyDelete
  71. I feel happy to say this I will deeply learn your blog and it’s really useful for me, keep sharing like this type valuable information regularly, I like to thanks for sharing this superb blog I hope I see you soon again time, thank you so much
    lenovo service center
    lenovo mobile service center near me
    lenovo mobile service centre in chennai

    ReplyDelete

  72. Being an academic writer from past 5 years providing assignment help to college and university students also associated with Myassignmenthelp platform. I am dedicated in providing best online academic writing services to the college students at the affordable rates.

    ReplyDelete

  73. Thank you for sharing such great information very useful to us.
    Python Training in Gurgaon

    ReplyDelete
  74. Your post was very helpful, I clearly understood the topic.
    Thank you for the information, i found the information very useful.
    If anyone looking for Python programming training in Bangalore i suggest Apponix Technologies, they provide best Python Programming training. For more information visit : https://www.apponix.com/Python-Institute/Python-Training-in-Bangalore.html

    ReplyDelete
  75. Its a wonderful post and very helpful, thanks for all this information. You are including better information.
    Python Training in Noida


    ReplyDelete
  76. Brilliant explained information. I thank you about that. No doubt it will be very useful for my future projects.
    AllAssignmenthelp.com reviews

    ReplyDelete
  77. I found this post quiet interesting and exciting, and the author of this post has explained everything in detail that is the best thing that i liked about this post. I am looking forward to such great posts.
    office.com/setup | norton.com/setup | mcafee.com/activate

    ReplyDelete
  78. I found this post quiet interesting and exciting, and the author of this post has explained everything in detail that is the best thing that i liked about this post. I am looking forward to such great posts.
    office.com/setup | norton.com/setup | mcafee.com/activate

    ReplyDelete
  79. I found this post quiet interesting and exciting, and the author of this post has explained everything in detail that is the best thing that i liked about this post. I am looking forward to such great posts.
    office.com/setup | norton.com/setup | mcafee.com/activate

    ReplyDelete
  80. Interesting information and attractive.This blog is really rocking... Yes, the post is very interesting and I really like it.I never seen articles like this. I meant it's so knowledgeable, informative, and good looking site. I appreciate your hard work. Good job.
    Kindly visit us @
    Sathya Online Shopping
    Online AC Price | Air Conditioner Online | AC Offers Online | AC Online Shopping
    Inverter AC | Best Inverter AC | Inverter Split AC
    Buy Split AC Online | Best Split AC | Split AC Online
    LED TV Sale | Buy LED TV Online | Smart LED TV | LED TV Price
    Laptop Price | Laptops for Sale | Buy Laptop | Buy Laptop Online
    Full HD TV Price | LED HD TV Price
    Buy Ultra HD TV | Buy Ultra HD TV Online
    Buy Mobile Online | Buy Smartphone Online in India

    ReplyDelete
  81. Thanks for sharing this interesting post.
    mcafee activate
    norton.com/setup
    office.com/setup
    cox webmail
    <a href="http://mychromecastsetup.com/”>chromecast.com/setup</a>

    ReplyDelete
  82. Hire a homework writer from students assignment help on homework helpers Australia service and find the best homework writing help from here by 24*7 hours customer support. Check the all avail services today.

    ReplyDelete

  83. Amazing Article! Your Artical is very informative and I felt quite interesting reading it. Thanks for posting such post.
    Please visit our site to undergo best foreign language courses

    Foreign Language classes in Chennai | English courses in Chennai | Foreign Language classes in Anna nagar

    ReplyDelete
  84. เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีเกมส์สล็อตออนไลน์ 1688 slot อีกมากมายให้คุณได้ลอง
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688

    ReplyDelete
  85. โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสมาชิกที่นี่ >>> Gclub online

    ReplyDelete
  86. AVG Support helps the troubled customers who are having issues

    with there antivirus software. Also the experts working at the AVG Support Number are accessible 24/7 to rescue every user.

    ReplyDelete
  87. At times, students do understand the topic but fail to write coursework papers because they do not know how to proceed with the topic. Coursework writing requires extensive research and substantial analysis. Students often do not know where to search for the right information and how to analyze data. We, on the other hand, have a grasp on the tricks of the business and therefore provide top quality coursework help services.

    ReplyDelete
  88. Thank you for sharing such valuable information with us..

    Website Designing Company in Delhi

    ReplyDelete
  89. Kaspersky Support resolves all those issues that the irritated customers may have issue with their antivirus software. Now get access to instant solutions on the same, as the experts available at Kaspersky Support Number would help you with quick resolutions.

    ReplyDelete
  90. Looking for latest update on TNPSC exams? Kalviseithi - #1 educational portal offer latest news about TN state government jobs, educational news and much more information.

    ReplyDelete
  91. Get pay and buy assignments services from our best and experienced writers who are working in this field from more than 10 years. Obtain good marks in college exam from submitting your assignment on time. Hire Extraordinary assignment writers to complete your assignment query on time and get higher marks in your academics for successful future.

    ReplyDelete
  92. I really like you post good blog,Thanks for your sharing.

    - Richard Groover

    ReplyDelete
  93. QuickBooks Payroll Support Number
    has made payroll management quite definitely easier for accounting professionals. There are so many individuals who are giving positive feedback if they process payroll either QB desktop and online options

    ReplyDelete
  94. Attend The Python training in bangalore From ExcelR. Practical Python training in bangalore Sessions With Assured Placement Support From Experienced Faculty. ExcelR Offers The Python training in bangalore.
    python training in bangalore

    ReplyDelete
  95. Problems are inevitable and so they tend not to come with a bang. All of us at QuickBooks Pro Support contact number is ready beforehand to give you customer-friendly assistance in the event that you talk with an issue using QuickBooks Support Phone Number.

    ReplyDelete
  96. As company file plays a really crucial role in account management, such that it becomes a little tough to spot. File corruption issue is a bit tricky, however, you should overcome it for very long as per the 2nd instances.
    VISIT : https://www.customersupportnumber247.com/

    ReplyDelete
  97. “Just dial our Quickbooks Support Phone Number to inquire of about for Quickbooks Payroll customer service to get rid of payroll issues. We make use of startups to small-scale, medium-sized to multinational companies."

    ReplyDelete
  98. QuickBooks Payroll Support Phone Number software may be the better option. You can certainly do WCA, PAYE, SDL along with UIF calculations. This generates annual IT3A as well as IRP5. Employees also result in the loan. How will you manage that? QuickBooks does that in ease.

    ReplyDelete
  99. Everbody knows you can find always two sides to a coin and QuickBooks Customer Support Number is not any different. This software also throws some errors over time. Sometimes it becomes rather difficult to know this is using this error code or message.

    ReplyDelete
  100. Great article quite informative, We provide support for office https://install-office.com/setup/

    ReplyDelete
  101. Edmonton DJ
    Edmonton DJ Services
    Wedding DJ Edmonton
    Edmonton Wedding DJ

    ReplyDelete
  102. UNINTERRUPTED SUPPORT AT QUICKBOOKS ENTERPRISE SUPPORT CONTACT NUMBER
    QuickBooks Enterprise Support Number team assists you to deal with most of the issues of QB Enterprise.

    ReplyDelete
  103. Our QuickBooks 24 Hour Customer Service channel- We understand the complexity and need with this accounting software in day to day life. You can’t wait for just about time for you to get a fix of each and every single QB error. Therefore we have designed a especially dedicated team of certified professionals at QuickBooks Technical Support contact number who are with the capacity of understanding your issues and errors in minimum time as well as in probably the most convenient way. Dial our toll-free and avail the QuickBooks Support Phone Number available at the essential pocket friendly price.

    ReplyDelete
  104. If you're in hurry and business goes down because of the QB error it is possible to ask for Quickbooks Consultants or Quickbooks Proadvisors . If you'd like to consult with the QuickBooks experts than AccountsPro Quickbooks Support Number is actually for you !

    ReplyDelete
  105. You simply have to build a straightforward charge less turn to our QuickBooks Support Phone Number variety and rest leave on united states of america country. Without doubt, here you will discover the unmatchable services by our supportive technical workers.

    ReplyDelete
  106. Norton Support rescue all those troubled customers who have issue with their antivirus software. To avail instant resolutions on the same, we advice all the customers to take help from experts available at Norton Support Number.

    ReplyDelete
  107. QuickBooks Tech Support Number that exist in the marketplace on our website. Unneeded to mention, QuickBooks has given its utmost support to entrepreneurs in decreasing the purchase price otherwise we’ve seen earlier, however, an accountant wont to keep completely different accounting record files. Using the assistance of QuickBooks, users will maintain records like examining, recording and reviewing the complicated accounting procedures.

    ReplyDelete
  108. Great article quite informative, We provide support for office https://install-office.com/setup/

    ReplyDelete
  109. Our Professionals have designed services in a competent means so they will offer you the required techniques to the shoppers. we now have a tendency to at QuickBooks Support Phone Number client Service are accessible 24*7 you just have to call our.

    ReplyDelete
  110. QuickBooks Error 3371, Status Code 11118 has been the pioneer in accounting solutions for businesses all around the globe. This software has spread like wildfire and is very effortlessly managing all of the accounting and finance related processes for businesses world over.

    ReplyDelete
  111. The article is very interesting and very understood to be read, may be useful for the people. I wanted to thank you for this great read!! I definitely enjoyed every little bit of it. I have to bookmarked to check out new stuff on your post. Thanks for sharing the information keep updating, looking forward for more posts..
    Kindly visit us @ Madurai Travels | Best Travels in Madurai | Cabs in Madurai
    Tours and Travels in Madurai

    ReplyDelete
  112. Intuit QuickBooks Payroll Support 2019 services are accessed by many people people business people, Accountants, CA, CPAs to calculate taxes and pay employees. Unfortunately, types of issues and errors arise for which they have to contact the Intuit Payroll support team.

    ReplyDelete
  113. Intuit has developed the QuickBooks Payroll Support Phone Number form with almost evolution to carry out all checks and taxes issues. Since no body is well in this globalization. Quite often when folks are protesting about incorrect calculation and defaults paychecks results.

    ReplyDelete
  114. QuickBooks Enterprise errors troubling you? Are you currently fed up with freezing of QuickBooks? If yes, you then have browsed off to the right place. QuickBooks Enterprise Support Phone Number is successfully delivering the whole world class technical assistance

    ReplyDelete
  115. The article you have shared here very awesome
    cat mario

    ReplyDelete
  116. At Quickbooks Support Number, you will find solution every single issue that bothers your projects and creates hindrance in running your company smoothly. Our team is oftentimes ready to enable you to with all the best support services you should possibly ever experience.

    ReplyDelete
  117. Even although you are feeling that the full time is odd to call for help, just pick up your phone and dial us at QuickBooks Enterprise Support Phone Number because we offer our support services 24*7. We believe that the show must go on and thus time will not be a concern for all of us because problems do not come with any pre-announcements.

    ReplyDelete
  118. Thanks for sharing this awesome post.

    - mawto

    ReplyDelete
  119. Great article quite informative, We provide support for Mcafee at:
    mcafee activate
    mcafee.com/activate
    www.mcafee.com/activate

    ReplyDelete
  120. Python is an interpreted programming language that lets you work quickly and is very portable so I like its convenience.
    douchebag workout 2

    ReplyDelete
  121. Excellent Blog. I really want to admire the quality of this post. I like the way of your presentation of ideas, views and valuable content. No doubt you are doing great work. I’ll be waiting for your next post. Thanks .Keep it up!
    Kindly visit us @
    Luxury Packaging Box
    Wallet Box
    Perfume Box Manufacturer
    Candle Packaging Boxes
    Luxury Leather Box
    Luxury Clothes Box
    Luxury Cosmetics Box
    Shoe Box Manufacturer
    Luxury Watch Box

    ReplyDelete
  122. On September 22, 2014, Intuit publicized the release of QuickBooks 2015 with types that users have been completely demanding through the last versions. Amended income tracker, pinned notes, better registration process and understandings on homepage are among the list of general alterations for most versions of QuickBooks 2015. It will also help for QuickBooks Enterprise Support to acquire technical help & support for QuickBooks

    ReplyDelete
  123. Intuit QuickBooks Payroll Technical Support Number accounting software enables you to prepare your invoices, manage your business payrolls, track your business inventory, control cash flow, and be tax-ready.

    ReplyDelete
  124. Amazing! I like to share it with all my friends and hope they will like this information.
    Regards
    Power Bi Training In Hyderabad
    Power Bi Online Training

    ReplyDelete
  125. Jobs divine is one of the best job consultancy in thrissur. We provide all types of jobs in thrissur. We do have many job vacancies in thrissur. Sign up now for a free account and get thrissur jobs instantly. The candidates who in search of good career in Thrissur can apply and get easily their dream job through jobs divine

    job consultancy in thrissur

    thrissur jobs

    top job placement agency in thrissur

    job vacancies at thrissur

    jobs at thrissur

    thrissur job vacancies

    ReplyDelete
  126. QuickBooks Enterprise Tech Support Number is sold as an all in one single accounting package geared towards mid-size businesses who do not require to manage the accounting hassle by themselves.

    ReplyDelete
  127. On earth filled with smart devices around the corner, QuickBooks online could be the perfect accounting software to get your accounting works done into the smartest way. QuickBooks online version offers you its new and smart features regularly as with Intuit is mainly focusing on development of its online software a lot more than the desktop one. To work with this digitalized and smart software, you'll need a technical assistance channel that can easily be accessed round the clock in just a single call. Your QuickBooks Support Number is available at QuickBooks Tech Support telephone number which provides you precisely what you will need for smooth working of QuickBooks software. In this website, we will be discussing the main cause and troubleshooting ways of this issue.

    ReplyDelete
  128. Amazing! I like to share it with all my friends and hope they will like this information.
    ThePromoX

    ReplyDelete
  129. you can go through AllAssignmentHelp reviews. It will help you to know about the services, and it will help you to know whether that site is reliable or not.

    ReplyDelete
  130. TutuApp is the most well known iOS Helper for iPhone, iPad gadgets. Download TutuApp Helper and begin introducing fun applications
    https://tutuapp.blog
    tutuapp
    tutuapp download
    tutuapp vip

    ReplyDelete
  131. GBWhatsApp isn't yet discharged for iOS which implies GBWhatsApp isn't accessible for iPhone, iPad and iPod Touch. Be that as it may, you can utilize WhatsApp Messenger by downloading the application from iTunes.
    https://gbwhatsapp.vip/
    gbwhatsapp
    gbwhatsapp download
    gbwhatsapp apk

    ReplyDelete
  132. Our QB Experts are pretty familiar with all of the versions of QuickBooks Enterprise released available in the market till now by Intuit. So whether it's selecting the most suitable type of QB Enterprise for your requirements or assessing the sorts of errors that are usually encountered into the various versions of QB Enterprise, Our QuickBooks Enterprise Support Phone Number will have no difficulty in delivering the correct guidance and help with any issues and errors that users may have with QB Enterprise version.

    ReplyDelete
  133. A small grouping of execs can handle you manually as a result of they’re absolute to offer the standard services. So, QuickBooks Support Phone Number in the event that you face any issue along with your package you don’t need to go anywhere except us.

    ReplyDelete
  134. That really work with you on QuickBooks Support contact number are responsible to manage every Quickbook technical issue that produces in https://www.fixaccountingerror.com/ software.

    ReplyDelete
  135. QuickBooks Payroll Support Phone Number Well! If you’re not able to customize employee payroll in Quickbooks which makes the list optimally, in QB and QB desktop, then read the description ahead.

    ReplyDelete
  136. Using those networks you surely will able to reach them for using their enterprise service.
    Any of the customers who want to active Intuit QuickBooks Support services, very first should have to active the hosting services.

    ReplyDelete
  137. If you are using an ‘Encryption software’ it is strongly suggested to disable it to get away with QuickBooks Error Code 6000-301. Using third-party software for encrypting your business file is not recommended. You really need to talk to a technical expert or encryption software vendor on how best to disable this choice.

    ReplyDelete