Monday, May 18, 2015

Water Effects with a Function generator

In this post, I describe how I re-created some really cool effects using a stream of water. This  was a popular Youtube video a while back and I thought that I could not only recreate the effect, but take it a step further with the capabilities that we have in our Trueform waveform generators.



I made (with the help of our video team in Keysight) a new set of videos that I hope that you have seen. If not, the first video has some background music that is timed to change when the water effects change. This video only shows the cool water streams and does not explain how to create the effects.


The second video goes into more depth on what equipment is used and how I use to signals to create the neat water stream effects. You will notice some flickering in the video, this is due to the timing of the camera and the timing of the light strobe light being misaligned.




If you came here from the video, you might be looking for some more details on how I created the effect. With out further ado, let's get into some details.

Equipment:
Trueform Waveform Generator with 2 channels
Ikea LED light
8 inch subwoofer
Audio amplifier
3/4" plastic tubing to route the water
Water pump from Amazon

Tub to catch the water

The basic setup:

To put it into laymen terms, the function generator produces a signal that is used to control the subwoofer speaker. The subwoofer is physically connected to a water hose that is going across the front of the speaker. I epoxied a tube connector to the front of my subwoofer. The subwoofer then moves the water hose in a repeated pattern at a frequency that I control with my function generator. The function generator does not produce enough power to drive the speaker so I put the audio amplifier between the subwoofer and function generator in order to get enough vibrations.

To get the different visual effects, I use the second channel on the function generator to control a LED spot light. This LED spot light can turn on and off faster than a human eye can see. When we turn the LED on/off at a really fast rate it looks like the light never turns off, but it does. This provides us with a strobe light effect that generates the cool water flows that we see in the video. I made a custom cable that when from a BNC connection of the generator to the LED light.

The water pump takes the water from the tub and recycles it through the front of the speaker.


The Effects:

Frozen in air

 The "Frozen" water effect has the  basic premise of having the water signal at the same frequency as the LED light.

Function generator channel 1 has a sinewave at 50 Hz. A sinewave the most simple and basic waveforms and provides us with a nice smooth movement on the water hose.


Channel 2 on the function generator has a pulse pulse at the same frequency (50 Hz) as channel 1. For those of you that are technically inclined the signal is 3Vpp with 1.5V offset. 1ms on time.

By setting the LED light's on frequency to be the same as the speaker, we are effectively looking at the same pattern of water every time the LED turns on. Since the frequencies are matched the same water "image" is captured due to the repetitive speaker and LED light patterns. Its like looking at a clock once every 24 hours. If you look at it exactly the same time every day, then time looks like it is standing still. The frequency that you are looking at the clock (24 hours) matches the frequency that it takes for the clock to repeat (24 hours).

TIP: The shorter the on time, the more crisp the water will look, but it does create the "flashing" or flicker elements that we see in the video. A longer on time will make the water look a little more fuzzy and the shape of the water will be not a defined. Longer on times do have the additional benefit of providing brighter light from the LED.

The other effects basically change the frequency or the size of the signal.
Speaker at 50 Hz,
LED light at 50 Hz.


Slow Gravity 

In this effect, the water looks like it is slowly falling down, almost as if gravity is not as strong here. Rest assured, we haven't broken gravity and we're not using slow motion video. But we have used the lighting to our advantage. The speaker is still set to 50 Hz, but the trick here is that the LED light is now slightly slower than the speaker. The LED is now at 49 Hz. By having the LED "look" at the water a little bit slower than the speaker frequency it looks like the water is slowly falling down. Going back to our clock analogy, if you look at your clock once every 24:01 hours (add a minute), then time will slowly go forward a minute per day.
Speaker at 50 Hz,
LED light at 49 Hz.


 

 

Anti Gravity

No your eyes aren't playing tricks on you, the water does look like it is flowing upwards. In this anti-gravity effect, it almost looks like I am reversing the video from above. Again its not a video effect and the fish aren't swimming backwards. If I reversed the video the fish would be.
 The speaker is still set to 50 Hz, but the trick here is that the LED light is now slightly slower than the speaker. The LED is now at 51 Hz. By having the LED "look" at the water a little bit faster than the speaker frequency it looks like the water is slowly traveling up, maybe looking like it is going back in time.  In our clock analogy, if you look at your clock once every 23:59 hours (subtract a minute), then time will slowly go backwards a minute per day.
Speaker at 50 Hz,
LED light at 51 Hz.


 

 

Yo Yo

In the Yo Yo effect, the water looks like it switches from going down to going up, like a Yo-Yo. Here's where it gets a little bit more interesting by using a function generator. In this effect, we keep the strobe light at a fixed 50 Hz. However, we now do a relatively slow frequency modulation between 40 and 60 Hz. Frequency modulation is the same signal modulation techniques that FM radio stations use. This is a simplified version in that the frequency changes between 40 and 60 at a continuous basis. The visual effect of this means that the speaker is sometime slower and sometimes faster than the strobe light thus causing the water stream to look like it is sometimes going down and sometimes
going up.
Speaker changing between 40 and  60 Hz,
LED light at 50 Hz.



Opening Fan

This effect has the water shifting from a narrow stream to a very wide stream of water. Similar to the yoyo effect, the opening fan effect uses a well known signal modulation technique. Amplitude modulation has been around for at least a century and is still used in AM radio stations. AM signals vary the size of a signal. So when the water's "fan" is wide open, the signal going to the speaker is large. When the fan is a single stream, the signal is small. Think of it as changing the volume on the speaker in a fast manner.  Again, we use a very slow changing AM signal here that changes so that you can see the water effect. Normally AM signals change much faster.
Speaker at 50 Hz,
LED light at 50 Hz.


Double Helix

In the Double Helix, it looks like there are two streams intertwining together. Its a simple concept to generate the Double Helix. If your light is at the same rate as your speaker, then you get one stream. But if the light is at twice the rate of your speaker you get 2 streams. You are basically looking at it twice as often. In the video we changed the speaker rate to 40Hz and put the LED light rate at 80 Hz. I found that 40 Hz was better than 50 Hz because the helix patterns were wider. If the frequency of the speaker was faster we would see more waves in our signal, too many waves would ruin the double helix effect.
Speaker at 40 Hz,
LED light at 80 Hz.

 

 

 

 Double Helix Slow Gravity

Just like the slow gravity effect with a single stream, the LED light is now just a little bit slower. Since we started with twice the frequency of the speaker, we are now just a little bit slower than twice the frequency. I chose 78 Hz because I liked the effect.
Speaker at 40 Hz,
LED light at 78 Hz.

 

 

 

 

 

Double Helix Anti Gravity

Just like the slow gravity effect with a single stream, the LED light is now just a little bit slower. Since we started with twice the frequency of the speaker, we are now just a little bit slower than twice the frequency. I chose 78 Hz because I liked the effect.
Speaker at 40 Hz,
LED light at 82 Hz.

 

 

 

 

 

 

Slinky Effect

In this effect, the water is "frozen" in air. However, the water stream quickly goes from a long stream to a stream with many curls. From the function generator, we are sweeping the frequency from a slow 20Hz to a faster 80Hz signal. We are able to keep the water frozen in air by keeping both channels of the generator at the same frequency as they change from 20 to 80 Hz.

 In this part of the video, you'll notice that the flicker on from the camera has a lot of black spots. This is because as we change the frequency of the lights, there are more conflicts with the frame rate of the camera.



 

Additional Tips

Note about the water flow. If you have a strong continuous water flow, you can create an effect that looks really good from top to bottom. The water pump that we had was ok and the stream was continuous for about 5-7 inches. At the end of the flow, the water started to break up and didn't have a great repetitive effect for us to view with the strobe light. Ideally you would use water from your sink or outdoor spigot as a water source.

The water tube should be placed so that the tip is just barely outside of the subwoofer's lip. Placing it too far from the subwoofer will allow the hose to move inconsistently and ruin the effect. Placing it to close will cause the water to hit the subwoofer and create streams in the water shape. Not to mention it gets your subwoofer wet.

Hope you enjoyed watching the videos and reading this blog entry. Thanks!



73 comments:

  1. Amazing generator its complete work on my terms thanks for share it warranty terms and conditions template .

    ReplyDelete
  2. These are various certified Laboratories and Calibration Centres which are giving testing & calibration services as per the Indian Standards. xenon test chamber

    ReplyDelete
  3. That's a great topic. How do you think, maybe you need someone to write my paper for you?

    ReplyDelete
  4. this is the reason that people love to visit this amazing and best torrenting site in the year 2018.

    ReplyDelete
  5. SSC exams take massive effects in the student’s life, and these are the first public examinations for the students, so students are worrying about the results, they are very panic about the examination results.

    upresults.nic.in

    ReplyDelete
  6. This is very interesting, You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Regards - www.office.com/setup
    www.office.com/setup

    ReplyDelete
  7. Now this tutorial is really useful. Thanks for sharing it, guys.
    บาคาร่าออนไลน์

    ReplyDelete
  8. I wanted to thank you for this great read!! I definitely enjoying every little bit of it I have you bookmarked to check out new stuff you post. OMC engine water pump

    ReplyDelete
  9. Pretty good post. I just stumbled upon your blog and wanted to say that I have really enjoyed reading your blog posts. Any way I'll be subscribing to your feed and I hope you post again soon. Big thanks for the useful info  KP-LOK

    ReplyDelete
  10. I have read your article, your article is very detailed and meticulous, thank you for sharing.
    temple run 3

    ReplyDelete
  11. I am convinced that your website is convinced that weblog is very new. Probably I am going to bookmark your site. There are certainly impressive stories. Passion for sharing your website with us.
    Regards - www.office.com/setup
    www.office.com/setup
    www.office.com/setup

    ReplyDelete
  12. Some genuinely superb posts on this site, thanks for contribution.
    Regards - www.office.com/setup
    www.norton.com/setup

    ReplyDelete
  13. Chase bank was originally founded in Chicago on December 1, 2000. It has been ranked as one of the finest banking institutions in Chicago. Being an 18-year-old institution, it has earned a huge respect and attained a great success.

    Chase Routing Number

    ReplyDelete
  14. its a good article andis very informative keep going on thank you. vidup.me pair
    The only annoying thing with vidup.me/pair is the pair error which prevents us from getting connected to the server and accessing movies, TV shows and much more

    ReplyDelete
  15. I am convinced that your website is convinced that weblog is very new. Probably I am going to bookmark your site. There are certainly impressive stories. Passion for sharing your website with us.
    Regards - www.norton.com/setup

    ReplyDelete
  16. you are actually a good webmaster. The site loading speed is incredible. It seems that you’re doing any unique trick. Also, The contents are masterwork. you have done a excellent job on this topic! FCPX

    ReplyDelete
  17. I have read through other blogs, but they are cumbersome and confusing more than your post. I hope you continue to have such quality articles to share with everyone! I believe a lot of people will be like to read this article!
    devast io

    ReplyDelete
  18. The subject of Philosophy and its subcategories have been widely discussed in both the Western and non-Western world albeit with different focuses. Philosophy includes many different subfields involving investigation into our existence. These subfields include epistemology, ethics, logic, metaphysics, philosophy of science, social and political philosophy, and Metaphilosophy. Epistemology focuses on the study of Knowledge, also known as “Theory of Knowledge”. Ethics involves the study of moral values and rules, Logic; the study of reasoning. Metaphysics is the study of being and knowing also known as the principles of reality. Read more at The concepts of reality

    One of the first points to be clear about is that a philosophical essay is quite different from an essay in most other subjects. That is because it is neither a research paper nor an exercise in literary self-expression. It is not a report of what various scholars have had to say on a particular topic. It does not present the latest findings of tests or experiments. And it does not present your personal feelings or impressions. Instead, it is a reasoned defense of a thesis.

    ReplyDelete
  19. Without fail, your writing style is top professional; even your website also looks amazing thank you for posting. buy youtube subscribers

    ReplyDelete
  20. Thank for your writting! It is easy to understand and detailed. I feel it is interesting, I hope you continue to have such good posts.
    run 3

    ReplyDelete
  21. telugu dj songs is an youtube channel for latest and old dj songs with easy download links of High Quality Mp3 Songs In 320KBPS & 128KBPS.

    ReplyDelete
  22. The blog post is great. It explores water effects with a function generator. You can find videos of cool water experiment along with the article. The first video only demonstrates the cool water streams and does not give details on how to create the effects. The next video goes into deep on what equipment is used and how to use signals to make the neat water stream effects.

    ReplyDelete
  23. Thanks a lot for sharing it, that’s truly has added a lot to our knowledge about this topic. Have a more successful day. SEO Services Kerala
    My Assignment Help Australia

    ReplyDelete
  24. This article is really fantastic and thanks for sharing the valuable post.

    mangafox

    ReplyDelete
  25. Thank you for that information you article
    happy wheels

    ReplyDelete
  26. Thank you for sharing valuable information. Nice post. I enjoyed reading this post.
    red ball 4

    ReplyDelete

  27. I have read your post. It solved some aspects of the problem. I think you need to make the problem clearer super smash flash 2

    ReplyDelete
  28. Your Water Effects creation is amazing.
    super fighters

    ReplyDelete
  29. When I'm sad I usually play games. It will make me more comfortable. I like to spend time like that
    happy wheels

    ReplyDelete
  30. Nice post
    If you are looking for an online homework helper that is gentle to your pocket .
    Best homework help Tutor is here .

    ReplyDelete
  31. Thank you for the information, may be useful for all people of course who read this article
    linebacker alley 2

    ReplyDelete
  32. The shorter the on time, the more crisp the water will look, but it does create the "flashing" or flicker elements that we see in the video. A longer on time will make the water look a little more fuzzy and the shape of the water will be not a defined. Longer on times do have the additional benefit of providing brighter light from the LED. krogerfeedback

    ReplyDelete
  33. This article is great. I like it very much. Thank you.
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete
  34. Thank you for making me realize this. It's great.
    เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete
  35. Students of all educational levels have experienced stress in face of their busy schedules and obligations that they can’t manage to catch up with. This website will cope with your writing tasks.

    ReplyDelete
  36. Nice post
    If you are looking for an online homework helper that is gentle to your pocket . Your best home work expert is here.visit our blogs at https://helpacads.com/subjects/

    ReplyDelete
  37. jangan lupa untuk bermain di situs judi online yang telah kami rekomendasikan ini. karena situs ini adalah situs judi online yang bisa membantu anda dalam menang banyak dalam permainan judi online
    asikqq
    dewaqq
    sumoqq
    interqq
    pionpoker
    bandar ceme
    betgratis
    paito warna
    prediksi hk

    ReplyDelete
  38. Fantastic blog post, thank you so much for sharing this.
    Bus Hire Sydney
    Bus Hire Colyton

    ReplyDelete
  39. Microsoft office is a set of application in which you create, open and share files of word, excel and power point online and offline also provide the facility of cloud storage. If you want to install setup.office.com
    https://m-soffice.net/com-setup/
    https://m-soffice.net/com-setup/
    https://m-soffice.net/com-setup/
    office setup
    office.com setup
    download office/
    www.office.com/setup
    support.office.com/setup

    ReplyDelete
  40. Nice! thank you so much! Thank you for sharing. Your blog posts are more interesting and informative. I think there are many people like and visit it regularly, including me.
    light novel

    ReplyDelete
  41. Nice post
    If you are looking for an online homework helper that is gentle to your pocket . Your best home work expert is here.visit our blogs at
    https://helpacads.com/branchdetail/Civil/

    ReplyDelete
  42. ar rental in Iran
    after arriving to Iran for exploring freely in different cities you can easily use car rental servicesand rent the car you want.
    tank u for any ting
    search and see Iran and enjoy that in Iran tour
    اجاره ون

    ReplyDelete
  43. This is really amazing. Great information about blog. myfirstpremiercard

    ReplyDelete
  44. JOKERINDO99 adalah salah satu agen joker123 / joker gaming , agen situs slot online, tembak ikan online dan live casino terpercaya
    Joker123
    data sgp

    ReplyDelete
  45. Tramadol is a drug which is an opioid pain medication and you can buy Best Tramadol online from us. The Online Pain relief Pills tramadol pills has been categorized as depressant and analgesic. The active component of this drug is Tramadol Hydrochloride (HCL) and it could be combined with the acetaminophen and they can be prescribed in the type of tablets.

    ReplyDelete
  46. We are the best writing company providing Custom Dissertation Writing Service combined with a vast array of services. We offer College Term Paper Writing Services, essay assistance, dissertation writing services and research writing help.

    ReplyDelete
  47. Thanks a ton for sharing a wonderful information which I am looking for a longer period of time.Now Download Microsoft Office Setup by entering 25 Digits Office Product Key and Get Started with Office Setup Installation in easy steps.
    office.com/setup

    ReplyDelete
  48. This comment has been removed by the author.

    ReplyDelete