Friday, September 20, 2013

Measuring Injected Current and Input Bias Current on a DMM

I recently did a webinar (Web based seminar) for the Truevolt series of DMMs. A question came up that I couldn't answer right away so I promised the person to blog about it. The question was about measuring injected current on the DMM.  Since I didn't know how to do it off the top of my head I needed to do some research.

Truevolt's datasheet highlights the DMMs' low level of injected current but there isn't a line item on the spec sheet for what the injected current should be. So I thought that I would measure the injected current and show my results on this blog. Keep in mind that this is not a specification and I'm only measuring on one unit, but it should give you an idea of the levels of injected current that you can expect.

When I started my investigation I got confused on whether I should be measuring input bias current and did some research into that too. I'll speak about the differences below between the two currents and how to measure both signals on my 34461A. These techniques should be viable for any DMM that you have on your bench.

Measuring injected current

Let's start off with the question from the webinar. What's the injected current level of a Truevolt DMM. You might be also asking yourself what is injected current. Injected current for a DMM is low level current that comes from the DMM earth referenced circuitry such as the transformer.  Since the DMM has floating inputs this current does not normally affect your measurements. However this current can be seen when your device under test's (DUT) signal is earth referenced as well. The injected current will affect your AC measurements if your signal is earth referenced or poorly isolated from earth ground.

We typically characterize the injected current as an AC current. If a DMM is designed poorly, then this injected current can introduce large errors on your measurements.

It turns out that the method to measure injected current is actually fairly simple for a DMM. The only connection that you need to make is to connect the high terminal to earth ground. Then setup your DMM to make ACV measurements.The connection is shown in this simple diagram. To make the earth ground connection, I took a BNA cable and connected it to the rear earth ground screw on the back of the DMM.





I then took a few readings and used the 34461A's internal statistics to show what my average and standard deviation are.
As you can see, the average was about 50mVrms with a standard deviation of 72uV. I did a quick check to see if the noise was normally distributed and it looked like a fairly normal Gaussian distribution. 

In order to calculate the injected current from this we simply divide the ACV measurement by the input impedance of the DMM which is 1Mohm for this function. With this measurement method I can use the 1Mohm input impedance of the DMM in ACV mode as a high value shunt.


So for my DMM the injected current is about 50nA. I'm not sure if this is typical but I would guess that most units would have less than 100nA of injected current. These levels are quite good for a 6.5 digit DMM and Agilent believes that Truevolt DMMs are among the top of the class for this parameter.

Measuring Input Bias Current

I mentioned above that I started investigating input bias current because I thought it was the same thing as injected current. It turns out that input bias current is floating current that flows in or out of your DMM. This current will affect not only your earth reference measurements but your floating measurements as well. Luckily this is fairly small in most cases and the Truevolt DMM have a characteristic of <30pA at 25 C.

There are two methods of measuring Input Bias current (Ibias). One method requires knowledge of the DMM's internal input capacitance while the other is a more straightforward but not as accurate version. I used the more straightforward method since I don't know what the input capacitance of my DMM is and you might not either if you are using a different type of DMM.

The more accurate version of measuring Ibias would be to calculate the time it takes the DMM to change from one voltage to another on a fixed range after initially shorting the input terminals. You then need the input capacitance to plug into the the following equation:


For example, if the DMM were to take 1 seconds to change from  0.775V to .9V. The deltaV would be 0.125V.  If we say that the input capacitance is 200pf (this is hypothetical) then



Since I don't know the input capacitance and I'm not sure that I'd be able to get my timing down very well I'm using a different method to measure the Ibias. The more straightforward measurement would be to put the DMM into DCV and change a couple of settings:
- Set Input Z to 10M
- Turn of Autozero

The connection to the DMM is even more simple. Keep the terminals open i.e. take off any cable or signals to the DMM. By setting the input impedance to 10M it will effectively bleed off any residual charge that might be on the terminals. I had my terminals open for a while before I started taking readings.

So with the terminals open, I took a screen shot of a number of readings. The screenshot also shows the DCV settings that I have which include the two setting changes from above. My average is 9uV.

Then to calculate the Ibias current, all I need is a simple equation. With this measurement method I can use the 10Mohm input impedance of the DMM as a high value shunt.

So the resulting Ibias = 9uV/10Mohm = 0.9pA. This result is for one unit but it does show that the input bias current of Truevolt DMMs is meeting it's specification with quite a bit of margin.


253 comments:

  1. We help in setting up and Installing Microsoft Office on your computer. We provide Technical Support and other services to you. We help you with great work and other details. We are here to help you. We help you with Microsoft Office and Office installation. We help you with Great technical services at an affordable price.
    Regards- www.office.com/setup

    ReplyDelete
  2. I just want to say that all the information you have given here on is awesome. Thank you Orthopedic Hospital in Hyderabad

    ReplyDelete
  3. You have done very well its really helpful post for skinny head . if you are not satisfy to other .you can check this link and get your dental treatments. Bariatric Surgery in Hyderabad

    ReplyDelete
  4. I just want to tell you that I’m all new to blogging and site-building. I really loved your web page. Very likely I’m want to bookmark your site . You amazingly have remarkable posts. Thanks a bunch for sharing your blog.
    Regards - www.office.com/setup
    www.office.com/setup
    www.office.com/setup

    ReplyDelete
  5. Sometimes Microsoft Office users face the issues after upgrading their Windows operating system. If you are also facing such type of issues related to your Microsoft Office setup installation then contact us at office.com/setup for the best support.
    office.com/setup

    ReplyDelete
  6. McAfee.com/activate – McAfee Antivirus is one of the most critically acclaimed security program across the globe. Protect your devices and data from viruses, malware, Trojan horses, worms, and other cyber threats with real-time protection and threat scanning. Get robust protection offered by McAfee by following the process (download, install, activate) on  www.mcafee.com/activate

    ReplyDelete
  7. Microsoft Office is one amongst the most useful productivity suites for Mac and Windows. Log in at office.com/setup and browse various packages for Office 2019, Office 365, Office 2016, Office 2013, Office 2010 and more. After downloading and installing its setup, activate it with the product key from  office.com/setup

    ReplyDelete
  8. Thank you so much for sharing these amazing tips. I must say you are an incredible writer, I love the way that you describe the things. Please keep sharing.

    For more information visit on office.com/setup | office.com/setup | office.com/setup | Norton.com/setup

    ReplyDelete
  9. Go to office.com/setup to purchase, download, install, and activate Office 2019, 365, 2016 and many more. Enter You Office Product key on www.office.com/setup to activate your Office setup.

    ReplyDelete
  10. While printing some important document, you may get an error message that HP Printer Offline and printer can’t print anything. At that situation, grab the quick solution from dexterous technicians via dialing our toll-free number instead of wasting time in wandering here and there. Hence, call on the provided number and bring your offline printer to online hassle-freely. https://www.hpprintersupportpro.com/my-hp-printer-is-offline

    ReplyDelete
  11. I am really influenced to read such a great post. It is requested to keep up this habit. You must go through link Assignment Help to reduce the hectic pressure.

    ReplyDelete
  12. Many users are successfully using Free Avast antivirus, but at some point, few of them are facing trouble due to installation of Avast antivirus on their system. This trouble becomes too critical and unable to handle by the own. In that situation, users immediately need to uninstall Avast Antivirus from their system. To do in a perfect way you need to contact tech experts for antivirus issues from getting a reliable Avast Customer Support and instant help as well. https://www.avastsupportnumber.us or https://www.youtube.com/watch?v=BpOK1vxQzCA

    ReplyDelete

  13. Thanks, great post. I really like your point of view. I m Marry Taylor, I working as a support executive for printer devices. I am offering support for HP Devices and If you need help then contact HP Tech Support Phone Number +1-888-902-8333 and you can also chat us to get assistance to fix issues regarding HP printer.

    ReplyDelete
  14. Brother Printer Support Phone Number team will help you with all your technical difficulties in using brother printer and will resolve all your doubts regarding the setup and installation process. calling the tech support team will save your time and money. so call us now on Brother Printer Support Phone Number +1-888-902-8333 to help you with your difficulties.

    ReplyDelete
  15. Brother printer gets offline suddenly because of the network connection problem. Therefore, if you are encountering the Brother Printer Offline issue, then don’t get panicked! Just check your cable connection. In case the cable is loose, plug it into the power-point tightly and then use your Brother printer. While printing, if yet you are getting an offline error message, then get united with the dexterous technicians. They will help you out within the least time interval.

    ReplyDelete
  16. webroot.com/safe Enter your product key online. Create or log into your Webroot account here. Manage your security across multiple devices, with any Webroot product. www.webroot.com/safe.
    http://www.webroot-webroot.com

    ReplyDelete
  17. norton.com/setup to install setup product key, Learn how to download, install, and activate Norton Setup on your windows and Mac device still facing problem call (toll free) +1-844-546-5500 or chat our technical experts they will help you.Norton setup
    http://nortonnortoncom.com

    ReplyDelete
  18. Get all Steps for installation and download, activate MS office setup. Enter your Office product key on www.office.com/setup.
    http://office-comofficecom.com

    ReplyDelete
  19. Office.com/setup - Office Setup can be downloaded and installed on your devices by visiting the link office.com/setup online. Microsoft Office suite includes a number of world-leading applications like MS Word, MS Excel, and many others.

    ReplyDelete
  20. Office.com/setup- download,Install and activate office setup with product key at office setup.

    ReplyDelete
  21. Norton.com/setup offers its clients two different ways to buy any of its items. These two different ways are online by means of Norton.com/setup and disconnected through an approved retail location.
    http://nortoncomusa.com/

    ReplyDelete
  22. Office.com/setup makes no structures or guarantees that the Office setup Website will be open on a, hair-raising, eating up, secure or mess up free begin.
    http://officecomoffice-office.com/

    ReplyDelete
  23. Office.com/setup has no relationship with any of these outsider affiliations aside from if such relationship is unequivocally showed up. Office setup permitted use and specific ensures related with the thing, mechanical gathering, and peripherals, you should contact the key removed.
    http://office-comoffice.com/index-2.html

    ReplyDelete
  24. Office.com/setup makes no diagrams or guarantees that the Office setup Website will be open on a, solid, determined, secure or goof free present. Any Content got to, downloaded or by and large got on or using the website is utilized at your own particular watchfulness.
    http://offiicecom-setup.com/

    ReplyDelete
  25. Are you seeking for assignment help in the USA? I am an assignment writer in students assignment help.com and I have more than 10 years of experience in assignment writing so if you need help visit our website and get online help.

    ReplyDelete
  26. Ireland Assignment Help provides the best Dissertation help for all students. Our professional expert writers provide academic assistance services to all students. Students can get help from our online assignment writers 24*7.

    ReplyDelete
  27. Find Awards Latest News, Videos & Pictures on Awards and see latest updates, news, information from Feeds Box. Explore more on Awards.
    http://feedsbox.com/awards/

    ReplyDelete
  28. After purchasing office.com/setup
    need to visit office activate online to install and we provide technical services help in office setup on your Computer. http://officecom-officecom.com

    ReplyDelete
  29. Find how to download, install, activate all versions of Microsoft Office setup and activate on office.com/setup
    http://office-office-com.com

    ReplyDelete
  30. Setup your norton Antivirus with help from norton setup , norton.com/setup after reaching the site go
    with the given steps. http://norton-nortoncom.com

    ReplyDelete
  31. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article
    Activation.Kaspersky.Com
    my.avast.com
    AvastLogin
    AvastLogin
    notornlogin
    notornlogin

    ReplyDelete
  32. See how to set up your email account and fix issues with email access. Also easily reset your password or get a username reminder online.
    Bt mail

    ReplyDelete
  33. Bt mail login, Bt yahoo mail, Bt mail sign in, Bt yahoo mail login, my Bt mail, Bt login mail, Bt E mail, Bt mail log in, Bt e mail log in, Login Bt mail, Bt yahoo mail sign in, Bt mail setting, Bt internet mail, Bt e-mail, Bt mail Yahoo, Bt premium mail, Bt Mail login Page, www.bt.com/login, bt.com/login

    See how to set up your BT Mail account and fix issues with email access. Also easily reset your password or get a username reminder online.
    bt mail

    ReplyDelete
  34. See how to set up your BT Mail account and fix issues with email access. Also easily reset your password or get a username reminder online.
    bt mail

    ReplyDelete
  35. See how to set up your BT Mail account and fix issues with email access. Also easily reset your password or get a username reminder online.
    bt mail

    ReplyDelete
  36. See how to set up your BT Mail account and fix issues with email access. Also easily reset your password or get a username reminder online.
    bt mail

    ReplyDelete
  37. See how to set up your BT Mail account and fix issues with email access. Also easily reset your password or get a username reminder online.
    bt mail

    ReplyDelete
  38. After purchasing office.com/setup
    need to visit office activate online to install and we provide technical services help in office setup on your Computer. http://officecom-officecom.com

    ReplyDelete
  39. Find how to download, install, activate all versions of Microsoft Office setup and activate on office.com/setup
    http://office-office-com.com

    ReplyDelete
  40. Setup your norton Antivirus with help from norton setup , norton.com/setup after reaching the site go
    with the given steps. http://norton-nortoncom.com

    ReplyDelete
  41. Microsoft Office often releases its latest updated version of its applications and productivity suite, and every latest update comes with various amazing and advanced features for the benefits of the users. Also, Microsoft provides a complete cloud-based productivity suite to fulfill the requirements of office and home users. To download, install, and activate office.com/setup, connect with the Microsoft expert team and avail optimum benefits. Learn how to easily enter 25 digit alphanumeric product activation key code and easily activate it. Get assistance for Office 2007, Office 2010, Office 2013, Office 2016, Office 365, etc.

    ReplyDelete
  42. Norton.com/setup - Now Install Norton Setup at http://www.nortoncomsetup.fr/. Just Enter Norton Setup Product Key Here at Norton.com/setup and Get Started Now
    Norton.com/setup

    ReplyDelete
  43. MyDrive Connect - Now you may TomTom Update using TomTom MyDrive Connect in Australia. TomTom Update, Register, Manage, Sync etc using TomTom Software Here
    MyDrive Connect

    ReplyDelete
  44. Garmin.com/express - Now Install Garmin Express in order to do Garmin Update at Garmin.com/express. Update, Register, Manage, install or Sync Garmin Express
    Garmin.com/express

    ReplyDelete
  45. Best Buy Geek Squad Help 123 is a 24/7 helpline available to protect and repair your systems from technical problems. Contact Geek Squad experts for immediate assistance.

    ReplyDelete
  46. Get great assistance on Geek Squad Webroot Antivirus software & get your issues resolved anytime. reach for these experts anytime you need their help & get affective help.

    ReplyDelete
  47. An ongoing Microsoft declaration gives some understanding of how the organization plans the arrival of new Office 365 ProPlus highlights. Microsoft utilizes the same "channels" lingo for MS Office 365 ProPlus includes refreshes as it does with Windows 10 highlight refreshes. Nonetheless, the extension and conveyance plan contrasts a bit on the Office 365 ProPlus side. More details available on office.com/setup .
    Office.com/Setup |
    www.Office.com/Setup |
    webroot geek squad

    ReplyDelete


  48. mcafee.com/activate registered trademarks, company names, product names and brand names are the property of their respective owners, and mcafee.com/activate disclaims any ownership in such third-party marks. The use of any third party trademarks, logos, or brand names is for informational purposes only, and does not imply an endorsement by mfmcafee.com or vice versa or that such trademark owner has authorized mfmcafee.com to promote its products or services.


    office.com/setup is an independent support and service provider for the most secure remote technical services for all Office products. Our independent support services offer an instant support for all software related errors in the devices, laptops, desktops and peripherals. We have no link or affiliation with any of the brand or third-party company as we independently offer support service for all the product errors you face while using the Office. If your product is under warranty, then you may also avail our support services for free from manufacturer’s official website office.com/setup.

    mcafee.com/activate is an independent support and service provider for the most secure remote technical services for all norton products. Our independent support services offer an instant support for all software related errors in the devices, laptops, desktops and peripherals. We have no link or affiliation with any of the brand or third-party company as we independently offer support service for all the product errors you face while using the norton. If your product is under warranty, then you may also avail our support services for free from manufacturer’s official website norton.com/setup.

    ReplyDelete
  49. office.com/setup - Microsoft Office setup is a complete package of productivity suite open for professional, educational, and personal use. www.office.com/setup is visited once you have bought your Office Setup Product office.com/setup is where you enter your product information to setup office.
    suddenlink email | brighthouse email | xfinity customer service | brighthouse email login | brighthouse webmail

    ReplyDelete
  50. Epson is mainly famous for its printers all over the world. Millions of people across the globe printing their documents by Epson printer. But you need technical help to avoid and resolve printing problems. You can contact Epson Support Phone Number to avail help from certified experts.

    ReplyDelete
  51. This is really informative article. I appreciate the in-depth knowledge I needed. Thanks a lot for sharing. Office.com/Setup

    ReplyDelete
  52. Norton.com/setup Enter your product key online. Manage your security across multiple devices, Norton Setup Antivirus is a form of application that the user downloads using the aim to protect their apparatus in their machine.

    Norton.com/setup | Norton.com/setup

    ReplyDelete
  53. Thank you so much for this Post and all the best for your future. You are really a talented person I have ever seen. I am satisfied with the arrangement of your post.

    HP Printer Assistant

    ReplyDelete
  54. Thanks for sharing such great information with us. If you are Looking for the easy steps to download www.webroot.com/safe antivirus? Find them all here and protect your device by activating this antivirus.

    avast customer service
    webroot.com/safe
    webroot geek squad
    webroot geek squad download
    brother printer support

    ReplyDelete
  55. Thank you so much for this Post and all the best for your future. You are really a talented person I have ever seen. I am satisfied with the arrangement of your post.

    Brother printer support

    ReplyDelete
  56. This is very helpful and interested post. I am looking forward to reading more of your posts. Thanks for sharing this amazing post with us.
    Office.com/Setup

    ReplyDelete
  57. The experts of Myassignmenthelp Australia are not only proficient in writing the analysis assignments, but they are also comfortable with other genres of assignment writing.
    Students always come to us and ask to do my assignment for me. For all sorts of assignment help services, our experts are capable enough to do your assignment online. Students will always get plagiarism-free papers from this service. All these utilities are available at reasonable prices.
    Essayassignmenthelp.com.au also provides urgent assignment help service to the students through which the students can get assignments within a few hours from placement of the order. This service is especially useful when the students are required to get their essays done immediately.

    ReplyDelete
  58. The professionals at My Assignment Help are thorough experts in their disciplines and have gone through similar academic and admission-related hurdles that the students are going through now. Hence, they are always in an advantageous position to understand the customized needs of each unique student. Know more about our custom assignment writing services.
    Students come to us to find the best essay maker online. If we talk about the reflective essay, it is usually required in a portfolio for admission in higher education. Its introduction gives a general overview of the goals pursued by the student and to what extent the goals have been delivered.
    The body of essay should reflect on how the student has grown in the course of learning and imbibing pedagogy. Hire the professional writing services now.

    ReplyDelete
  59. Thanks for posting this valuable information, really like the way you used to describe. Hope I'll get such posts in future too.

    norton.com/setup | office.com/setup | mcafee.com/activate |office.com/setup

    ReplyDelete
  60. This is very insightful post. I appreciate the in-depth knowledge you have. I am satisfied with your post. Thanks for sharing.
    Office.com/Setup

    ReplyDelete
  61. Norton products are easy to set up and activate to your computer. Once you have downloaded and installed it to your computer, half of the job is done. Now you only need to click on the installed product, and by entering your product key that you can redeem at the time of purchase, the job will be done. To activate the Norton.com/setup, you need to open it again and enter the product key and click to activate it. In case if you face any problem, you can take the assistance of experts by contacting at Norton setup where you will be getting the easiest and prominent solutions.
    For More:-
    Norton.com/setup

    ReplyDelete
  62. Thank you so much for this Post and all the best for your future. You are really a talented person I have ever seen. I am satisfied with the arrangement of your post.

    Mcafee.com/activate

    ReplyDelete
  63. I must say that this is a great post.Really I am impressed from this post.
    office.com/setup
    office.com/setup

    ReplyDelete
  64. There are large numbers of the printer brands available in the market but the Epson is one of the leading preferable brands. The company provides the printer and scanner with advanced features. The paper jam is the major problem that the users are confronting while using the device. If you are having problem with paper jam any other error with your Epson printer, then place a call at Epson Printer Support Number to contact expert tech-geeks.

    ReplyDelete
  65. Canon printer might appear offline when it cannot communicate to with the PC. To fix this problem, check that your printer should not be in offline mode. If everything is fine but your Canon printer offline Windows 10 then contact certified experts to fix the problem immediately.

    ReplyDelete
  66. office.com/setup - For Downloading, Installing and activating the Office product key, visit www.office.com/setup and Get Started by now Office setup.
    office.com/setup
    http://officecomcomoffice.com/

    ReplyDelete
  67. Great information you have shared through this post. Keep sharing good information with us. Thanks for sharing.
    Office.com/Setup

    ReplyDelete

  68. I am thankful for the article post.Looking forward to visit more.
    office.com/setup
    office.com/setup

    ReplyDelete
  69. Get in touch with the experts at HP Support & avail great technical help in just one call. Reach for HP Support experts anytime to get resolution at whatever point you think you require them the most.

    ReplyDelete
  70. It gives us immense pleasure to introduce ourself and our travel hub one of the premier travel hubs in the state of Jammu & Kashmir.
    kashmir tour packages

    ReplyDelete
  71. A pilgrimage is a very important part of your life. Vaishno Devi visit is one such pilgrimage that every Hindu desires to do in their lifetime.
    vaishno devi helicopter booking

    ReplyDelete
  72. Get one stop arrangement with Norton antivirus security programming and secure your gadgets from different sorts of malware and digital assaults. It is effectively accessible in the market or over the web. A client can without much of a stretch buy it from the retail location or direct from the official site norton.com/setup. Get help for downloading, introducing, re-introducing and actuation Norton antivirus. For enacting the product, you have to enter 25 digit alpha-numeric item initiation key code and effectively actuate the product into your gadget.

    ReplyDelete
  73. McAfee is one of the main American antivirus security programming organization which secure gadgets from various malware, infections, and other digital dangers. McAfee cases to be one of the biggest security organization innovation organization which gives exhaustive security insurance to the clients and utilized by a large number of clients the nation over. For downloading, introducing, and initiating mcafee.com/activate and enter 25 digit alpha-numeric item actuation key code.

    ReplyDelete
  74. Jobs divine is one of the best job consultancy in thrissur. We provide all types of jobs in thrissur. We do have many job vacancies in thrissur. Sign up now for a free account and get thrissur jobs instantly. The candidates who in search of good career in Thrissur can apply and get easily their dream job through jobs divine

    job consultancy in thrissur

    thrissur jobs

    top job placement agency in thrissur

    job vacancies at thrissur

    jobs at thrissur

    thrissur job vacancies

    ReplyDelete
  75. Wonderful blog! I found it while browsing on Yahoo News
    office.com/setup

    ReplyDelete
  76. Thank you so much for this Post and all the best for your future. You are really a talented person I have ever seen. I am satisfied with the arrangement of your post.

    Mcafee.com/activate

    ReplyDelete
  77. Hello, I'm Smith Warner. If you are facing issues with mcafee, norton and office product. then you can visit my website.

    Mcafee.com/activate
    Mcafee activate
    norton.com/setup
    office.com/setup
    office.com/setup

    ReplyDelete
  78. Wonderful blog! I found it while browsing on Yahoo News

    Regards= office.com/setup

    ReplyDelete
  79. Thank you so much for sharing these amazing tips. I must say you are an incredible writer, I love the way that you describe the things. Please keep sharing
    Office.com/setup

    ReplyDelete
  80. Get Started with Office For Download, Install and activate the Office product .
    office.com/setup |
    office setup

    ReplyDelete
  81. Talking of good antivirus, we recommend the best antivirus in the market that is Norton Antivirus. norton.com/setup

    ReplyDelete
  82. Engineers who wish to migrate to Australia must submit a Competency Demonstration Report and the Engineers Australia must approve it. Thus, engineering students look forward to getting Cdr Australia which assists them to get a flawless CDR. This reduces the chances of rejection by the EA.
    Most students and experienced civil engineers are today looking forward to migrating to Australia as the job scope is better and bigger with a high pay scale. Therefore, getting CDR help is the only scope to gain entry into the country.
    The CDR for Engineers Australia must be impressive and abide by the ANZSCO code and guidelines. It should also showcase the skills of the applicants as a suitable civil engineer to work according to the Australian rules and regulations.
    The service providers who assist the students with CDR have experienced cdr report writers. These writers know the requirements of a CDR and do it accordingly.

    ReplyDelete
  83. Always we are working to give best and updated assignment service always. Don't search more for the research paper topic you can get it's best service at studentsassignmenthelp.com. World's best experts are continue giving amazing service and can finish all your demands. Our experts are online to offer you amazing services and they are offering 24x7 online facility.

    ReplyDelete
  84. You can call this HP printer support helpline number 24 hours a day, 7 days a week on. It will get you straight through to the correct team. If for any reason you experience any problems with this HP printer toll free number.

    Hp printer customer support | Brother printer support | Dell printer support

    ReplyDelete
  85. Brother Printer Support is a team of well experienced experts available round the clock to resolve your printer problems. If you face any problem with your device like cable problem, cartage problem, paper jamming and others then reach the experts at Brother Printer Support Number and get instant help.

    ReplyDelete
  86. HP Printer Support is active helpline that is available round the clock to resolve Hp printer problems. If you face any problem with your printer like device is not working properly, paper jamming issue, cable wire problem and others then reach experts of HP Printer Support Number and get instant help.

    ReplyDelete
  87. Dell Printer Support is a team of well experienced experts who takes care of your dell device problems. If face any problem with your device like your device is crashed, device is not working properly, paper jamming or others then contact at Dell Support and get instant help.

    ReplyDelete
  88. QuickBooks Support Phone Number is available round the clock to fix all errors. Connect with experts at QuickBooks Support Phone Number with 24/7 availability to resolve all errors associated with QuickBooks Support. Get best guidance and support for error free software.

    https://www.bloglovin.com/@chris81043/quickbooks-support-phone-number
    http://bit.ly/2R65OYV.
    http://bit.do/eUKRT
    https://www.google.se/url?sa=t&source=web&cd=1&ved=0CBcQFjAA&url=https://quickbooks-customer-service.org/quickbooks-support-phone-number/

    ReplyDelete
  89. webroot secureanywhere antivirus download is just a one click go at webroot safe , get all 3 ways to install , renew or upgrade webroot secureanywhere.Webroot Geek Squad Download Reinstall on Mac Device For Mac users, follow the below steps Visit Webroot Geek Squad from your Mac device's browser; It will download a file named "wsamac.dmg" Once the download is completed, double-click on the wsamac.dmg file and follow the on-screen guidance


    www.webroot.com/safe
    webroot.com/safe
    www.webroot.com/login

    ReplyDelete
  90. Acer Support is a team of well experienced experts who takes care of your Acer devices. If you are facing any problem with your Acer device like your device is crashed, device is not working properly or any other problem then contact toll free number of Acer Tech Support and get instant help.

    ReplyDelete
  91. Canon Printer Support is a team of experts who takes care of your canon device issue. If face any problem with your device like your device is crashed , device is not working properly or others then contact Canon Support and get instant help.

    ReplyDelete
  92. AOL Tech Support Phone Number is a customer care helpline that is offered by one of world's best mail service provider. The experts at this toll-free helpline renders all your forget password, password recovery and other related issues. Reach them anytime of day or night at AOL Tech Support whenever you need their help.

    ReplyDelete
  93. Students assignment help experts are continue to offer the amazing service to every student who wants. So all the student of programming and demanding to finish assignment quickly then why you are wasting time our team is ready to give programming assignment help service. Students can get this service by simply come to the studentsassignmenthelp.com.

    ReplyDelete
  94. Wonderful blog! I found it while browsing on Yahoo News

    Regards= office.com/setup

    ReplyDelete
  95. Epson Printer Support is available whole day and night to resolve your printer problems. If you face any problem with your epson printer device like device is not working properly, cable problem, cartage problem, blank screen and others then contact at Epson Support and resolve your issue in no time.

    ReplyDelete
  96. To get started Office 2019, 2016 and office 365 download or installation you must need valid 25 character product key & visit-

    office.com/setup |
    www.office.com/setup |
    office.com/setup

    ReplyDelete
  97. Wonderful blog! I found it while browsing on Yahoo News

    Regards= office.com/setup

    ReplyDelete

  98. Hello guys i am john wick and i provide securty services regarding all types of antivirus . Avast antivirus is one of them So any query related to avast visit our official website .

    My.Avast.Com

    ReplyDelete
  99. AOL mail application provides various features and benefits along with enhanced security. This software has various merits but if not installed in a proper way, it may not give satisfactory performance. So we are always available to provide support for AOL Gold Download. Our experts are trained and well experienced to give satisfactory solutions.

    ReplyDelete
  100. Microsoft workplace setup includes a sort of workplace product with varied options that you simply will get from workplace.com/setup. If you would like to use workplace setup like Outlook, OneDrive, & Skype, then you certainly want a Microsoft Account. Everything that you simply want for your home, school, and office, then transfer it from office.com/setup
    Office.com/Setup |
    norton.com/setup |
    mcafee.com/activate |
    mcafee activate

    ReplyDelete
  101. mcafee.com/activate - Follow the steps to activate mcafee, download and install at www.mcafee.com/activate. Find 25-digit alphanumeric product key on registered email or backside of the retail card to mcafee activate.

    norton.com/setup - Follow the steps to set up Norton, download and install at www.norton.com/setup. Find 25-digit alphanumeric product key on registered email or backside of the retail card to activate norton setup.

    office.com/setup - Enter Key office setup, after purchasing MS Office from visit www.office.com/setup, sign in to your Microsoft account then enter product key for Office Install.

    ReplyDelete
  102. Get Certified Online Help for Roadrunner Email

    Roadrunner email is a famous email service used all over the world to send/receive emails. There may be a possibility of having technical issue with the roadrunner email like login issue, forget password and much more. You can get help by contacting Roadrunner Support Phone Number to resolve all the issues related to Roadrunner email.

    ReplyDelete
  103. Learn how to download, install, activate, and uninstall Microsoft Office Setup on different devices and operating systems such as Mac and Windows. Activate your 25 character alphanumeric product key for Office 365, Office 2016, Office 2013, Office 2010, or Office 2007 at Office.com/setup.
    Visit- office.com/setup

    ReplyDelete
  104. You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Norton.com/setup |
    Mcafee.com/activate |
    Norton.com/setup |
    Mcafee.com/activate |
    Norton.com/setup

    ReplyDelete
  105. AVG Support helps the troubled customers who are having issues with there antivirus software. Also the experts working at the AVG Support Number are accessible 24/7 to rescue every user.

    ReplyDelete
  106. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avastlogin

    ReplyDelete
  107. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avastlogin

    ReplyDelete
  108. If you are looking for Accounting Assignment Help, complete my assignment is here to help you. It provides solutions anytime when you want.

    ReplyDelete
  109. Thank you for sharing this. The blog is very informative. We also provide affordable Accounting Assignment Help in uk.

    ReplyDelete
  110. HP printers support are popular across the globe. If you encounter any issue or error, dial the HP printer toll-free phone number and get instant help from the HP printer customer support service that is available 24/7.

    ReplyDelete
  111. Are you looking for printer support? Getting frustrated with your printer related issues? Don't get panic now. We're here to provide you best technical support for printers. Call us anytime on our toll-free number: USA/Canada: +1-888-480-0288 & UK: +44-800-041-8324. Our team provide instant solution for your issues such as: Brother Printer Offline, Brother Printer Offline Mac, Brother Printer Won't Connect To Wi-Fi and many more. You can visit our website for more information.

    ReplyDelete
  112. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avastlogin

    ReplyDelete
  113. Need Amazon Alexa Helpline? We help you resolve issues like Alexa slow to respond, Alexa won’t connect to Wi-Fi, Alexa having trouble understanding, Alexa offline, Echo Dot offline, Echo registration failure error, Alexa ring light issue, etc… our expert technician can offer you a lifetime experience for the best technician advice. Call Amazon Alexa Customer Service today to get the amazing helpline by our experts. Alexa Helpline Number at US/Canada Toll-Free: +1 888-949-4666 and UK Toll-Free: +44 800-041-8324 available 24/7. You can also visit Alexa Helpline anytime.

    ReplyDelete
  114. You are very good at that.
    คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete
  115. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avastlogin

    ReplyDelete
  116. Download, install, and activate, Norton and enter 25 digits alpha-numeric code for secure login. and Download Office 2007, Office 2010, Office 2013, Office 2016, and office 365 and many other.

    norton.com/setup | norton.com/setup | office.com/setup | office.com/setup | office.com/setup

    ReplyDelete
  117. We offer research papers writing help that focuses on satisfying the academic needs of students at any time they need help and also affordable custom essay writing help services.

    ReplyDelete
  118. This post is not just informative but impressive also. If you're looking for my assignment help, programming assignment help services. You can email us at info@goassignmenthelp.com.au or Phone Number: +61-283-206-023

    ReplyDelete
  119. We have a team of professional assignment writers who have experience in providing law assignment help, our work is 100% plagiarism free.

    ReplyDelete
  120. office 365 setup will help the users in activating, downloading and installing Microsoft Office on their PC . It will provide you the Step-by-Step guide for Microsoft office. If the subscription has expired, learn how to renew it. Get the complete guide to download, install and activate MS office setup.
    office.com/setup |
    Office.com/myaccount |
    Office 365 Setup

    ReplyDelete
  121. Thanks For share such a nice platform for know our horror scope. If any one want to resolve their problems talk to astrologer for free.

    ReplyDelete
  122. If you are using obsolete data in your Garmin GPS device then you may face problem in tracking the right way for your journey. So, it is advised to you that get latest Garmin GPS Update to navigate correctly. If you are having any problem in updating the data then contact certified expert immediately.

    ReplyDelete
  123. MyAssignmentHelp being one of the most active assignment help websites has a pool of over 4500+ assignment experts from Australia, UK and US.
    If you Google with the keywords ‘need thesis help’ you will see a long list of competing writing service providers making a lot of promises. What you will also see is MyAssignmenthelp.com standing in the first place. And do you know why? Because it has been almost a decade we are in the writing industry serving the students and who knows the students’ requirements better than us. Know the reasons why students choose only us to get thesis help

    ReplyDelete
  124. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avastlogin
    office.com/setup

    ReplyDelete
  125. If you want to fix kindle won't connect to wifi or any other kindle issue then dial kindle customer service number USA/Canada +1 888-949-4666 & UK +44 800-041-8324. Our expert technicians are available 24/7 at your service so call us any time or visit us at kindle help guides.

    ReplyDelete
  126. If you need help to resolve Canon printer is offline mac issue then contact our expert team. Call us on toll-free canon printer helpline number US/CA: +1 888-480-0288, UK: +44 800-041-8324 or visit us at canon printer offline. We are available 24/7 at your service so call us any time to fix canon printer issues.

    ReplyDelete
  127. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.What is lvdt

    ReplyDelete
  128. Thanks for sharing this kind of information. It’s really nice and useful for me. If any engineering student has to prepare a CDR report and submit that report to the Engineers Australia. Then you have don’t go here and there you have simply visit needcdrreport and also contact our expert team and get CDR Help. We have provided high-quality CDR report.

    ReplyDelete
  129. Here I am sharing a very useful resource for students looking for assignment help. ProAssignmentHelp providing all sort of assignment writing in various subjects like as : Electrical engineering assignment help , electronics assignment help , MATLAB assignment help , management assignment help , etc.

    ReplyDelete
  130. Everybody gets so excited about the awesome use of Quantum Physics in Endgame, but it is totally different when they have to write a long research paper on this topic. For those hard times, our physics homework help is there for you. Tophomeworkhelper.com is here to make Physics fun for you.

    ReplyDelete
  131. From device repair to set up and support you can count on experts available at Staples Tech Support for convenient and steadfast solutions. Obtain the best in-store services by connecting with Staples near me. Take Staples advantage by connecting with experts for world class solutions and services.

    ReplyDelete
  132. My Assignment Services is no. 1 when it comes to providing assignment help in Australia. We have a team of expert writers who are qualified in every level of econometrics, from basic to advanced econometrics. Some of these tutors are still working in this field, so they are well aware of the latest trends and are able to describe them well. Each assignment that we deliver, undergoes proper editing & proofreading and plagiarism check, so that there are no errors. My Assignment Services will always be there standing tall 24x7. We provide help for a wide range of assignments and styles like, dissertation, report writing, essays, case study, etc. My Assignment Services is ready for Australian students rely on our resume writing services Australia services due to our amazing features like, plagiarism free content, after sales service, error free papers, etc. You don’t have to involve much, as we want you to relax and let our experts do the work for you. My Assignment Services has been serving students from past 11 years now and we have gained good name among students due to our excellent quality of work. My Assignment Services not only help with healthcare, but also other subjects like higher business management, economics, finance, computer science, biology, etc. If you also have any unfinished management assignments, then we are here to provide you the best management assignment help. Our quality is unbeatable and we provide plagiarism free content. No need to worry now, as you can avail our project management assignment help services with amazing discounts and cashbacks. There is no need to panic, as we are here to help. So, order now.

    ReplyDelete
  133. Download, install, and activate, Norton and enter 25 digits alpha-numeric code for secure login. and Download mcafee global threat intelligence (gti) is a comprehensive cloud-based threat intelligence service .

    norton.com/setup | mcafee.com/activate | mcafee.com/activate

    ReplyDelete
  134. MyAssignmentHelp being one of the most active assignment help websites has a pool of over 4500+ assignment experts from Australia, UK and US.
    This is where MyAssignmenthelp.com can save the day by providing the prospective students of Malaya with timely dissertation assistance in a budget-friendly way. We have some of the best in class dissertation support personnel that can help you with the task and make things hassle-free in the long run.

    ReplyDelete
  135. There are lots of virus threats are available on the internet like virus and malware. Millions of customers across the globe using Norton antivirus to protect their PC from threats. Go to norton.com/setup to get the easy setup process of Norton antivirus and secure your PC.

    ReplyDelete
  136. We are the best writing company providing Legitimate Essay Writing Services as our company also ensures the client receives quality Cheap Term Papers.

    ReplyDelete
  137. Thanks for sharing useful information to getting Assignment Help in correct way. If you need any information for hiring an academic writer, place your call via greatassignmenthelp and talk to expert for resolving your concerns.
    Assignment Help Online
    Online Assignment Help
    Assignment Help Online Services
    Assignment Helper
    Assignment Assistance
    Assignment Help Experts
    Online Assignment Help Services

    ReplyDelete
  138. Brother Printer UK is the team of best technical support experts who can provide you the best technical support services for printers such as brother printer offline , Brother Printer Offline Mac, Brother Printer Won't Connect to Wi-Fi and etc. Call us USA/Canada: +1-888-480-0288 & UK: +44-800-041-8324.

    ReplyDelete
  139. Thanks for updating the post! Your post has shared all essential information of Assignment Help very clearly. Students should opt for online assignment writing services in order to save their time. For more details regarding the best academic writing, connect with customer care services of assignmenthelpshop
    Assignment Help Online
    Online Assignment Help
    Assignment Help Online Service
    Assignment Helper
    Assignment Assistance
    Assignment Help Experts
    Online Assignment Help Services

    ReplyDelete
  140. http //ij.start.canon for mac is a software configuration canon printer for macOS X

    ReplyDelete
  141. Thanks for letting us comment on your awesome post
    office.com/setup

    ReplyDelete
  142. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avast login
    office.com/setup
    Rand McNally Update

    ReplyDelete
  143. Are you facing any type of problems or errors in your Dell Printer? Visit our website and connect with our experts they will assist you with the solution related to your Dell printer.
    Dell Printer Support

    ReplyDelete
  144. Thus students seek help assignments online so that they can score better grades and also learn from the experts who provide assignment writing services online.

    ReplyDelete
  145. There could be many reasons for receiving message Brother Printer Is Offline. Follow the easy steps in the article to resolve Brother Printer Offline issues.

    ReplyDelete
  146. Why is my Epson Printer Offline? Follow the easy steps in page or connect with experts at Epson Printer Support to find the accurate solution.

    ReplyDelete
  147. It is amazing post, i am really impressed of your post. Its really useful. Thank you for sharing this article.
    avast login
    office.com/setup
    Rand McNally Update

    ReplyDelete
  148. Use Epson Email Print, Remote Print, or Scan to Cloud by downloading Epson Connect Printer Setup utility. Print and scan from any corner of the world wirelessly.

    ReplyDelete

  149. Norton Setup and Instal Process – For both PC and mobile users. Highly popular among the PC

    users, the Norton antivirus software has been eliminating malware, viruses and other kinds of

    online and offline threats from affecting the performance of a computer for years.

    Norton.com/setup , being a security solution providing company has created
    office.com/setup ..
    norton.com/setup
    norton.com/nu16
    office.com/setup

    ReplyDelete
  150. Bitdefender login offers a wide range of products making it a truly versatile security solution. While some are dedicated to specific operating systems. Yet others are designed for cross-platform compatibility.
    Bitdefender Login

    ReplyDelete
  151. My.avast.com can be purchased through various channels. You can get it through either online or offline store.

    my.avast.com

    TomTom Home - Download TomTom MyDrive Connect Software in order to do TomTom Update. Update Your Navigation Device and Enjoy TomTom GPS Here.

    TomTom Home

    ReplyDelete
  152. You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Sony Printer Support
    Kodak Printer Support
    Samsung Printer Support

    ReplyDelete
  153. mail.aol.com - AOL Mail Login at login.aol.com and Manage Your Aol Mail Account. You may do Aol Mail Sign in, Create an AOL Account, Reset Your AOL Password.

    mail.aol.com

    Webroot.com/safe - Just Visit the Website and Enter the 20 Digits Webroot Safe Keycode to Download Webroot SecureAnywhere and Get it Installed Here.

    Webroot.com/safe

    ReplyDelete
  154. trend micro login offers incorporated, modern and holistic solutions for ensure against consistently developing on the web dangers like infections, malware, spyware, ransomware, phishing, trojans and so on.

    ReplyDelete
  155. TomTom Update - Now Update Your TomTom Navigation Devices using TomTom MyDrive Connect and Manage the Device using TomTom Home Management Tool. update tomtom | how to refresh tomtom | Tomtom home

    ReplyDelete
  156. Using Avast Login you can perform following exercises: check what is the status of all of your licenses/enrollments and restore them, see all of your devices, incorporate more devices, control Avast Anti Theft or drop auto-energizing participation. My.Avast.com | Avast Account | My Avast Account

    ReplyDelete
  157. Avast Antivirus is exceptional web security application made by my.avast.com All comprehensive advanced risks and malware ambushes has risen recognizably. We all in all expected to make sure with the security of our devices and Avast performs amazingly. Thusly, Avast Antivirus never stops. Avast login | My Avast Account | My Avast

    ReplyDelete
  158. trend micro login offers incorporated, modern and holistic solutions for ensure against consistently developing on the web dangers like infections, malware, spyware, ransomware, phishing, trojans and so on.

    ReplyDelete
  159. Brother Printer UK is the team of best technical support experts who can provide you online support for printer such as Brother Printer Offline issue,brother printer offline mac issue, brother printer won't connect to Wi-Fi and etc. Call us anytime on our toll-free number for instant support: USA/Canada: +1-888-480-0288 & UK: +44-800-041-8324.

    ReplyDelete
  160. webroot.com/safe is excellent for Windows PC/Laptop, MAC, Android devices. You can use webroot key code which is on your retail card and get webroot to install easily on your devices. For the Installation of the product , go to URL : webroot.com/safe and then put the code...

    ReplyDelete