The Agilent 34401A has become the worldwide de-facto standard of excellence in the 6.5 digit DMM market – with unequaled measurement performance and reliability. It has also been out on the market for more than 15 years. Today Agilent announced the new Truevolt series of digital multimeters that include the 34461A and 34460A. The 34461A is designed to be a drop in replacement of the 34401A. The 34460A offers a basic entry point into the 6 ½ digit class of Agilent DMMs.
With Agilent's Truevolt DMMs
- Display DMM results in ways you never have before
- Easily display, save and document your measurement results
- Measure with unquestioned Truevolt confidence
- Worry about the quality of your design, not the quality of your measurement
- Move to the next generation 34401A with 100% assurance
- Everything you depend on with the 34401A and more
The very first thing you are likely to notice with these new
DMMs is the large, bright, high-resolution color graphical display. This display enables many of the new features
you will enjoy: graphical views (histogram, trend chart, bar meter) of your
measurement results, easy navigation through measurement set-up options, or preferences
that can be configured and pulled up automatically at the next instrument
start-up.
I personally feel that the new histogram and trendchart/datalogging display modes will save me a bunch of time. Coupled with the in-box statistics, I can now view and analyze my data without doing any programming and visually see my measurements. The trendchart mode is like a crude digitizer, I've been able to check if my signal is drifting or if there is a glitch in the signal. Histogram mode has allowed me to determine if my signals are noisy or if they have a Gaussian distribution. With the large 10,000 reading memory, I can export the data on the fly if I need to do any further analysis on the PC.
Through the display and intuitive,
menu-driven interface, you can easily save and document all your DMM
results. First, pick your I/O of choice
– USB, LAN or GPIB, or easily access your data from the front-panel USB
connection. You can also easily access
the files on your DMM using drag-and-drop file access to transfer files from
your DMM to your PC directly – no software required!
Finally, we have new DMM Connectivity Utility
software that allows you to control, capture and view your DMM’s data on your
PC or mobile device. This free utility from Agilent will not only support the new Truevolt DMMs, but many of the older Agilent DMMs including the 34401A, 34410A, 34411A and the new 34450A. It has the ability to log data, visualize it, and export to Word/Excel/Matlab. In addition, you can simultaneously control, analyze, and measure with multiple DMMs.
What is Truevolt confidence?
Truevolt is all about the trust, confidence, long-term guarantee and
stability of Agilent DMM measurements.
It is comprised of three elements.
The first is our patented analog to digital converter architecture. Only Agilent DMMs offer direct digital
sampling for AC measurements – this ultimately allows for crest factors up to
10 without additional error terms (other 6½ digit DMMs will likely have a 5:1
crest factor rating). The second element
is around noise – eliminating all the extraneous noise from the instrument and environment
that can affect your measurements.
Agilent’s Truevolt DMMs have the lowest injected noise and input
bias current of all 6½ digit DMMs.
Finally, Truevolt is derived, compliant and guaranteed
specifications according to ISO/IEC 17025 methodology, as well as new safety
and regulatory standards. These have
changed a lot in the past 20 years. The
new Truevolt family is the first DMM to be compliant with the latest industry
safety standards that require even more rigorous abuse testing and safety
margins that will go in effect in late 2013.
Agilent’s specifications are not just numbers on a piece of paper. Using ISO 17025 methodology for documenting
and communicating the performance of our DMMs means the specifications are
valid for a whole variety of environmental conditions – shake, shock,
vibration, EMI/RFI, temperature, humidity. Numbers may look the same on a piece
of paper as you compare different DMM solutions, but Truevolt and Agilent DMMs
will show a vast performance difference in the level of conformance and
repeatability of the instrument.
Now, move to the next generation 34401A with 100%
assurance. The 34461A was designed
intentionally, by many of the same engineers that designed the 34401A, to be the
34401A replacement. The 34401A is used
in thousands of test systems all over the world and being a drop-in replacement
is critical. With the Truevolt family
and the 34401A, Agilent is the original designer and manufacturer. We have our
own source code as reference so that we can migrate that into the design
systems for the software development of the Truevolt family. While much of the
34401A syntax is documented, there are other firmware paths that are accepted that
are not documented, that only the Agilent design team knows. That is all carried forward and maintained in
the Truevolt program code syntax execution.
Only Agilent can provide this advantage in a 34401A replacement – it is
not an emulation mode, it is native and intrinsic to the design.
Here is a video highlighting many of the feature of the Truevolt DMMs. A nice easter egg from the video shows a picture of the development team. It shows a few younger faces but a lot of veteran engineers that have been around the block. It highlights the maturity and dedication that Agilent has in the company. These DMMs should reflect the quality that HP/Agilent has shown throughout the years.
http://khairyayman.inube.com/
ReplyDeletehttp://emc-mee.jigsy.com/
شركة نقل عفش الرياض,شركة نقل عفش بجدة,شركة نقل عفش بالمدينة المنورة,شركة نقل عفش بالدمام
شركة نقل عفش بالرياض
شركة نقل اثاث بجدة
شركة نقل عفش بالمدينة المنورة
شركة نقل عفش بالدمام
easteldmam
ReplyDeleteeast-eldmam
شركة نقل عفش بالدمام
شركة نقل عفش
شركة نقل عفش
http://khairyayman.eklablog.com/
ReplyDeleteشركة نقل عفش بالمدينة المنورة
شركة نقل عفش بجدة
شركة نقل عفش بالرياض
شركة نقل عفش بالدمام
شركة نقل عفش بمكة
Flawless and amazing online journal!
ReplyDeleteeidas timestamp
PLC Training in Chennai | PLC Training Institute in Chennai | PLC Training Center in Chennai | PLC SCADA Training in Chennai | PLC SCADA DCS Training in Chennai | Best PLC Training in Chennai | Best PLC Training Institute in Chennai | PLC Training Centre in Chennai | PLC Training Chennai | PLC Training Institute Chennai | PLC Training in Chennai | PLC Training Institute in Chennai | PLC Training Center in Chennai | PLC SCADA Training in Chennai | PLC SCADA DCS Training in Chennai | Best PLC Training in Chennai | Best PLC Training Institute in Chennai | PLC Training Centre in Chennai | PLC SCADA Training in Chennai | Automation Training Institute in Chennai | PLC Training in Kerala
ReplyDeleteEmbedded Training in Chennai | Best Embedded Training in Chennai | Embedded System Training in Chennai | Embedded System Training Institute in Chennai | Best Embedded System Training Institute in Chennai | Embedded Course in Chennai | Embedded System Training Institutes in Chennai | Embedded System Training Center in Chennai | Best Embedded System Training in Chennai | Embedded Systems Training in Chennai | VLSI Training in Chennai | VLSI Training Institute in Chennai
ReplyDeleteVLSI Training in Chennai | Best VLSI Training in Chennai | VLSI Training Centres in Chennai | VLSI Courses in Chennai | VLSI Training Courses in Chennai | VLSI Training Institute in Chennai | VLSI Training Institutes in Chennai | Best VLSI Training Institute in Chennai
ReplyDeleteWe help in setting up and Installing Microsoft Office on your computer. We provide Technical Support and other services to you. We help you with great work and other details. We are here to help you. We help you with Microsoft Office and Office installation. We help you with Great technical services at an affordable price.
ReplyDeleteRegards- www.office.com/setup
I would like to read more of your posts. Very nice post thank you for sharing.
ReplyDeleteusps tracking
I just want to tell you that I’m all new to blogging and site-building. I really loved your web page. Very likely I’m want to bookmark your site . You amazingly have remarkable posts. Thanks a bunch for sharing your blog.
ReplyDeleteRegards - www.office.com/setup
www.office.com/setup
www.office.com/setup
great post thanks for sharing this wonderful post
ReplyDeletetutuapp apk
tutuapp latest version
tutuapp for ios
tutuapp alternative
tutuapp for mac
tutuapp download
tutuapp for iphone
tutu helper
tutuapp
tutuapp for android
tutuapp web
tutuapp for blackberry
tutuapp for pc
tutuapp mod apk
tutuapp windows
tutu helper free
best tutuapp alternative
tutuapp apk download
tutuapp for pc
tutuapp for ios
tutuapp for ios 11
tutuapp for android
tutuapp alternative
tutuapp vip
tutu helper
tutu helper vip
tutuapp for blackberry