Sunday, March 3, 2013

Agilent's New RTSA Capability on its PXA Signal Analyzers

In this post I wanted to share the new real-time spectrum analysis (RTSA) feature that Agilent added to its PXA line of high performance signal analyzers. The RTSA feature gives the signal analyzer the ability to continuously capture spectra without any dead time between acquisitions. The PXA's maximum capture rate is 3.57us so that means it has a probability of intercept of 100% for signals with a duration of 3.57us or more. This feature is incredibly useful when trying to analyze intermittent or dynamic signals such as those used in radar and electronic warfare applications.

Let me give a quick explanation of what "dead time" means when referring to instruments like scopes, counters, and signal analyzers. When one of the example instruments makes a measurement or acquisition it then displays the results and prepares to make another measurement. The time in between two consecutive measurements (sometimes referred to as re-arm time) is dead time because no measurement is being made. Often, especially in the case of scopes, the dead time is longer then the measurement or acquisition time so any changes that the signal goes through during the dead time is not captured or measured by the instrument. When an instrument such as a signal analyzer has continuous or gap-free measurement capability it has no dead time time between acquisitions it simply continuously acquires data at its set sample or rate.

With the addition of the RTSA capability the PXA also added some advanced display capabilities to show the continuously captured data in a useful easy to interpret way to users. This includes a display persistence setting, mask testing, a histogram display, and a spectra versus time display. Below is an example of a frequency hopping radar signal displayed using the persistence and mask testing capability.



Besides the new RTSA option capability the PXA signal analyzer line includes a number of industry leading specs and features including:
  • –157 dBm at 10 GHz average noise floor which ensures low level signals do not get lost in the "grass"
  • 160-MHz real-time bandwidth for looking at wide-band modulated signals
  • up to 75 dB spurious-free dynamic range to see small signals in the presence of large ones
If you have any questions from this post feel free to email me and if you have anything to add use the comments section below.

Update (1/30/14) - Agilent RTSA recorder and analyzer application released:
Agilent has released the new RTSA spectrum recorder and analyzer application (available as Agilent RTSA option RTR) that allows you to directly record spectrum signal data on the RTSA signal analyzer itself, and then immediately play back the recording to look for signal anomalies. The option includes the application example (delivered as a MATLAB App), modifiable source code, and a MATLAB software license to execute and modify it. You can learn more about using this RTSA application and the option’s contents in my Agilent RTSA recorder blog entry.


For more information on the new RTSA feature on the PXA click here





37 comments:

  1. Download Airshou ipa & install it on your iPhone/iPad without JailBreaking.
    Airshou ipa

    ReplyDelete
  2. Download tutuapp latest version for android and ios devices to install paid apps and games for free. Click on the below link to download directly.
    tutuapp ios

    ReplyDelete

  3. download m4ufree




    Just download this app 3ds emulator for free apps.

    ReplyDelete
  4. Root Checker apk is a small and simple application checks Root access. For more click here
    root checker apk

    ReplyDelete
  5. Lucky patcher is an one stop solution for Android to block ads, remove license verification, remove app permissions. Download Lucky patcher no root apk now
    lucky patcher tanpa root

    ReplyDelete
  6. Here you can get the Complete Details about Airshou For Android.
    Airshou android

    ReplyDelete
  7. MovieBox allows downloading and watching movies in your smartphones for free. For more click here
    MovieBox

    ReplyDelete
  8. From test cricket to one-day internationals to T20 and now to it’s the turn of T10 cricket. With time cricket has encountered a decrease in its arrangement. The amusement has turned out to be more glittery in the previous one decade T10 Cricket League Live Streaming
    T10 Cricket League 2017 Live Streaming

    ReplyDelete
  9. Indian Super League season is the fourth season of the Indian Super League, the football league, since its establishment isl live streaming
    big bash Live Streaming

    ReplyDelete
  10. India Post Speedpost Tracking Page. Today: Sat, 18 Nov 2017. Your Consignment No: Click here to get current tracking status for your Speedpost Speed Post Tracking
    Speed Post Tracking

    ReplyDelete
  11. Download Your Favourite Free Ringtones from Myxer App: Are you looking for the most effective and superior windows phone app? myxer
    vshare
    tutuapp
    myxer

    ReplyDelete
  12. I just want to tell you that I’m all new to blogging and site-building. I really loved your web page. Very likely I’m want to bookmark your site . You amazingly have remarkable posts. Thanks a bunch for sharing your blog.
    Regards - www.office.com/setup
    www.office.com/setup
    www.office.com/setup

    ReplyDelete
  13. Here is a good Weblog You might Come across Fascinating that we Encourage You
    เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสล็อตออนไลน์ได้ที่นี่ >>> Golden slot
    ร่วมลงทุนสมัครเอเย่น Gclubกับทีมงานของเราได้เลย

    ReplyDelete
  14. Nice Post. Thanks for sharing this post. Apart from this, I am Johny Sins from Plumbers In Oregon to provide the plumbers in your area.

    ReplyDelete
  15. Our college research paper services is meant to transform the academic profile of any student from a downward trend to an upward trend in their grades.

    ReplyDelete
  16. TreasureBox is operated by a group of young, passionate, and ambitious people that are working diligently towards the same goal - make your every dollar count, as we believe you deserve something better.
    Check out the best
    rabbit hutch nz
    bed frames nz
    cheap outdoor furniture nz

    ReplyDelete
  17. I like to know about more and more things here..
    You did a very good job here.. Find some valuable things here..
    DJMAZA | VIP Marathi

    ReplyDelete
  18. Thanks for sharing such great information with us. Your Post is very helpful and information is reliable for new readers. Keep Thanks again for sharing such a useful post.
    Management Homework Help

    ReplyDelete