Monday, September 24, 2012

Simulating Power Supply Noise

Designs ranging from transceiver chips for smart phones to radar assemblies for fighter jets require power supply noise immunity testing, which is often referred to as power supply rejection ratio (PSRR) testing. Characterizing the design’s ability to reject or attenuate supply noise is critical because the noise can manifest itself as bit errors in the case of transceiver chips and inaccurate target data in the case of radar assemblies. In this post, we will discuss the challenges involved in simulating power supply noise signals for PSRR testing and look at two economical methods for doing it.

Challenges in simulating power supply noise
When you test PSRR, one challenge is modulating a quantitative noise signal onto a DC power supply level. This task is difficult because the power supply inputs typically present extremely low input impedance to any AC signal because of the high input parallel capacitance. While high-performance power supplies do have built-in arbitrary waveform capability, the output bandwidth of power supply waveforms is typically limited to less than 30 KHz. This limitation only allows you to simulate low frequency noise sources, such as power line ripple. It falls well short of the more critical noise source frequency ranges, such as power supply switching noise which ranges from 50 KHz to greater than 20 MHz.

To put the first challenge in perspective, let’s consider an example transceiver chip for a smart phone. The power supply input most likely has a parallel 1-uF bypass ceramic capacitor as well as a large 10-uF electrolytic capacitor to serve as an energy reservoir for the sharp transmit transients. That means a 1-MHz sinewave modulated onto the power supply level of the RF power amplifier would, in theory, only see a load of less than 20 mOhms. In practice, the equivalent series resistance (ESR), equivalent series inductance (ESL), and other parasitic impedances boosts the load impedance up to more than 50 mOhms, but that still presents low input impedance to any AC signal content.

Let's look at two solutions for simulating power supply noise that use (for the most part) general-purpose test equipment and simple components that you can find around the office or lab.

The op amp/MOSFET solution (OMS)
The OMS solution can be seen in the below figure. The solution requires two power supplies, a function/arbitrary waveform generator (FG/AWG), an op amp, and a high-power N-type MOSFET. In Figure 1, C1, C2, and the resistance value labeled “Load” make up a circuit representation of the device under test’s power supply input.


The OMS solution uses the MOSFET as a variable resistor between the power supply and the DUT (load). By varying the MOSFET’s drain to source resistance we can modulate the power supply's DC level with the desired noise signal. The op amp is used to maintain the desired voltage level at the DUT. With the op amp's inverting input connected to the same node as the input to the load, the op amp will drive the MOSFET's gate such that the amplitude level at its inverting input is the same as the amplitude at its non-inverting input.

The FG/AWG’s output creates the amplitude level and noise signal at the DUT's input. The power supply output voltage should be set comfortably higher than the desired amplitude plus any added noise signal amplitude to ensure the MOSFET stays properly biased. This OMS circuit allows you to accurately generate noise signals with bandwidths up to about 500 KHz. The bandwidth can vary depending on the DUT's input impedance and how well the OMS circuit was constructed. For best results, keep wiring and leads as short as possible to prevent oscillations.

As an example, the OMS circuit was implemented using an Agilent 33521A function/arbitrary waveform generator, N6762A power supply, E3630A dual-output power supply (to power the op amp), an IRFP150N N-type MOSFET, and an NE5534A op amp. The below scope capture shows the example OMS implementation generating a 200-mVpp 500-KHz sine wave onto a 5-VDC level. The same DUT load shown in the above diagram was used for this example, the 100-uF capacitor is electrolytic and the 1-uF capacitor is ceramic.


When you implement the OMS, you will need to use a high-performance power supply because you need a supply with a fast transient response and a stable output to ensure the supply can handle the rapidly varying load levels caused by the noise signal. Also, in the OMS the DC level value is limited to the max voltage of the FG/AWG, which today is typically 10 V. To overcome this limitation, you could add a voltage amplifier between the op amp and the FG/AWG.

Amplified modulation solution (AMS)
The AMS does not have the voltage or bandwidth limitations that the OMS has, but it does have a higher price tag. The AMS is shown in the below figure. The AMS consists of a power supply, FG/AWG or signal generator, wide-band or RF power amp and coupling capacitor section.


The FG/AWG and RF amp are used to modulate the DC level from the power supply with the desired noise signal. The coupling capacitor section blocks the DC level from the RF amp's input and provides a low-impedance path for the AC output of the power amp. The power amplifier is needed to boost the noise signal power to deal with the low impedance to AC that the DUT's input presents. You'll want to make the coupling capacitor section's impedance as low as possible, so you may want to use multiple capacitor values and types in parallel to reduce the effects of ESR and ESL. The exact circuit setup, the DUT's true input impedance, and the bandwidth of the noise signal will all determine how many watts the RF amp should be. A good place to start is 50 W, and you can go up from there. Note that the RF amp's output impedance should be as low as possible, which is typically going to be 50 ohms. With the DUT's impedance being so low, the RF amp will see a large amount of reflected power at its input, so when you choose an RF amplifier, be sure to select one that can handle a short-circuit condition.

As an example, the AMS circuit was implemented using an Agilent 33521A function/arbitrary waveform generator, an N6762A power supply, an E&I 1040L RF power amplifier, and 10-uF and 0.1-uF capacitors in parallel (for the coupling capacitor section). A 1040L RF amp provided up to 400 W of output power, which was more than necessary, but I used what was available to me in the lab. Using the same load used in the OMS example, the AMS was used to create a single tone noise signal. The below scope capture shows a 1-Vpp 5-MHz sinewave was modulated onto a 10-VDC level.


Test and measurement power supplies typically have a high capacitance value at their output. In the AMS, the power supply is in parallel with the load in regards to the RF amp’s output. That means the noise signal actually has two low-impedance paths to take, the load and the power supply output. It is hard to know the power supply’s AC power handling characteristic across its input capacitance since it is not specified by the power supply manufacturer, so you may want to contact the manufacturer to avoid costly damage.

One safety precaution you can take is adding blocking impedance between the power supply output and the coupling capacitor section. The blocking impedance can either be an inductor or a resistor. Its purpose is to protect the power supply from being damaged by the noise signal by adding higher series impedance before the power supply output. The inductor is ideal because it acts like a short to the DCV from the power supply, but presents high impedance to the AC noise signal. However, the inductor can cause large oscillations on the DC level if the DUT has a very dynamic current.

Using a resistor avoids the oscillations problem. Be sure to use the power supply’s sense leads to regulate the output voltage at the load to compensate for the voltage drop across the resistor. Also be sure to use a low-value resistor no higher than 1 Ohm. This is to ensure a low voltage drop across the resistor so you do not damage the sense lead circuit on the power supply.

Conclusion
PSRR testing is required on a wide range of devices today from smart phone chips to electronic assemblies for aircraft. Testing PSRR includes generating high-frequency noise signals on power supply levels. This task is challenging due to the high capacitance present at most power supply inputs. In this article we looked at two low-cost solutions for modulating noise signals on power supply levels. If you have any questions on the post send me an email and if you have anything to add use the "Comments" section below.

17 comments:

  1. Replies
    1. good article,Jotrin Electronics is electronic components distributor

      Delete
  2. Hello! Good article!I tried to make the same scheme with this model of power supply http://hardware.nl/power-supply/dell/td570.html but it was unsuccesful( Tell me please, does these tips appropriate for everyhthing?

    ReplyDelete
  3. If you set out to make me think today; mission accomplished! I really like your writing style and how you express your ideas. Thank you. electronic components distributor

    ReplyDelete
  4. https://issuu.com/emc-mee/docs/______-____________-__________-____ شركات نقل العفش بالدمام
    https://issuu.com/emc-mee/docs/______-______-________________1_.do نقل عفش بالدمام
    https://issuu.com/emc-mee/docs/______________________________.docx نقل اثاث بالدمام
    https://issuu.com/emc-mee/docs/________-______-______-_____________5eee6b62b0c947 شركة نقل عفش بالمدينة المنورة
    https://issuu.com/emc-mee/docs/___________________________________ شركة تنظيف خزانات بجدة

    ReplyDelete
  5. https://issuu.com/emc-mee/docs/________-______-______-________.doc شركة نقل عفش بجدة
    https://issuu.com/emc-mee/docs/________-______-______-____________ شركة نقل عفش بالرياض
    https://issuu.com/emc-mee/docs/____________________________________76c983dc869693 شركة تنظيف بالطائف
    https://issuu.com/emc-mee/docs/____________________________________be97b233ba8cdb شركة تنظيف خزانات بالمدينة المنورة
    https://issuu.com/emc-mee/

    ReplyDelete
  6. This comment has been removed by the author.

    ReplyDelete
  7. You may be interested in this site, if you ever asked yourself a question "who do I pay to do college homework"

    ReplyDelete
  8. A study conducted on the market of high voltage power electronics has shown a possibility of a boom in them in the near future. Leading companies have started showing interest in production of high voltage power electronics and have already started doing R&D to improve technologies.attuatori pneumatici

    ReplyDelete
  9. شركة نقل اثاث بمكة شركة نقل اثاث بمكة
    شركة نقل اثاث بمكة شركة نقل اثاث بمكة
    شركة نقل اثاث بجدة شركة نقل اثاث بجدة
    شركة نقل اثاث بمكة شركة نقل اثاث بمكة
    شركة نقل اثاث بجدة شركة نقل اثاث بجدة
    شركة نقل اثاث بجدة شركة نقل اثاث بجدة
    شركة نقل اثاث بمكة شركة نقل اثاث بمكة

    ReplyDelete
  10. Great site! You making an astounding showing with regards to. I truly lik it.
    https://allpowersolution.com/used-mwm-generators/

    ReplyDelete
  11. This comment has been removed by the author.

    ReplyDelete
  12. I didn't have any idea on this kind of information on Simulating Power Supply Noise, something that was very new to me until I came across this post. It could be great if you could keep on sharing. If you realize that the most reliable and relevant paraphrasing service is what you need, you can count on us. We do deliver the most credible and relevant services.

    ReplyDelete
  13. SEO Friendly team digital marketing services Illinois are tailored to the unique needs of each audience and brand objective, ensuring improved sales growth a profit. You can top rank website marketing for specialized marketing consulting services that include: SMO, PPC, Email Marketing, website design, SEO, Typing work, content writing marketing etc. We offer complete packages of efficient digital marketing services New York that adapt to fit your company needs. Click hers to see how we can help you(Related keyword for this services:- top Digital Marketing Services in Illinois, best online marketing company Connecticut, faster Internet marketing agency Palos Heights, businesses promotion firm Kewanee, marketing solutions provide advertisers Winnetka, Lincolnwood, business promotion Markham, effectively digital company Centralia, experience agency Pflugerville, digital advertising organization Rowlett, San Marcos)

    Visit us for more info- Contact Writing Services in Pennsylvania
    Typing Work Services in Pennsylvania
    Digital marketing services in Georgia
    SEO Services in Georgia
    PPC Services in Georgia
    SMO services in Georgia
    Web design services in Georgia
    Contact Writing Services in Georgia
    Typing Work Services in Georgia
    Digital marketing services in North Carolina

    ReplyDelete
  14. SEO is a critical component of internet marketing. At SEO friendly team we use a combination of the latest onsite and offsite strategies to produce top results. There are a variety of SEO services Illinois which offer for ranking issues and website traffic. Depending on your goal and needs one or a combination of the below for this services may be right for your website. SEO services in Illinois at a affordable prices. Contact us today. (SFT provider of this services:- SFT provider of this services Top SEO Services Company in Illinois, Affordable SEO services Connecticut, SEO Packages in Palos Heights, search engine optimization Services Kewanee, Create a traffic on website in Winnetka, Increase website ranking Lincolnwood, Experienced SEO services provider Markham, Best Leading SEO agency Jewett City, Multilingual and International SEO Danielson, Google update Groton, First page of search engine in Derby, White hat, Off page, On page)

    Visit us for more info- SEO Services in North Carolina
    PPC Services in North Carolina
    SMO services in North Carolina
    Web design services in North Carolina
    Lead Generate services in Georgia
    Email Marketing Services in Georgia
    web development Services in Georgia
    Contact Writing Services in North Carolina
    Typing Work Services in North Carolina
    Lead Generate services in North Carolina

    ReplyDelete