Monday, August 27, 2012

What is Trueform Waveform Generation Technology?

Trueform waveform generation technology is an exclusive technology found in Agilent’s new 33500B Series waveform generators. Trueform technology provides sizable advantages over direct digital synthesis (DDS), the incumbent technology used in waveform generators. These advantages include significantly lower waveform jitter for less test uncertainty and a true representation of the selected waveform, not an approximation. In this blog post, we will look at Trueform and compare it to DDS.

Conceptually, the simplest way to generate a waveform is to store its points in memory and then read those points out one after another and clock them into a DAC. After the last point has been read, the generator jumps back to the first point again to begin the next cycle. This is sometimes called “point per clock” (PPC) generation. Even though this method seems like the most intuitive way to create waveforms, it has two big drawbacks. First, to change the waveform’s frequency or sample rate, the clock frequency has to change, and making a good low-noise variable-frequency clock adds cost and complexity to the instrument. Second, since the stepwise output of the DAC is undesirable in most applications, complex analog filtering is needed to smooth the steps out. Because of its complexity and cost, this technology is used mainly in high-end waveform generators.

DDS uses a fixed-frequency clock and a simpler filtering scheme, so it’s less expensive than the PPC method. In DDS, a phase accumulator adds an increment to its output in every clock cycle, and the accumulator’s output represents the phase of the waveform. The output frequency is proportional to the increment, so it’s easy to change frequency even though the clock frequency is fixed. The output of the accumulator is converted from phase data into amplitude data typically by passing it through some type of look-up table. The phase accumulator design allows DDS to use a fixed clock, but still execute waveforms at a perceived faster sample rate than the clock. So with DDS, not every individual point is being expressed in the resulting output waveform. In other words, DDS is not using every point in waveform memory, but it creates a really good approximation. But since it is an approximation, waveform data is changed in some way. DDS can skip and/or repeat aspects of the waveform in an unpredictable way. In best-case scenarios, this leads to added jitter; in worst-case scenarios, severe distortion can result. Small features in the waveform can be partly or completely skipped over.

Agilent’s new Trueform technology represents the next leap in waveform generation technology. Trueform provides the best of both worlds. It gives you a predictable low-noise waveform with no skipped waveform points like PPC technology, but at the price point of DDS technology. Trueform works by employing a exclusive virtual variable clock with advanced filtering techniques that track the sample rate of the waveform. In the following sections, we will look at some of the waveform generation advantages Trueform provides over DDS.

Improved signal quality
One of the key advantages Trueform provides over DDS is better overall signal quality. One of the best ways to show this is by doing a jitter measurement comparison with DDS. The following figures show a jitter measurement made on a 10-MHz pulse signal using a high-performance oscilloscope. The scope view is zoomed in on the rising edge of the pulse signal with the persistence setting of the scope turned on. The histogram function of the scope is used to measure the period jitter of the signals. The standard deviation measurement in each figure is circled in red and represents the signal’s RMS jitter. The Trueform pulse signal jitter measurement is shown in the below figure and the DDS pulse signal jitter measurement is shown in the next figure.

Trueform signal with < 5ps of RMS jitter
DDS signal with > 50ps of RMS jitter
In the above figures both the amplitude and time scales for the scope are the same. The Trueform pulse waveform has more than 10 times less jitter compared to the DDS pulse waveform. The substantially lower jitter that Trueform offers over DDS means less uncertainty in your tests. This is especially true when you consider edge-based timing applications like generating a clock signal, trigger signal or communication signal.

The waveform you create is the waveform you get
As we mentioned earlier, DDS uses a fixed clock and a phase accumulator so it cannot guarantee that every point or feature in a waveform will be played. The higher the frequency, the more gaps you will see in the output waveform compared to the ideal waveform. Trueform, on the other hand, plays every waveform point regardless of the set frequency or sample rate. This becomes critical when you are dealing with a waveform that may have a small detail that is critical to the test you are performing. As an example, we created an arbitrary waveform that consisted of a pulse with seven descending amplitude spikes on top of the pulse. The waveform was then loaded into a Trueform waveform generator and a DDS waveform generator. First the waveform was played at a 50-KHz frequency on each generator. The result was captured on a scope, shown in the below figure. The yellow trace is the Trueform waveform and the green trace is the DDS waveform.
Trueform on top in yellow and DDS in green

At 50 KHz, each generator was able to reproduce the waveform with seven spikes on top of the pulse. You can see that the Trueform spikes reached higher amplitude. In the below figure scope screen shot, the waveforms were played again, but this time at 100 KHz.

Trueform on top in yellow and DDS in green. Note that all the DDS spike points were skipped
At 100 KHz, the Trueform waveform generator played all seven spikes and the DDS generator did not play any of the spikes. In the below figure scope screen shot, the waveforms were played again, but the frequency was doubled again to 200 KHz.

Trueform on top in yellow and DDS in green. Note that DDS only shows 3 of the seven spikes

At 200 KHz, once again, the Trueform waveform generator shows all seven spikes in the waveform. The DDS generator went from playing no spikes at 100 KHz to playing three spikes at 200 KHz. Notice that the three spikes played in the 200 KHz waveform do not match the correct time location of any of the seven spikes that are in the actual waveform points. These waveform examples demonstrate that when working with waveforms that have fine detail, DDS cannot be trusted.

Agilent’s Trueform technology offers a new alternative that blends the best of DDS and PPC architectures, giving you the benefits of both without the limitations of either. Trueform technology uses an exclusive digital sampling technique that delivers unmatched performance at the same low price you are accustomed to with DDS.


For more info on the 33500B series with Trueform technology click here






10 comments:

  1. every product has its merits and demerits. In essence, take product reviews with a pinch of salt

    ReplyDelete
  2. Your blog provided us with valuable information to work with. Each & every tips of your post are awesome. Thanks a lot for sharing. Keep blogging,
    Shortener

    ReplyDelete
  3. We Provide Our Customers With Latest and up-to-date Dumps Questions & Answers with 100% Exam Passing Guarantee. We Promise Exceptional Success in First Attempt. ADM-201 exam dump

    ReplyDelete
  4. The article you have shared here very good. This is really interesting information for me. Thanks for sharing!
    light novel

    ReplyDelete
  5. In the past few decades there has been a revolution in computing and communications, and all indications are that ada progress and use of information technology will continue at a rapid pace. Accompanying and supporting the dramatic increases in the power and use of new information technologies has been the declining cost of communications as a result of both technological improvements and increased competition. According to Moore's law the processing power of microchips is doubling every 18 months. These advances present many significant opportunities but also pose major challenges. Today, innovations in information technology are having wide-ranging effects across numerous domains of society, and policy makers are acting on issues involving economic productivity, intellectual property rights, privacy protection, and affordability of and access to information. Choices made now will have long lasting consequences, and attention must be paid to their social and economic impacts.

    ReplyDelete
  6. Throughout my years of movie watching and electronics sales, I have noticed one trend that I find kind of amusing, and might help explain how we *cough* "know" who the Nerds are... Spend Management Software Say what you will about Nerds, nerds and technology are almost interchangeable terms. Regardless of whatever else they are fans of, nerds LOVE their technology, and are often the first to embrace the newest technological advances.

    ReplyDelete