Monday, August 13, 2012

Testing DC to DC Converters with a Single Instrument

This post features two videos by a colleague of mine who presents a single instrument solution for testing DC to DC converters targeted for handheld or portable devices where power optimization is critical. Typically when testing a DC to DC converter you need a long list of test equipment including a power supply, eload, multi-channel scope or digitizer, current shunt or probe, and a waveform generator to vary the output of the power supply or eload. Agilent's N6705B DC Power Analyzer provides a single instrument solution. The N6705B is a modular power supply with up to four power outputs, voltage and current digitizers, and power waveform capabilities. There are over 30 power modules to choose from. The SMU modules shown in the video can source and sink power so one is connected to the input of the DC to DC converter and the other sits on the output as a load.

The first video provides an overview and example measurements for using the N6705B for testing DC to DC converters. The second video goes into more detail on a DC to DC converter efficiency measurement and shows an example.











15 comments:

  1. This was a good suggestion that you put up here...dude…..hope that it benefits all the ones who land up here. 
    Electrical Wholesalers

    ReplyDelete
  2. Hi,


    Very usable video about the how to testing DC to DC converters with a single instrument. The first video provides an overview and example measurements for using the N6705B for testing DC to DC converters and the second video is goes into more detail on a DC to DC converter efficiency.

    Redundant Power Supply

    ReplyDelete
  3. Find the great deals on 5v Converter in Test Equipment DC Power Supplies in Test Equipment DC Power Supplies. This circuit offers a variety of Buck DC to DC converters. Because as circuit increase voltage of 5 volts to 12 volts. Shop with confidence.

    ReplyDelete
  4. With the growing retail industry garment and fabric exports from India has improved to a vast extent, impacting the large evolution of Textile testing industry. xenon test chamber

    ReplyDelete
  5. This was a good suggestion that you put up here...dude…..hope that it benefits all the ones who land up here.


    goldenslot casino
    บาคาร่าออนไลน์
    gclub casino


    ReplyDelete
  6. The crockmeter is a logical gear made for material production lines to unbending level metal where the test example can held immovably. Therefore scraping finger rubs against it.

    For the most part the stage is settled on the base of the logical hardware which lies in a flat plane and it scraping texture grabs shading is lost when the test example amid rubbing. The arm is moved by a physically worked wrench and interfacing line...If want more more please check it out: http://www.testextextile.com/product/electronic-crockmeter-tf411

    ReplyDelete
  7. I found your this post while searching for information about blog-related research ... It's a good post .. keep posting and updating information. best-film-to-digital-converters

    ReplyDelete
  8. A testing machine to test the wear resistance of all kinds of structures including fabrics, leather, and rubber, paper, metals, paints, plated surfaces, coated materials, glass, etc. Taber abraser online

    ReplyDelete
  9. 90minup ข่าวกีฬา ฟุตบอล ผลบอล วิเคราะห์บอล พรีเมียร์ลีก ฟุตบอลไทย
    ข่าวกีฬา
    ตารางคะแนน
    ฟุตบอลไทย
    ไฮไลท์ฟุตบอล
    ดูบอลออนไลน์
    ผลบอลสด
    90minup

    ReplyDelete