Tuesday, August 21, 2012

Agilent Announces a New Family of Waveform Generators with Exclusive Trueform Technology

In this blog post we will look at Agilent's new family of waveform generators, the 33500B series. The new family is made up of 8 models that offer bandwidths from 20 to 30 MHz and offer one or two channels. The 33500B family features the exclusive Trueform waveform generation technology. Trueform technology plays every point in an waveform, unlike the incumbent direct digital synthesis (DDS) technology which only provides an approximation of a waveform (not every point is played). Also Trueform technology delivers waveforms with extremely low jitter typically around 4 ps of RMS jitter, which is more than 10x less jitter than a DDS generator. I will have more detailed info on Trueform in a future post. Here are some more 33500B series headlines:

  • Full bandwidth pulse and square waves
  • Sine waves with 5x lower harmonic distortion
  • IQ signal player option
  • Advanced modulation features such as sum modulation and channel to channel modulation
  • 16 bits of resolution with 1 mVpp to 10 Vpp amplitude
  • Noise function with variable bandwidth adjust and no repetition for over 50 years of continuous play
  • The ability to upload arbitrary waveforms and sequences without a remote connection


For the two channel version there is an IQ signal player option available. IQ signal waveforms can be played from the 33500B without the option, but the option adds an easy to use single user interface for setting up and controlling both channels at once. Also the option offers features such as channel skew adjust and balance control for adding non-ideal conditions to the signal to test the limits of your design. 

For an IQ example a 64 QAM baseband signal was created in software. It was then uploaded to and played by the 33522B waveform generator using the IQ signal player option. The resulting IQ baseband signal was captured by a high performance scope using vector signal analysis software, as shown in the below figure.


With Trueform technology the 33522B was able to deliver a 64 QAM baseband signal with only 0.3 % error vector magnitude! Notice too that the phase error is in milli-degrees and the magnitude error is in mV.

In my next post I will go into more detail on what Trueform technology is and do some comparison measurements with DDS. As always if you have any questions related to this post please feel free to email me and if you have something to add use the comments section below.

15 comments:

  1. If You are here to buy Electronics featured product deals, Electronics discounts, Electronics coupons and much more with great savings. Just visit the site dealaboo.com and get your best electonics item in a best possible low prices.

    ReplyDelete
  2. These types of machines always fascinated me. When I look at one, I feel like I am looking at a sci-fi spaceship control panel. Waveform generators are an amazing development in the science field. I can't believe how far we have come. Thank you for sharing this comprehensive post on waveform generators. I feel more confident discussing this topic now that I have read this post.

    ReplyDelete
  3. I have you bookmarked your site to check out the new stuff you post.
    Used Lab Equipment For Sale

    ReplyDelete
  4. DO you need an academic paper asap? You can order here! Just take a minute and tell us what you need!

    ReplyDelete
  5. Geek squad support provides the best troubleshooting solutions regarding your technical issues, if you need the best service for the hardware devices then we are here to give you the
    best services for your devices.Geek Squad tech support is a 24/7 helpline provider.

    ReplyDelete
  6. Geek Squad Tech Support provides the best technical help and guidance. Get in touch with extensively trained tech support team for all sort of queries and issues regarding your devices. You can contact Geek Squad round the clock according to your convenience.

    ReplyDelete
  7. the solutions to all the technical issues with all your electronic appliances at Geek Squad Tech Support. Avail wide no of services, on-site, and over the Internet via remote access and In-store, and also provides 24/7 telephone and emergency on-site support. Reach the experts at Geek Squad Tech Support for removing all technical glitches with your devices

    ReplyDelete
  8. Geek Squad Webroot being an antivirus software is very crucial in respect to today's time. The experts working behind the toll-free helpline of this antivirus are great at resolving all your virus and malware issues. Call Geek Squad now for expert help, anytime.

    ReplyDelete