Monday, April 30, 2012

ECU Fuel Injection Loop Calibration

In this post we will look at how a precision DC source or an SMU can be used to calibrate the fuel injection loop in a automobile or other engine powered equipment. The fuel injection flow to an engine is controlled by a solenoid that is adjusted either more open or more closed by a driver output from the engine control unit (ECU). Fuel injection control has always been an important part or a vehicle design, but recently the precision it is tested to has become even more critical because it is closely tied to a vehicle's fuel efficiency. Tight control over fuel injection means at any given moment the engine is getting the right mixture of fuel and air to ensure maximum efficiency.

Below is a basic circuit diagram of a fuel injection control circuit. The inductor at the top represents the fuel injector solenoid. The amount of current flowing through the solenoid determines how open or closed it is, which in turn controls the flow of fuel to the engine. The amount of current flowing through the solenoid is controlled by the MOSFET, which is pulse width modulated by a control circuit from the ECU. The rate of the PWM is determined using the control signal from the accelerator and the output of the current sense circuit. The test we will look at is used to calibrate the control loop to the output of the current sense circuit at various current levels.


There are two ways the calibration factors could be determined. The first is by isolating the circuit from  Vbatt and the solenoid and just forcing a known amount of current through the circuit using a current source. Below is a an example of how the test was done by an engineer at an automotive company using the Agilent N6762A Precision DC Source.

The DC source is used in constant current mode so it acts like a current source. Precision DC sources have high accuracy current sourcing capabilities which is ideal for this application. To perform the test iterate the output current value of the DC source through the full range of the solenoid, open to closed. Then use the measured values to build a look up table or create a curve fitted equation. Instead of a precision DC source a source measure unit (SMU) could also be used. An SMU will typically deliver slightly better current accuracy, but at a higher price. 

The second way to calibrate the fuel injection control is by operating the whole circuit in normal operation with Vbat and the solenoid or at least something that simulates Vbatt and the solenoid. You then use an SMU as a zero ohm shunt in series with the current path. To use an SMU as a zero ohm shunt you simply insert it into the circuit set it for 0V so its output is regulated at 0V. That way there is no voltage dropped across it so it doesn't effect the circuit. The circuit current from Vbatt will then flow through the SMU (it is sinking the current). The SMU would then accurately measure the current flowing through it. Using an SMU as a zero ohm shunt is much better then using a real current shunt, because a real shunt will add a non-zero amount of resistance to the current path. For this type of setup you want to make sure the SMU has a fast transient response spec to ensure proper regulation at 0 volts in the face of dynamic current changes.

In this post we looked at two ways to calibrate the fuel injection control loop in an automobile using either a precision DC source or an SMU. If you have any questions on this post please email me and if you have any insights to add just use the "Comments" section below.





18 comments:

  1. Proper calibration is the essential process which can help you in derive of quality product.This post is quite informative as it has helped people to gain information in this context.
    Calibracion Santo Domingo

    ReplyDelete
  2. This is a good place to find information on test & measurement products. Here you describe a very good article on measurement product.




    Test Tags

    ReplyDelete
  3. The information shared in this post is quite effective as it has given a clear idea that proper calibration services is essential for the accurate functioning of a fuel injection loop. I think you have a deep knowledge in the field of calibration.

    ReplyDelete
  4. Great post!,Thanks for sharing this useful information.We will wait for your next article soonly.Very nice and valuable post! Thanks for sharing this. raspberry ketones for weight loss

    ReplyDelete
  5. Truck scale scale repair los angeles services including scale calibration, scale repair, weight calibration and preventative maintenance.

    ReplyDelete
  6. Crucial engine parts including fuel injectors at the lowest prices from the UK's number one supplier of car parts. try this web-site

    ReplyDelete
  7. Cool stuff you have and you keep overhaul every one of us
    You have done a amazing job with you website
    www.isfcalibration.org

    ReplyDelete
  8. نقل عفش بالرياض
    شركات نقل العفش بالرياض
    http://www.pearltrees.com/khairyayman/
    http://www.pearltrees.com/khairyayman/item193051311

    ReplyDelete
  9. It was wondering if I could use this write-up on my other website, I will link it back to your website though.Great Thanks.
    you could try here

    ReplyDelete
  10. Thanks for taking the time to discuss this, I feel strongly that love and read more on this topic. If possible, such as gain knowledge, would you mind updating your blog with additional information? It is very useful for me.
    try here

    ReplyDelete
  11. Your article for Engine Control Units is very nice. I find it very useful & it is covering every detailed aspects about Engine Control Units. Get more information about ECU from here.

    ReplyDelete
  12. คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete
  13. Are you looking to hire a credible and high-quality Custom Descriptive Essay Writing Service? Is preparing a unique research paper proving to be a daunting and strenuous task? Hiring the best Buy Descriptive Essay Online is the best choice a prudent student can make to ensure they relish better grades and quality work from professional authors.

    ReplyDelete