Monday, March 5, 2012

Building an Electronic Load with General Purpose Test Equipment

In this post we will look at how to build a low cost DC electronic load (eload) using general purpose test equipment found on every engineer's test bench and some simple circuit components. The eload we build can be used for testing and validating power supplies and other power sources.

The below figure shows the eload circuit. The only piece missing from the figure is the measurement instrument(s) which are used to measure the voltage across the eload and the current through the eload. To measure voltage or current a scope, DMM, or digitizer could be used. The measurement points for the voltage and current measurements are mark in the figure as "Vmeas" and "Imeas" respectively.

Circuit Diagram of the eload
 The following list explains each part of the eload circuit and its function:

  • The device under test (DUT) is the DC power source we are testing with our eload circuit.
  • The N-Type MOSFET serves as a variable resistor and is the main component making up the load that the DUT is connected to. Its resistance is dynamically controlled by the op amp. The MOSFET will be dissipating the majority of the DUT's output power so power handling is a critical spec when choosing a MOSFET. You also want to ensure the MOSFET has proper heat sinking.
  • R1 serves as a sense resistor. The voltage drop across R1 is used by the op amp to control the current output of the DUT. R1 is also used to measure the output current from the DUT.
  • The op amp dynamically controls the resistance of the eload. It works by taking a control voltage level into its non-inverting input. It will then drive the gate of the MOSFET so that the same voltage value is at its inverting input, which is connected to the R1 node. This means the op amp allows us to control the voltage drop across R1 regardless if there is a change in the DUT's output. Since we know the value of R1 we can control the amount of current through R1. Since R1 is in series with the load, this means we can control the output current of the DUT.
  • The function / arbitrary waveform generator (FG / AWG) provides the control voltage to the op amp, which means it determines the output current of the DUT. The FG / AWG can be used as a simple DC bias to create a static output power from the DUT or a waveform could be used to create a dynamic load change (we look at an example of this later).
  • A basic bench top power supply can be used to power the op amp. You can use a bipolar supply to provide both the positive and negative supply voltages for the op amp.
  • To measure the voltage across the eload or the current through it a scope, DMM, or digitizer can be used. To measure both simultaneously you will need two channels. The voltage is measured from the drain of the MOSFET to ground. The current is measured by measuring the voltage drop across R1 and using the value of R1 and Ohm's Law to calculate current. The DMM is only good for static measurements. The scope or digitizer should be used when trying to capture dynamic voltage and current measurements.
Now that we know how the eload circuit works lets look at an example implementation of it measuring the transient response on a 10 V power supply. For this example we want to measure the supply's transient response time (within 3% of 10 V) to a load change from 0.5 A to 2.5 A. The following instruments and components were used for the implementation of the eload circuit:
  • 33521A function / arbitrary waveform generator
  • E3630A DC power supply
  • MSO7054A scope (4 analog channels)
  • NE5534A op amp. Chosen for high output bandwidth and low noise output.
  • IRFP150N power MOSFET. Chosen for its high power handling and low "on" resistance. Used with a metal heat sink.
  • 1 ohm 30 W power resistor
To create a sharp repeating load transient that ranged from 0.5 A to 2.5 A, the 33521A was setup to output a pulse signal that ranged from 0.5 V (0.5 V * 1 Ohm = 0.5 A) to 2.5 V (2.5 V * 1 Ohm = 2.5 A). Below is a screen capture from the scope showing the voltage across the eload (yellow) which is the power supply's output voltage and the voltage drop across the eload's sense resistor (green) which is the power supply's output current since the sense resistor is 1 Ohm. The blue trace is the pulsed output of the 33521A FG / AWG.


Notice from the green trace the load toggles between drawing 0.5 A and 2.5 A. This is equivalent to the eload toggling between 20 Ohms and 4 Ohms. Notice the positive and negative spikes on the yellow voltage trace, they are power supply transients caused by the sharp load changes, this is what we want to measure.

In the below figure, using the scope cursors, the power supply's transient response time was measured to within 3% of 10 V.


As you can see in the above figure the transient response time of the supply was < 1.4 us. We can also see the max deviation of the supply's voltage level due to the sudden load change, which is about 1.25 V or 12.5% of the nominal voltage level.

One thing you have to watch out for when building the eload circuit is oscillations. To prevent oscillations be sure to keep all wiring, connections, and traces as short as possible. Use a large ground plane and be careful to avoid ground loops. You can also add coupling capacitors as needed. 

In this post we looked at how to build a simple bench top DC electronic load for testing power supplies and other DC power sources. The eload design employs some general purpose test equipment and basic circuit components. The best part about the eload design that was presented in this post is it is essentially free since it uses common benchtop instruments and basic components that can be found in lab stock. If you have any questions on this post email me. If you have any comments or personal insights to add use the "Comments" section below.

82 comments:

  1. Thanks a ton for being my own mentor on this theme. I actually enjoyed your current article greatly and most of all liked the way in which you handled the aspect I regarded as controversial. You're always extremely kind towards readers like me

    Daniel Schmitt and Co.

    ReplyDelete
  2. You made some good points there. I did a search on the topic and found that most people will agree with you.
    National Power Supply Engines

    ReplyDelete
  3. Nice information, thanks towards the author. It can be incomprehensible to me now in general, the usefulness and significance has my head spinning. Thanks again and best of luck!
    National Power Supply Generators

    ReplyDelete
  4. A simple circuit, but with excellence thunder spark idea. Thanks for your Creation.

    ReplyDelete
  5. Oh!.. That was new learning... Do you know the new Fluke Multifunction Electrical Tester are out... It can be more helpful in such cases.. Thanks

    ReplyDelete
  6. Excellent post, I am searching this such as content on Internet for new information and learning whatever I can, and in doing so I sometimes leave comments on blogs. Thanks....
    Plastic Level Sensor

    ReplyDelete
  7. Nice and cheap way for testing and it’s also useful one.

    ReplyDelete
  8. It's not easy to build an electronic load with general, it takes a lot of experimentation before you figure out the right formula. The students from procustomwriting.com are currently doing the same project, it's a good thing they now have a basis on how to go about with it.

    ReplyDelete
  9. This is a great inspiring article.I am pretty much pleased with your good work.You put really very helpful information... Testing Machine

    ReplyDelete
  10. Building Maintenance Baton Rouge. We can work with owners and investors to develop a plan Building Maintenance Baton Rouge Facilities maintenance is a difficult challenge for homeowners and businesses both large and small in Louisiana.

    ReplyDelete
  11. at was a very interesting article. I’ve never really thought about how I write comments or the meaning behind them. I see so many rude and meaningless comments on sites like YouTube. People should put meaning behind their comments.

    bursting strength tester

    ReplyDelete
  12. You may want to check out this site, if you sometimes asking yourself a question "Who would do my homework for me"

    ReplyDelete
  13. Walmart, the world’s largest company by revenue, mostly accepts Discover,Amex (American Express) or Visa cards. Walmart offers two credit card options to its consumers – a store-only card and a MasterCard.

    walmart credit card login

    ReplyDelete
  14. Automatic induction and bursting system, can be connected with computer and printer, test curve, test result is easy to output and read. mullen bursting tester

    ReplyDelete
  15. Great blog.you put Good stuff.All the topics were explained briefly.so quickly understand for me.I am waiting for your next fantastic blog.Thanks for sharing.Any coures related details learn...

    software testing course in chennai

    ReplyDelete
  16. Thanks for a very interesting blog. What else may I get that kind of info written in such a perfect approach? I’ve a undertaking that I am simply now operating on, and I have been at the look out for such info. london scaffold hire

    ReplyDelete
  17. Thank you for your post. After hours of searching, this post is the only one, that I could find, that dealt with injecting a Function Generator signal, into an electronic load. I am, presently, building a DIY e-load and I want to add this feature.

    I am a hobbyist, with limited understanding. However, I note two things, about your schematic... One, the FG signal, which I think should be ac (meaning to have both positive and negative amplitude, from ground,) is only referenced to positive and ground, on the op amp. Won't this chop off the negative component, of the signal? Two, I see no conditioning of the FG signal. Shouldn't there be, at least, a voltage clamp/limiter? I have a thread going, about these very things, at http://www.eevblog.com/forum/projects/hacking-a-dynamic-electronic-load-circuit-to-use-an-external-function-generator/msg1819739/#msg1819739 I would greatly appreciate it, if you would join us, there.

    ReplyDelete
  18. Hi Thanks for the nice information its very useful to read your blog.
    Web Design Training

    ReplyDelete
  19. We provide a list for top asked PHP interview questions and answers to help you get success in your interview. Find out PHP technical interview question & answers for fresher’s and professionals.

    ReplyDelete
  20. Hey, Your post is very informative and helpful for us.
    In fact i am looking this type of article from some days.
    Thanks a lot to share this informative article....best regards.
    websphere training in hyderabad

    ReplyDelete
  21. This also gives the students some time to review them and ask for revisions, if needed. You can trust our academic ghostwriters completely to get best quality write-ups including case studies, research proposals, dissertations and Assignment Help Melbourne, and more.

    ReplyDelete
  22. Hello there. I found your web site by the use of Google at the same time as searching for a comparable subject, your site came up. It seems great. I have bookmarked it in my google bookmarks to come back then.

    Telugu Status Download
    Telugu Whatsapp Video Status
    WhatsApp Video Status in Telugu
    Telugu Status Video
    Telugu Status Video Songs Download
    Telugu Status Video Songs Download
    Malayalam Status Video Songs Download

    ReplyDelete
  23. Great post! You are sharing a lot of information and this is really useful. I'm glad that I came across your post. Thanks for sharing.

    WordPress Training in Chennai
    WordPress Course in Chennai
    Excel Training in Chennai
    IoT Training in Chennai

    ReplyDelete
  24. This post is a pool of information. The readers are quite impressed after reading this impressive post. This impressive post certainly encourages to choose Assignment Help Australia Services. You can email us at cs@Myassignmenthelpau.Com or Phone Number: +61-2-8005-8227

    ReplyDelete
  25. I think this is the best article today about the future technology. Thanks for taking your own time to discuss this topic, I feel happy about that curiosity has increased to learn more about this topic. Artificial Intelligence Training in Bangalore. Keep sharing your information regularly for my future reference.

    ReplyDelete
  26. Online Assignment help Australia being one of the most active Online Assignment help websites has a pool of over 4500+ experts by Assignment help Australia, UK and US. They are highly qualified and skilled professional writers who have vast experience in writing assignments, dissertations, essays, research papers, term papers etc. Each expert is chosen after rigorous testing and has to prove his academic credentials.

    ReplyDelete
  27. What is the best place to study artificial intelligence in Delhi NCR?
    The advantage of finding out in the associate institute in Delhi NCR additionally stems from the actual fact that even the most effective teaching employees from all across the country return here to show within the completely different schools. If you want to more details to contact us: #LoginForExcellence,#EmbeddedSystemsTraininginChennai, #EmbeddedSystemsTrainingInstituteinChennai,#TraininginVelachery,
    Python Training in Chennai

    ReplyDelete
  28. Thank you for your informative content. I really appreciate it. However, I would like to recommend every single student that is facing any kind of challenges in their academic assignment, about highly accurate Australian assignment help services that are being offered by Industry best assignment help provider My Assignment Help.

    I could recall an event where I once urgently needed professional assignment writing service to help me make a perfectly structured essay in 2 hours. This is when the best assignment help Australia services offered me a chance to avail their professional services and in a couple of days, I was rewarded with a huge round of applause for preparing the best assignment in front of the whole batch.

    ReplyDelete
  29. Please visit to the site My Assignment help writing service reviews. This site contains different type of the resume forms, structures and tips, and also helps to give best guidelines about all the resume writing. This is very good and clear one.

    ReplyDelete
  30. Well it’s good to find such a useful content on your website. You have nicely designed website. Like your website our website also help students in their assignment related issues. Students often feels issues in writing assignment, so to make students comfortable in assignment we help them to write their assignments. If ever you feel any problem in writing something you can visit our website.
    assignment help uk

    ReplyDelete
  31. please visit the students assignment help for online assignment help.We provide assignment help services in very cheap prices.

    ReplyDelete
  32. No doubt getting online assignment help is a good idea, but if you are suffering from such a thing, you must first try to overcome it. You must understand the causes that are prohibiting you from writing the papers.
    Survey has shown that Australian students are at the top of the list who suffers from this anxiety. So they look for Australian assignment help because the assignments must match the high academic standards of the universities.

    ReplyDelete
  33. I really happy found this website eventually. Really informative and inoperative! Thanks for the post and effort! Please keep sharing more such article. I've really like your blog and inspire me in many ways. Brother printer error ts-07

    ReplyDelete
  34. Outstanding article! I want people to know just how good this information is in your article. Your views are much like my own concerning this subject. I will visit daily your blog because I know. It may be very beneficial for me. Assignment Help

    ReplyDelete
  35. Thanks for this informative content. It’s really good. Actually, I want to share some thoughts and reviews about assignments help Australia and the popular brand for this service is SAMPLE ASSIGNMENT. Here, I am working as an Academic Expert. To look at our online academic assistants who provide reference assignment including Accounting, Management, Finance, IT, Economics, Computer Science, Nursing, Marketing; all Academic subjects to University Students all over the Australia or even worldwide, Here is a big online assignment help providers who help students to get HD grades according to assessment guidelines and instructions. Those who are searching for assignment help experts in Melbourne, Perth, Brisbane, Adelaide etc. get a touch with Sample Assignment - the No.1 Assignment provider. Any student really wants to buy an assignment at the cheapest price goes to our branded website and has a look and opts our amazing and informative services, you can avail of our convenient online assignment help and samples available on our website for free. You can download it if you want. Are you ready to get 100 out of 100 in your university assessment? We assign the best writer according to the subject for your academic problems and provide support in assignment writing services. Our Customer Care Executives are available 24*7 hours to assist you in the best possible manner. Phone calls and emails are the best methods used by online assignment help providers.

    ReplyDelete
  36. Get all seo top submission sites. Her all top sites provide the on-page or off page seo tools activities list and also discrible the seo tools which make your seo easier

    ReplyDelete
  37. Brother Printers frequently indicate technical hitches because of inward reasons. There are numerous reasons which can cause brother printer not printing .Call us now to get a reliable solution.

    ReplyDelete
  38. Are you demanding for Assignment Help? Turn towards LiveWebTutors and stay tension free. We have professional and experienced subject experts offering you the most favourable assignment help services and ensure quality solutions and delivery in time.
    Visit us@ Assignment Help

    ReplyDelete
  39. GotoDissertationHelp.co.uk is leading plagiarism free essay writing help in U.K. We provide customized dissertation help service. We are leading the market for more than a decade now and have acquired the name of being the best academic help service for our comprehensive services at pocket-friendly rates.
    dissertation writing services
    dissertation writing services
    custom dissertation writing services
    dissertation editing services online

    ReplyDelete
  40. Very good, I think I found the knowledge I needed. I will see and refer some information in your post. thank you
    office.com/setup

    ReplyDelete
  41. Excellent blog. Very interesting to read. I really love to read such a nice article. Thanks! keep rocking.
    norton.com/setup

    ReplyDelete
  42. Students can easily get the best Do My Assignment services from the well-qualified writers of StudentsAssignmentHelp.com. Whether you are studying in UK university or New Zealand university our experts will guide you adequately according to your asked university standards.

    ReplyDelete
  43. Trinetra is a Coffee table book project on jyotirlinga promoting ,story of jyotirlinga,indian heritage,indian culture,jyotirlinga,hinduism,sadhoowad,name of jyotirlinga,Mallika Empire in whole world

    ReplyDelete
  44. Assignment Help Shop doesn't make empty promises and has always achieved what we promised our clients by online management assignment help. If you need any academic consultation for any assignment type, our team of assignment help shop is available ready to cater to your needs any given moment.

    ReplyDelete
  45. Best team of masters and Ph.D. degree professionals that understand students requirement and complete all the task properly. We are working with team of native writers from the USA, Ireland, Australia, Singapore, UK, New Zealand, etc. Professional college assignments help online is available at StudentsAssignmentHelp.com.

    ReplyDelete
  46. Marsbahis giriş adresi değiştiğinde en hızlı ve doğru olarak öğrenmek ve marsbahis kullanıcı şikayetlerini okumak için takipte kalın. Marsbahis

    ReplyDelete
  47. Piaybet Üyelik ile; Piabet Giriş Adresi, Piabet Bonus ve Diğer Bilgileri Sitemizden İnceleyebilir, Diğer Ziyaretçilerimizin Yorumlarını Görebilirsiniz. Piabet

    ReplyDelete
  48. A programmable load, these AC or DC electronic loads can be used by power supply, battery, solar, wind, or other manufacturers who want to thoroughly test their power sources iTunes Login.

    ReplyDelete
  49. Professional college assignments help online is available at StudentsAssignmentHelp.com. Best team of masters and Ph.D. degree professionals that understand students requirement and finish all the task properly. We are keeps moving with team of native writers from the USA, Ireland, Australia, Singapore, UK, New Zealand, etc.

    ReplyDelete
  50. If you are facing any problem for write assignment. Don’t worry; we are here to resolve your query. We provide homework helper. Our essay helpers are well-versed with all the writing topics and deliver great writing for the students. Hire Now!

    ReplyDelete
  51. Great post! I am actually getting ready to across this information, is very helpful my friend. Also great blog here with all of the valuable information you have. Keep up the good work you are doing here. Fix Activation Error code 0xc0004f074

    ReplyDelete
  52. Güvenilir canlı bahis siteleri, online casino, casino oyna, bahis şirketleri, kaçak bahis ve kaçak iddaa, illegal bahis firmaları ile listemiz en iyilerle. Bahis siteleri

    Güvenilir Canlı kaçak bahis siteleri, iddaa siteleri, bahis şirketleri, bahis firmaları, illegal bahis, mobil casino siteleri ve canlı casino seçenekleriyle karşınızdayız. Güvenilir bahis siteleri

    ReplyDelete
  53. Slotbar casino sitesine güncel giriş adresi ve slotbar üyelik için sitemizi ziyaret edebilirsiniz. Slotbar

    2003 yılından beri piyasada olan ve sektörün en tecrübeli şirketlerinden birisi olarak dikkat çeken Kingbetting, Curacao oyun komisyonu lisanslıdır. Kingbetting

    ReplyDelete
  54. Every year, thousands of students avail CDR assignment help from my CDR Report Writer and have a smooth sail towards a promising professional career in Australia. You can also enjoy the amazing CDR writing services from My CDR Report Writer and enjoy the exciting features of our services from anywhere in the world. If you are willing to pursue your career as a CDR Engineer in Australia, it is time to procure valuable CDR help from the CDR Australia experts.

    ReplyDelete
  55. Do you want to get best cost accounting help? Then don't have to wait more come to our experts of StudentsAssignmentHelp.com for assistance. Our experts will easily complete all your task in the proper format and structure the paper well according to your university guidelines.

    ReplyDelete
  56. Your choice of topic is incredibly sensible and additionally well written.. Thanks for sharing. I want all of your ideas arincredible! nice job!!!
    mcafee.com/activate | office.com/setup |norton.com/setup mcafee.com/activate |norton.com/setup |office.com/setup

    ReplyDelete
  57. Betpas bahis oynama sitesi zaman zaman giriş sorunları yaşatmaktadır. Kullanıcılarını üzen bir site ve ödemelerinde de sıkıntılar bulunuyor. Betpas

    Restbet bahis sitesi güvenilir mi? Restbet güncel giriş bilgileri, Restbet mobil giriş, üyelik, iletişim, şikayet ve Restbahis hakkında her şeye ulaşın. Restbet

    İmajbet bahis sitesi değerlendirmesi, İmajbet giriş güncellemeleri, kayıt-üyelik, İmajbet iletişim, hesap silme, şikayet ve İmajbet yeni giriş adresi. İmajbet

    Günümüz de birçok kişi tarafından kullanılmakta olan Vevobahis bahis sitesi, 5 nisan 2015 yılında Türkiye içerisinde hizmete girmiştir. Vevobahis

    Perabet Türkiye'nin en iyi canlı bahis alt yapisina sahiptir.Günde 300'den fazla canlı bahis seçeneğini en yüksek bahis oranlarını sizlere ... Perabet

    ReplyDelete
  58. Really Appreciate, This impressive post certainly encourages to choose Assignment Help Services. Get Assignment help

    services by the best qualified and experienced assignment experts of Complete My Assignment.

    Assignment Help

    Civil Engineering Assignment Help

    ReplyDelete


  59. Hi there,


    Thanks for providing such an important imformation through your blog, I would like to appreciate you for awesome content delivery.
    Also, visit blog posted by John Brown
    hptechnicalsupportphonenumber.com

    ReplyDelete
  60. We understand the frustration of trying to juggle work, a social life and university assessments, which is why we’re here to help you get the most out of your university experience. Our dissertation writing services UK are widespread across all the cities in UK including Bristol, London, Edinburgh, Birmingham, Newcastle, Liverpool, Glasgow, etc. When you use our Dissertationwritingservicesuk, you can order the full dissertation all at once, or just the individual chapters you need.

    ReplyDelete
  61. Great post! I am actually getting ready to across this information, is very helpful my friend. Also great blog here with all of the valuable information you have. Keep up the good work you are doing here. fix canon printer support code 5100

    ReplyDelete
  62. Great post! I am actually getting ready to across this information, is very helpful my friend. Also great blog here with all of the valuable information you have. Keep up the good work you are doing here.Call +1-888-209-3034 HP Laptop Technical Support Number, HP Helpline

    ReplyDelete
  63. Dissertation writing service students always need. We help you any time and any type of dissertation writing. Forget all the other services and hire our writers. You can easily hire our experts at Australiasssignmenthelp.com.

    ReplyDelete