Tuesday, February 21, 2012

Using a DMM as a Low Frequency Analyzer

Just about every electrical engineer and technician has a DMM on their bench. They are used for their high resolution and high accuracy voltage, current, and resistance measurement capabilities. One capability that most high performance DMMs have that users are typically not aware of is their low frequency digitizing capability. In this post we will look at combining a DMM's high resolution measurement capability with its digitizing capability to create a Low Frequency Analyzer (LFA). We will also look at some free software for performing LFA functionality with a DMM.

Most modern high performance DMMs provide a digitizing capability built-in. The sample rate is adjustable and ranges from around 1 S/s at greater than 20 bits of resolution to 50 KS/s at 14 bits of resolution. At 50 KS/s we can analyze signal frequency components below 25 KHz. This makes the DMM a useful solution for analyzing signals in applications such as:
  • Measuring total harmonic distortion on power line signals. Click here to check out an article on this application.
  • Vibration measurement and analysis.
  • Audio frequency analysis.
The challenge is there is no useful way to analyze the digitized measurements on the DMM itself. To make the digitized measurements available for analysis we have to pull them off the DMM and post process them. If we want to use our DMM as LFA that post processing includes performing a Fast Fourier Transform (FFT) on the measurements so we can view the signal's frequency components.

Let's use Agilent's 34411A high performance DMM as our example DMM we want to use as a LFA. The 34411A provides two ways to access its digitizer functionality and retrieve the readings. The first is using its LXI web interface via a LAN connection to the instrument. This method provides the advantage of needing no custom software. All you need is a web browser. There is a past GPETE post that shows a video using the 34411A as a digitizer via its LXI web interface. To check out the video click here. Once you have the readings from the web interface you can then transfer them to a program like Excel for FFT analysis. Click here to learn how to do FFT analysis in Excel.

The second way is to use custom software to connect to the 34411A, set it up as a digitizer, retrieve the measurements, and analyze them. Popular test and measurement software environments like Matlab, LabView, and VEE provide instrument drivers, FFT libraries, and plotting capabilities to make this easy as possible for experienced programmers. But if your not an experience programmer or you just don't have time to put together some custom software, I created two free programs that allow you to use the following DMMs as low cost LFAs: 34411A, 34410A, and the L4411A. Both programs use LAN to connect and control the DMMs. The first program is based off of Matlab and is entitled "Dynamic Signal Analyzer 34411A." It can be downloaded from Matlab Central (link: http://www.mathworks.com/matlabcentral/fileexchange/35161). As an example I used Dynamic Signal Analyzer 34411A to capture a 60 Hz power line signal for analysis using the 34411A. The resulting frequency domain and time domain plots from the program can be seen below.
Frequency spectrum from 60 Hz power line signal

The second LFA program was done using Agilent VEE and it is called "34411A LFA." The great thing about VEE is you can run a VEE program without using any for pay software. All you need to do to run a VEE program is to download its free run time environment. If you are interested in the VEE program just shoot me an email, tell me about your application, and I will send you the program with some instructions (neil_forcier@agilent.com). Keep in mind that both of these programs are offered "as is" and are not supported by Agilent (just me). 

In this post we talk about how high performance DMMs, with their high resolution and digitizing capabilities, can be used as a low cost LFA. We talk about how we can access the digitized measurements for post processing and analysis. Finally we looked at two free programs available to you for using the following Agilent DMMs as LFAs: 34411A, 34410A, and the L4411A. If you have any comments or personal experiences to add to this post use the comments section below.


29 comments:

  1. Our programming assignment are really helpful for the students and can be us easily.

    ReplyDelete
  2. I have to say that after reading your blog post, I had so much to learn and would like to read more of your articles in the future.You have an expertise way of writing your articles ,making them interesting to read. As a postgraduate when you are doing your research and you have been stuck on writing your literature review chapter, get our reliable Literature Review Chapter Writing Help from our skilled experts and be assured to get a top-notch literature review paper.

    ReplyDelete
  3. I must admit that prior to coming across this site, I didn't know that one can use a DMM as a Low Frequency Analyzer. You have done such a great thing to share this information with us. Feel free to click on Professional Writing Services | Writing Academic Papers

    ReplyDelete
  4. As an established Australia assignment help organization, we always aim to increase the number of in-house experts we have so that we can offer you the perfect assignment writing help in conventional courses like Management, Law, Engineering, etc. We understand how important academic assessments are in developing a student's career and future opportunities, this is why we take extreme measures to ensure that all our solutions are best-in-class. During higher studies in colleges, students often have to prepare multiple documents, quizzes and surprise tests. But somehow that doesn’t seem sufficient enough as students from those top-notch colleges are still opting for online academic assistance in the quest of their respective university assignment help service providers. It can be a very complex subject for those who do not give proper attention to it. Reasons could be many, but our team of psychology assignment help experts are highly qualified in this subject to assist you.

    ReplyDelete
  5. thank you for sharing information, information on your site is very useful for many people. I think will often come back to your site.
    packers and movers in patna

    ReplyDelete
  6. My Assignment Services is one such Australian Assignment Help provider which provides a helping hand to all your academic related queries. They have a lot of professional experts who are skilful in giving you guidance and providing you with cheap assignment help services. You are free to contact their experts by visiting their website and get your pending presentations completed on the time. Given below are some of the steps that they follow while drafting your assignments. Many students see that Assignment Help UK experts are proficient in writing your assignments but no one wonders the reason behind it. However, students pursuing IT need to understand the concepts of Java because it holds down the concept of object oriented programming. The programming concepts are complex to understand and brings a havoc to students, that is why, My Assignment Services bring you our online assignment help services. Taking out some time to consider and contrast about what options that you have that you can include by writing them on a piece of paper. You can also contact some real time Cheap Assignment Help Australia experts to assist you with the following topics.

    ReplyDelete
  7. Assignment Firm service providing all college students online assignment help. Our psychology aassignment help experts provide 100% plagiarism free content for college and university students. Thank you.

    ReplyDelete
  8. Here is a good Weblog You might Come across Fascinating that we Encourage You
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete

  9. Enjoyed studying this, very good stuff, thanks.เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete
  10. Hey, your post is very informative. AbAssignmentHelp provides online assistance to complete your assignment, and they guarantee you the lowest possible price of assignment help with unmatched quality of assignment in the UK.

    ReplyDelete
  11. Relating to keeping an individual's carpets browsing good together with performing good, regular vacuuming has to be your first shield. Yet, most vacuum cleaners can mainly manage to accummulate a percentage within the dirt that carpet is probably going to hold, cleaning company in dubai

    ReplyDelete
  12. You should take part in a contest for one of the best blogs on the web. I will recommend this site!

    Website
    Information

    ReplyDelete
  13. Suria Permai Apartment is a Leasehold apartments, located in Seri Kembangan, Selangor. Also get Taman Equine House for Sale and apartments for rent at best price with www.suriapermai.com

    ReplyDelete
  14. Book kajang avenue & Kajang Condo for sale in Kajang at discounted rates. Find almost anything for sale in Selangor @ Pearl avenue condo. Book today! https://www.pearlavenuekajang.com/

    ReplyDelete
  15. Tramadol is a drug which is an opioid pain medication and you can buy Best Tramadol online from us. The Online Pain relief Pills tramadol pills has been categorized as depressant and analgesic. The active component of this drug is Tramadol Hydrochloride (HCL) and it could be combined with the acetaminophen and they can be prescribed in the type of tablets.

    ReplyDelete
  16. If you are in need seeking legitimate research writing services, visit us at any time. Our company is not after getting cheap money from students and that is why we are rated among the best custom paper service provider.

    ReplyDelete
  17. At Web Design Sarawak, We offer highly authentic and professional web designing service to my valuable clients with a complete focus on the user interface. As I believe that at the end of the day, a site is ultimately used by the potential clients, and it should be according to their expectations. Contact us for best Web Design Sabah.

    ReplyDelete
  18. At Benedict, we are a team of freelance web designer & developer malaysia who understand the importance of developing and designing impressive visual to keep the captivate users immerse in your website by making it easy for them to find exactly what they need. I always do my best to provide the aspiring feel to your website so that users can easily connect with you. visit www.benedict.my
    freelance graphic designer malaysia
    freelance website designer malaysia

    ReplyDelete
  19. thanks for sharing it i found it so amazing youtube go for pc

    ReplyDelete
  20. I think this is an informative post and knowledgeable. I would like to thank you for the efforts you have made in writing this article
    packers and movers in patna

    ReplyDelete