Friday, January 6, 2012

Triggering a DMM with No Hands

Making a DMM measurement on a really really small pin on a chip is not an easy task. You drink a little less coffee that morning and carefully position your probe tip on the pin. Then your frozen scared to move your head to look at the DMM's display in fear the probe tip will slip off before you catch a glimpse of the reading. Has this ever happen to you? In this post we will look at easy way that a colleague of mine came up with to capture a DMM reading on the display without moving your head or your hands.

All you need is a DMM with external triggering capability, a mechanical switch, and some cabling. Here is the setup:

  • Set the DMM for manual external triggering. This means the DMM will only take a measurement on an external trigger event.
  • Position the switch on the ground under your bench by your feet.
  • Wire up the switch to the external trigger input of the DMM
From there position your probe tip on the tiny measurement pin and without taking your eyes off the measurement or moving your hands, toggle the switch with your foot. Remove your probes from the measurement point and look up to view your captured measurement on the DMM display.

When you close the switch with your foot the external triggering input of the DMM is pulled low, which in turn triggers a measurement on the DMM. To avoid the hassle of ordering a switch you could always cannibalize it from an old piece of electronics. For instance, my colleague used an old mouse. They wired a BNC adapter to a switch connected to one of the mouse buttons. The below figures show the mouse setup.




If you have any helpful comments or personal incites to add to this post just use the "Post a Comment" section below.






11 comments:

  1. That was helpfull for some beginners. DMM formation not that simple as amused, but I tried for once. I have been learning for Asic Chip Design. My learning included fast, low power with high speed designs for automotive and electronic desin

    ReplyDelete
  2. Becoming an enginner is something very important so write job application letter for engineer perfectly and have best services of that.

    ReplyDelete
  3. Great post, you have pointed out some excellent points, I as well believe this is a very superb website.
    moved here

    ReplyDelete
  4. This article gives the light in which we can watch the truth. This is extremely pleasant very detailed information and enlightens.I personally thank you for this wonderful post.For more impeccable articles get reliable assistance at our firm as we are known to offer the best web content writing service for other bloggers like you and other related sites that needs content.Hire us today.

    ReplyDelete
  5. نقدم لكم الآن خصومات هائلة من شركة تنظيف بالبخار بمكة على جميع الخدمات المنزلية المتكاملة التي تحتاجها لمنزلك و التي يمكنك من خلالها الحصول على اقل اسعار شركة مكافحة حشرات بمكة التي تقدمها لكم شركة العنود الرائدة في مجال الخدمات المنزلية مثل الخدمات التي تقدمها لكم شركة تنظيف شقق بمكة ذات الخبرة الكبيرة في تنظيف جميع انحاء المنزل .
    كما انه من خلال التواصل معنا في شركة جلي رخام بمكة المتخصصة ستتمكن من الحصول على خدمات متكاملة لتنظيف منزلك من خلال شركة تنظيف خزانات بمكة التي تتميز بانها واحدة من كبرى شركات الخدمات المنزلية الموجودة في المملكة العربية السعودية

    ReplyDelete
  6. هل تعاني من رادئة مستوي عمليات التنظيف الان مع شركة تنظيف مفروشات في الطائف حيث النظافة الشاملة وتنظيف اي بقع في السجاد والموكيت وغيرهم تواصل معنا الان واحصل علي خدمات شركة صيانة خزانات في الطائف حيث النظافة الامثل للخزان والمياة والحصول علي مياة نقية تماما الان لن يكون هناك فرصة لاي نوع من انواع الحشرات ان تزعجك فنحن في شركة مكافحة حشرات في الطائف سنقضي لك علي كل الحشرات التي توجد في منزلك احصل الان علي افضل عروض شركة تنظيف منازل في الطائف وتمتع باافضل نظافة من خلال فريق متخصص في عملية التنظيف هل عانيت كثيرا من سوء طرق نقل الغفش الان شركة نقل عفش في الطائف ستوفر لك افضل طرق نقل الاساس وبااقل اسعار من الان لن ترهق في تنظيف السيراميك والرخام وغيرهم الان مع اكبر شركة في جلي سيراميك في الطائف سنوفر لك اعلي جودة في نظافة جميع انواع الارضيات تواصل الان واحصل علي الافضل دائما ودع الان النمل الابيض تماما من منزلك فنحن في شركة مكافحة النمل الابيض في الطائف سنخلصك منه وستنعم بحياة نظيفة وصحية

    ReplyDelete