Tuesday, January 31, 2012

Matlab Function for Creating Arbitrary Waveform Files

This post features a Matlab function called convertToArb( ) that converts a vector / array of data into a waveform format that can be loaded onto Agilent's 3352xA function / arbitrary waveform generators (33521A one channel and 33522A two channel). This function converts a row or column vector into a 3352xA format .arb file (a waveform file that can be loaded onto the 33522A or 33521A). The vector data should contain voltage values ranging from 10 V to - 10 V. The convertToArb( ) function will generate a .arb file in the current Matlab open directory. The file can then be imported to the 33521A or 33522A via a USB memory stick. You can copy the code for the function below or you can download the function from Matlab Central (link at the end).

function convertToArb(data,samplerate,fName)

%check if data is row vector, if so convert to column
if isrow(data)
    data = data';
end
    
%data=importdata(filetoread1);
numberofpoints = length(data);

%Get max and min values from waveform data
data_min=min(data);
data_max=max(data);

%range has to be the maximum absolute value between data_min and data_max
range=abs(data_max);
if(abs(data_min)>abs(data_max))
    range=abs(data_min);
end
    
%Data Conversion from V to DAC levels
data_conv=round(data*32767/range);

fName = [fName '.arb']; %add file extension to file name

%File creation and formatting
fid = fopen(fName, 'w');
fprintf(fid,'%s\r\n','File Format:1.10');
fprintf(fid,'%s\r\n','Channel Count:1');
fprintf(fid,'%s\r\n','Column Char:TAB');
fprintf(fid,'%s%d\r\n','Sample Rate:',samplerate);
fprintf(fid,'%s%6.4f\r\n','High Level:',data_max(1));
fprintf(fid,'%s%6.4f\r\n','Low Level:',data_min(1));
fprintf(fid,'%s\r\n','Data Type:"Short"');
fprintf(fid,'%s\r\n','Filter:"OFF"');
fprintf(fid,'%s%d\r\n','Data Points:',numberofpoints);
fprintf(fid,'%s\r\n','Data:');
%Write data to file and close it
fprintf(fid,'%d\r\n',data_conv);
fclose(fid);

The input arguments for the convertToArb( ) function are as follows:
  • 'data' is the vector containing the waveform points that you want to convert to a .arb file
  • 'samplerate' is the sample rate setting for the 33521A or 33522A. The total time of your waveform is equal to: samplerate * number of points in the file.
  • 'fName' is the name you want to assign to the .arb file that is created, for instance "myArb" will create a "myArb.arb" file.
The following example Matlab script uses the convertToArb( ) function to create a waveform that consists of three different sine waves summed together.

%example script to demonstrate function convertToArb(data,samplerate,fName) 
xAxis = 0:.001:1; %create x axis for plot
count = length(xAxis); %get size of waveform
yAxis = zeros(1,count); %allocate array

for i = 1:count
    %build waveform that consists of three sinewaves summed together
   yAxis(i) = sin((2*pi)*xAxis(i)) + (.5*sin((2*pi)*xAxis(i)*3)) + (.3*sin(pi*xAxis(i)));
end

%call function to convert it to .arb file named myArb.arb
convertToArb(yAxis,1e6,'myArb');

Below is the resulting waveform generated with the example script captured on a scope.






10 comments:

  1. The academic transcription services are really helpful when you have so many tasks to do and data setting becomes difficult.

    ReplyDelete
  2. Photography is the art, application and practice of creating durable images by recording light or other electromagnetic radiation, either electronically by means of an image sensor, or chemically by means of a light-sensitive material such as photographic film Wedding photographer in ludhiana

    ReplyDelete
  3. Let’s explore a little bit more on these. Here I am going to provide you Australianhelp review rating which are one of the most used sites by students for doing their dissertations.
    The Edubirdie review rating show that they are really unprofessional people who do not know how to behave with the students. There are times when the students feel that they have not been approached rightly by the assignment writing services. They often resort to rude behavior with the students, which make them furious. Owing to the rough behavior of the support staffs, the students sometimes feel that they have committed a crime. The support staff is often impolite to the students, which makes them dissatisfied and discontent.
    Go through some of the reviews of this service provider and know their original potential and know myassignmenthelp Reviews Rating and student feed back.

    ReplyDelete