Friday, December 16, 2011

Simulating Power Transients for Testing ECUs

Electronic control units (ECUs) used in automotive and aerospace/defense applications need to be immune to the harsh power systems in which they operate. Power system surges and drop-outs are common, so you need to thoroughly validate your ECU to assure proper operation. To assist ECU designers, standard ISO test specifications have been developed that replicate the power transients seen in automotive applications. These test specifications are rigorous, and the test equipment required to generate these transients is specialized and expensive. As a result, this equipment typically remains in the quality control (QC) lab, and it may not be accessible to the design engineers who need it most.

In this post we will look at how modern high performance power supplies and their arbitrary waveform (arb) generation capability provide an easy to use and capable platform for power transient testing of ECUs. To do this we will generate two example waveforms common in the automotive industry. The focus of each example will be ease of use (no code) and the power supply's arb performance. To generate the waveforms we will use the N6705B DC Power Analyzer. N6705B is a modular high performance power supply with up to 4 supply outputs and over 20 modules to choose from. Outputs can be put in series or parallel for higher voltage and current needs. For creating power arbs 50 W and above the N675xA series of modules is the best choice for ECU power transient testing. The N675xA series can generate arbs with edge rates of ~33V/ms into a full resistive or capacitive load up to 680 uF.

The first figure below shows a power supply reset test pulse train that is commonly used for ECU test. In this case, the N6752A module is used to create a simple pulse-train using a sequence of pulses (created right from the front panel). The device under test (DUT) was a load of 100 Ω in parallel with 10 μF. A close up of the final pulse shows a rise time of 553 μs (second figure below). Fall time (not shown) was measured to be 206 μs. Rise and fall times of approximately 1 ms are commonly called for in these types of tests. 



Next let’s generate a transient waveform for engine crank immunity testing using a high performance power supply like the N6705B. We will use the Starting Profile waveform in the ISO 16750-2 specification, which is pictured below.


At first glance this waveform seems complex but really it can be divided into four common waveforms, three ramps and one repeating sinewave. Using the N6705B and its built-in waveforms along with its waveform sequencing capability, we can easily build the engine crank waveform. Below are some screen shots (click on to enlarge) that show building the four waveforms and sequencing them together all from the N6705B's front panel.


And finally below we get to the resulting engine crank output waveform into a load of 100 Ω in parallel with 10 μF.


If you have to capture and recreate or just create complex custom waveforms this can be done fairly easy too. Typically you can capture a waveform on a scope or generate it using software like Matlab and then transfer it to the power supply via a CSV file using a remote connection or a USB memory stick. In some cases the power supply may have its own waveform editing software. For instance the N6705B has accompanying software (model number 14585A) that provides waveform editing as well as other measurement features. 

In the post we looked at how modern power supplies like the N6705B can be used to generate complex power transients for ECU testing. They provide an easy to use power transient testing alternative to design engineers who can't easily access expensive test setups in the quality control lab or who want to avoid expensive back and forth trips to compliance testing labs. If you have any personal incites or comments you want to add please use the comments section below.

21 comments:

  1. we have probably seen the equipment before.
    Our consultants will use their experience from many sites to ensure that critical to quality parameters are considered during this process.
    We've seen what works and what definitely doesn't.

    equipment validation

    ReplyDelete
  2. Written cleaning procedures should be established. Attention should be addressed to dedicate certain equipment to specific products,
    such as fluid bed dryer bags and to residue originating from the cleaning detergent or solvent themselves.
    By packaging equipment I am referring to primary packaging equipment.


    equipment validation

    ReplyDelete

  3. I totally agree with this,
    and in fact I was about to mention some importance of equipment validation in my comment below.
    It’s certainly a fact that helps makes us work more and faster.see more

    equipmentvalidation

    ReplyDelete
  4. This is amazing job done by the author. The qualitative and quantitative data analysis can only be attained by professionals.

    ReplyDelete
  5. It may need a particular type of tool to get the job done. Many new companies often rent out these as they have limited investments. So they rent the tools instead of spending on brand new testing devices. Tester

    ReplyDelete
  6. Sometimes you ask "why are students receiving too much homework ?"
    Well, there's a whole story about it. Click on a link I've provided.

    ReplyDelete
  7. Your article for Engine Control Units is very nice. I find it very useful & it is covering every detailed aspects about Engine Control Units. Get more information about ECU from here.

    ReplyDelete
  8. I am very happy to read this. This is the kind of manual that needs to be given and not the random misinformation that’s at the other blogs. Appreciate your sharing this best posting. A top notch Assignment Help UAE Service provider offering high quality services to students, all over the world, by the team of subject experts. Assignment Help Experts offers Online Assignment Help and Assignment Writing services in Australia and US. Paper will written by US and Australian Experts.


    ReplyDelete
  9. Damaged or broken equipment can be costly to a company and downtime can have a serious knock on effect on developments. Textile Testing Equipments

    ReplyDelete
  10. Nothing compares to Weber using Genesis sort of grills. That is certainly the type gas grills which have been that will always make sure that they deliver a high performance part of down interval ToolsClubs

    ReplyDelete
  11. Assignment Help online
    Try to add only relevant data and information. If you feel that you are stuck, you can take assignment help online to get a proper idea. There are several web services which can help you to find out a suitable solution to your problems.

    ReplyDelete

  12. When you're tired, you want to relax after a stressful working hours, you need to have time to take care of the kids active.
    Please visit our website and play exciting flash games.
    Thanks you for sharing!
    visit our website

    ReplyDelete
  13. you can go through AllAssignmentHelp.com reviews. It will help you to know about the services, and it will help you to know whether that site is reliable or not. This is a way of understanding the opinion of users, and it helps the website to maintain its functionality and reliability.

    ReplyDelete
  14. obtain you help uaeassignmenthelp.com. then we gives you best assignment help uae . because our 3000+ expert research for assignment help. our writer have decades years experience. just send an email info@uaeassignmenthelp.com

    ReplyDelete
  15. Singapore Assignment help provides Essay writing help services to Singapore University students by its well-educated professional with highly dominant facts and statistics collected together for reference or analysis.

    ReplyDelete
  16. students fear of fail in exam. then uaeassignmenthelp.com gives you write my essay . because our assignment writer uae help you complete assignment in boudation time. just send an email info@uaeassignmenthelp.com

    ReplyDelete
  17. It is nice to read such high-quality content. It is a good article that discusses the topic at hand quite well. I am looking forward to read more articles from your site. Keep up the good work.
    assignment expert

    ReplyDelete
  18. COPE TECHS is an organization of Technology experts🖥️💻 with the aim to help individuals with solving Technology difficulties. We offer the best hacking services as well as our aim is not for Theft purpose but to help individuals overcoming Technology issues with our skills.

    ✴️For example-: There are so many individuals out there who owe a lot of debts💶💷 to Banks and other Loan Firms and are working hard 🛠️⚒️to pay back but really can't pay. That's were our services can help you, we have a way of generating Bitcoin and funding it into a PayPal account and by this you can pay your debts.

    ✴️Another Example of our service-: A Man or Woman who suspects his/her Spouse of Cheating but have no prove, we could help by HACKING the Spouse Cell phone📱 so he/she could get access to Chats, Emails📩, Location📍, Phone calls 📞and text message✉️ of the Spouse anywhere they are.

    ✴️We also Help student in Universities/College/High Institute📚 in changing their Grades/results saving them from repeating exams and giving them a better Degree.
    Other services we offer are-:
    ✴️Clearing of Bad Records from Courts and Police facilities.
    ✴️ Detection of weakness in Computer system security⚛️
    ✴️Funding a PayPal account💷💵
    ✴️Cyber Attacks☣️ and lots more
    Put this on your mind, "AS LONG AS IT'S TECHNOLOGY, IT CAN BE HACKED"
    We belong to the HACKERS forum HackerOne and we have the Top hackers in the forum always ready to take the risk and do a job. If you need hacking Services, contact-: COPETECHS@GMAIL.COM
    We look forward to hacking for you.

    ReplyDelete