Friday, December 9, 2011

Digitizing with a DMM

The following video demonstrates how to use one of Agilent's high performance DMMs as a low frequency digitizer and plot the result without writing any code. This can be useful in applications like DC to AC inverter distortion analysis. Where you want to capture the resulting AC voltage or current waveform from the inverter output to analyze its distortion in the time or frequency domain.


The video demonstrates collecting the measurement data from memory using the DMM's web interface and then transferring to Excel by cutting and pasting. Another easy way to do this without any code is by using Agilent's free Command Expert software. Command Expert allows you to create an Excel spreadsheet that will connect to the DMM, configure the measurement, execute the measurement, collect the measurement data, and plot it. Click here to check out my post on Command Expert.

Click here to go to the 34411A DMM product page

10 comments:

  1. you must have rewriting services are exactly what mostly students needed at the time of exams because it helps them a lot.

    ReplyDelete
  2. Awesome blog. I enjoyed reading your articles. This is truly a great read for me. I have bookmarked it and I am looking forward to reading new articles. Keep up the good work! Best assignment writing service in Brisbane by professional’s writers at best price. Assignment Help Experts offers online Assignment Help Brisbane with A+ grade. Assignment Help Experts offers Online Assignment Help and Assignment Writing services in Australia and US. Paper will written by US and Australian Experts.


    ReplyDelete
  3. Nice Blog!!
    Passage of current and application of electronic goods have made you take up electrical engineering. But now you need to regularly deal with it and so a proper clarity in concepts is required. Check out electrical engineering students assignmentin knowing those loose points.

    ReplyDelete
  4. Hey there! I can't see this video for some weird reason. Can you upload it here once more?

    ReplyDelete
  5. Your stuff is incredibly helpful.
    For Assignment Help visit our site AllAssignmentHelp

    ReplyDelete
  6. The wishes for electronic instrumentation and issue designers are far one-of-a-kind and plenty greater annoying for each size accuracy and analysis times. Because of the electronic additives, these engineers paintings on becoming an increasing number of smaller and more sophisticated, the size necessities for high-quit dmms further growth for the continually smaller currents, voltages, and resistances. Knowledge shared by Do My Dissertation Help Online | AllAssignmentHelp.Org

    ReplyDelete