Monday, November 7, 2011

Comprehensive Look at Sources of Error in DC Voltage Measurements Part 1

In this two part post we will (or at least attempt to) take a comprehensive look at all of the factors that can lead to errors in a DC voltage measurement with a DMM and how to eliminate them so you can achieve the highest accuracy possible in your measurement. In part one we will cover radio frequency interference, thermal EMF errors, noise caused by magnetic fields, and common mode rejection. If you are a seasoned DMM measurement veteran and you feel I missed something in the following sections please add it as a comment.


Radio Frequency Interference -- Most voltage-measuring instruments can generate false readings in the presence of large, high-frequency signal sources such as nearby radio and television transmitters, computer monitors, and cellular telephones. Especially when the high frequency energy is coupled to the multimeter on the system cabling. This effect can be severe when the cabling is 1/4, 1/2, or any integer multiple of the high frequency wavelength. You probably have experienced this type of effect first hand if you ever placed a mobile phone near speaker wiring and heard bursts of noise from the speaker that were certainly not part of the intended audio experience. To reduce interference, try to minimize the exposure of the system cabling to high-frequency RF sources. You can add shielding to the cabling or use shielded cabling.  If the measurement is extremely sensitive to RFI radiating from the DMM or your DUT, use a common mode choke in the system cabling, as shown in the figure below, to attenuate DMM emissions. Often you can see this same EMI reducing method being used on the data cable for your computer monitor.


Thermal EMF Errors -- Thermoelectric voltages, the most common source of error in low level voltage measurements, are generated when circuit connections are made with dissimilar metals at different temperatures. Each metal-to-metal junction forms a thermocouple, which generates a voltage proportional to the junction temperature. It is a good idea to take the necessary precautions to minimize thermocouple voltages and temperature variations in low level voltage measurements. The best connections are formed using copper-to-copper crimped connections. The figure below shows common thermoelectric voltages for connections between dissimilar metals.

Agilent benchtop DMMs use copper alloy for their input connectors
Noise Caused by Magnetic Fields -- When you make measurements near magnetic fields, take precautionary steps to avoid inducing voltages in the measurement connections. Voltage can be induced by either movement of the input connection wiring in a fixed magnetic field, or by a varying magnetic field. An unshielded, poorly dressed input wire moving in the earth’s magnetic field can generate several millivolts. The varying magnetic field around the ac power line can also induce voltages up to several hundred millivolts. Be especially careful when working near conductors carrying large currents. Where possible, route cabling away from magnetic fields, which are commonly present around electric motors, generators, televisions and computer monitors. In addition, when you are operating near magnetic fields, be certain that the input wiring has proper strain relief and is tied down securely. Use twisted-pair connections to the multimeter to reduce the noise pickup loop area, or dress the wires as closely together as possible.

For more on magnetic coupling and other spurious coupling issues in measurements check out the post Ground Loops and Other Spurious Coupling Mechanisms and How to Prevent Them

Common Mode Rejection (CMR) -- Ideally, a DMM is completely isolated from earth-referenced circuits. However, there is finite resistance between the DMM’s input LO terminal and earth ground. This can cause errors when measuring low voltages that are floating relative to earth ground. Check out the post Understanding Common Mode DMM Specifications for more information on CMR.

Stay tuned for part 2 next week!


21 comments:

  1. Nicely written--This post is equally informative as well as interesting . Thank you for information you been putting on making your site such an interesting If you have time please visit my RTCA-Do160 page.

    ReplyDelete
  2. I want someone to help me with my chemistry homework because that is too tricky and complicated so i needed help

    ReplyDelete
  3. Current clamps are electrical devices with two jaws that open to allow clamping around an electric conductor.www.themultimeterguide.com

    ReplyDelete
  4. Multimeter is good tool for testing. Read more best multimeter reviews here http://www.zoniv.com/best-multimeter/

    ReplyDelete
  5. Java is an object oriented programming language. It is used in a variety of computing platforms, you can see it nearly everywhere nowadays, from embedded devices and mobile phones to enterprise servers and supercomputers. See more c language cheat sheet

    ReplyDelete
  6. I think that you should examine this blog for some useful tips on how to write good essay. This kind of stuff could save you in the future

    ReplyDelete
  7. Thanks for sharing these tips, its too useful for everyone. We offer protection plans for your electronic gadgets on low prices. You can contact at Geek squad support assistance we guides you which plan are best for you. Geek Squad Tech Support

    ReplyDelete
  8. Well, this article is interesting. It was cool to read that. I enjoy reading your posts, friend.

    ReplyDelete
  9. Great post, I really like your knowledgeable information, our company iPad Rental Virginia also appreciate your work.

    ReplyDelete
  10. Amazing article, i really amazed to see this informative post you share wonderful information like this https://logonick.com/

    ReplyDelete
  11. This is really an amazing blog. Your blog is really good and your article has always good thank you for information.

    คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete
  12. Students who encounter trouble with completing their buy pre written essays and pre written research papers can contact our company as we have expert writers in the field.

    ReplyDelete
  13. Experts working at the geek squad tech support are amazingly great in helping the customers with some of the best services. Reach these experts anytime and you would be helped for any issue you might face. So call the experts at geek squad tech support now and grab expert help.

    ReplyDelete
  14. Obtain master assistance for fixing all technical flaws with your appliances at Geek Squad Support. Feel free to reach tech savvy experts at Geek Squad Support round the clock as per your convenience for addressing all your concerns related to electronic appliances.

    ReplyDelete
  15. Get Solution for all technical errors or complicated issues with your gadgets at Geek Squad Support Number. So if you face any issues Avail this wide Number of services and support at Geek Squad Support Phone Number for gadgets or devices.

    Geek Squad Tech Support Number

    ReplyDelete