Monday, September 19, 2011

DMM Resistance Measurement Considerations

The digital multimeter or DMM offers two methods for measuring resistance: 2–wire and 4–wire ohms. For both methods, the test current flows from the input HI terminal and then through the resistor being measured. For 2–wire ohms, the voltage drop across the resistor being measured is sensed internal to the multimeter. Therefore, test lead resistance is also measured. For 4–wire ohms, separate "sense" connections are required. Since no current flows in the sense leads, the resistance in these leads does not give a measurement error. In this blog post I will discuss some general considerations and tips when making DMM resistance measurements.

4–Wire Ohms Measurements
4-wire ohm measurement use the HI and LO DMM leads as well as the HI-Sense leads (that is why they are called "4-wire"), the setup for a 4-wire ohms measurement is shown below. 

The sense leads essentially extend the DMM measurement to the DUT junctions instead of the HI and LO terminals . This eliminates the voltage drop across the HI and LO leads caused by the test current. Since the sense leads are high impedance there is essentially no current flow into the sense inputs. The 4–wire ohms method provides the most accurate way to measure small resistances. Test lead resistances and contact resistances are automatically reduced using this method. Four–wire ohms is often used in automated test applications where resistive and/or long cable lengths, numerous connections, or switches exist between the DMM and the DUT.

Removing Test Lead Resistance Errors
Modern DMMs offer a built-in function, often labeled as "Null" or "Math", for eliminating test lead error.To use the Math function on a DMM you short the test leads to together. The Math function will then make a resistance measurement of the test leads and store it. The DMM will then mathematically subtract the measured lead resistance for subsequent resistance measurements to cancel out the lead resistance error.

Minimizing Power Dissipation Effects
When measuring resistors designed for temperature measurements (or other resistive devices with large temperature coefficients), be aware that the DMM will dissipate some power in the device–under–test. If power dissipation is a problem, you should select the DMM's next higher measurement range to reduce the errors to acceptable levels. The following table shows examples of Agilent's 34410A and 34411A DMMs source current for various measurement ranges.


Errors in High Resistance Measurements
When you are measuring large resistances, significant errors can occur due to insulation resistance and surface cleanliness. You should take the necessary precautions to maintain a "clean" high–resistance system. Test leads and fixtures are susceptible to leakage due to moisture absorption in insulating materials and "dirty" surface films. Nylon and PVC are relatively poor insulators (10^9 Ω) when compared to PTFE (Teflon) insulators (10^13 Ω). Leakage from nylon or PVC insulators can easily contribute a 0.1% error when measuring a 1 MΩ resistance in humid conditions.

Click here to check out the DMMs that Agilent offers



13 comments:

  1. This comment has been removed by a blog administrator.

    ReplyDelete
  2. but with the help of the clamp meter, it becomes much easier to even measure in such big electrical machinery. www.themultimeterguide.com

    ReplyDelete
  3. شركة نقل اثاث بالدمام التفاؤل شركة نقل اثاث بالخبر كما انها افضل شركة نقل اثاث بالجبيل نقل عفش واثاث بالجبيل والخبر والقطيف والدمام
    شركة نقل اثاث بالدمام
    شركة نقل اثاث بالجبيل
    شركة نقل اثاث بالقطيف

    ReplyDelete
  4. https://issuu.com/emc-mee/docs/______-____________-__________-____ شركات نقل العفش بالدمام
    https://issuu.com/emc-mee/docs/______-______-________________1_.do نقل عفش بالدمام
    https://issuu.com/emc-mee/docs/______________________________.docx نقل اثاث بالدمام
    https://issuu.com/emc-mee/docs/________-______-______-_____________5eee6b62b0c947 شركة نقل عفش بالمدينة المنورة
    https://issuu.com/emc-mee/docs/___________________________________ شركة تنظيف خزانات بجدة

    ReplyDelete
  5. https://issuu.com/emc-mee/docs/________-______-______-________.doc شركة نقل عفش بجدة
    https://issuu.com/emc-mee/docs/________-______-______-____________ شركة نقل عفش بالرياض
    https://issuu.com/emc-mee/docs/____________________________________76c983dc869693 شركة تنظيف بالطائف
    https://issuu.com/emc-mee/docs/____________________________________be97b233ba8cdb شركة تنظيف خزانات بالمدينة المنورة
    https://issuu.com/emc-mee/

    ReplyDelete
  6. If you want to read more about Monica Crowley plagiarism, you can check https://dissertationauthors.com/blog/monica-crowley-plagiarism-and-why-this-example-is-negative-for-students out. It might be really useful for students.

    ReplyDelete
  7. شركة تنظيف شبابيك بالرياض متكاملة الخدمات التي تسعى نحو الأفضل منذ النشأة الأولى لها وتواجدها بالميدان؛ وما هذا إلا لعرض أفضل

    المصدر: شركة تنظيف شبابيك بالرياض

    تعمل مختلف شركات التنظيف المتواجدة في الرياض على توفير أفضل الأدوات والتجهيزات التي تمنحك البريق واللمعان خلال دقائق معدودة، فهي تهتم بادق التفاصيل وتحرص على توفير ايدي مدربة ومؤهلة على ذلك بجانب تقديم عدد من العروض التي تشمل تنظيف غرف النوم مع غرف الريسبشن والمطبخ والحمام، وفي بعض المناسبات أو الاحتفالات يتم توفير عروض أخرى ذات أسعار مناسبة للكثير من الأسر.

    المصدر: شركة خدمات تنظيف بالرياض

    يمكنك سيدتي الآن التخلص من مشكلة تنظيف الكنب بصورة نهائية خاصةً تلك المصنوعة من القماش المخمل أو الشامواه بل والتي يصعب إزالة الكسوة الخاصة بها، حيث تتواجد بعض البقع الزيتية أو الخاصة بالمشروبات التي تجف على السطح وتظل عالقة في نسيج القماش ويصعب إزالتها بالطرق التقليدية.

    المصدر: شركة تنظيف كنبات بالرياض

    كذلك مجرد تواجدك في مكان نظيف رفقة العائلة أو الأصدقاء سيدخل الراحة النفسية عليك، على هذا الأساس تجد أن عمليات التنظيف المعتادة والتي تقوم بها ربات المنازل قد تزيل من خلالها البقع والأوساخ إلا أنها قد لا تتمكن من إزالة الأثار التي قد تخلفها كذلك الأمر بالنسبة للأضرار الأخرى التي تصيب الفرشات.

    المصدر: شركة تنظيف فرشات بالرياض

    يعد تنظيف المنزل أحد المهام الشاقة التي تقع على عاتق ربة المنزل خاصةً إذا كانت امرأة عاملة فلم يتبقى لديها متسع من الوقت لكي يتم تنظيفه أو في حالة كبر مساحته وتعدد طوابقه ووجود الاطفال به مما يجعله أكثر عرضة للإتساخ، ولذلك يكون السبيل الوحيد أمامك سيدتي هو الإستعانة بشركات تنظيف المنازل التي تمنحك أفضل النتائج من حيث اللمعان والبريق والتطهير العميق.

    المصدر: شركة خدمات منزلية بالرياض

    شركة تنظيف نجف بالرياض الأناقة اليوم لم تعد مقصر على ملابسك الخاصة بل امتدت إلى المكان الذي تتواجد به مع تواجد الأنتيكات أو النجف التي تتناسب مع ذوقك الخاص

    المصدر: شركة تنظيف نجف بالرياض

    شركة تنظيف وصيانة مسابح بالرياض هي المكان المناسب الذي يعمل كل شخص بداخلها على تقديم خدمة مثالية للسادة العملاء داخل أو خارج الرياض

    المصدر: شركة تنظيف وصيانة مسابح بالرياض

    ReplyDelete
  8. Check out this this article it is about easy essay topics. This will be especially helpful for college students!

    ReplyDelete
  9. Online assignment help services by Sample Assignment have been trusted by many students worldwide for over a decade. Assignment Experts providing best digital marketing assignment help to students struggling with their assignment tasks given by Universities. Whether it is an essay, dissertation, case study or any other form of assessment, you can trust us for 100% original and plagiarism free content by which get HD Grades. An Australian assignment provider such as Sample Assignment, is well-known for its 24-hour online assistance on the WhatsApp platform. Students can reach out to us with their queries at any point of the day or night and get the most effective solutions for them. Our best online assignment help experts talk about how to select and evaluate the right academic sources, which will help you clear all your assignment-related doubts at best and affordable price. Whenever need to search for ‘do my assignment for me’, our experts will be assist you.

    ReplyDelete
  10. لهذا يلزم المراعاة وتوجيه الرعاية عن ظهور أية آثار للإصابة ومحاولة التنبؤ بها قبل وقوعها بواسطة مؤسسة مختصة مثل مؤسسة مكافحة النمل الابيض بالاحساء صاحبة الخبرة الطويلة في ذلك الميدان ،
    افضل شركة مكافحة حشرات
    شركة مكافحة النمل الابيض بالجبيل
    شركة مكافحة حشرات بالجبيل
    شركة رش مبيدات بالجبيل

    ReplyDelete
  11. Along with our write my essay online services, we offer a range of other help such as research buy college papers online, custom research papers and term paper writing service help among others.

    ReplyDelete
  12. Assignment help who have been providing help to the students of various renowned colleges and universities of Java assignment help step-by-step.

    ReplyDelete