Tuesday, August 16, 2011

Simple Way to Use the Power of the Cloud for Test and Measurement

In today's economy technology companies have their resources spread across the globe. These global engineering resources have to work closely together throughout the design and testing life cycle of a product. One major challenge these global engineering teams face is sharing real test data access or control of testing resources across thousands of miles and country borders. In this blog post we will look at a simple but secure example of how to use cloud computing or the cloud to share test data and test resource control across the globe.

Cloud computing refers to using hardware and software computing resources in a computer network, such as the internet, for computation and storage, instead of just on a local computer. I am going to use the term “cloud” in this article to refer to computing assets on the internet that are provided by a third party such as Google or Amazon. The cloud can provide three main benefits to test:

1. Share test data across global engineering teams that can be accessed anywhere at any time without a company firewall getting in the way.

2. To serve as an always connected intermediary between your test software and your computing device. Imagine starting or stoping a test from your smart phone at the airport.

3. You can leverage the massive computing capability of the cloud for test applications that require a lot of computing power for post processing measurement data.

In this post we will focus on cloud benefits for bullets 1 and 2. For our cloud test example we will use a popular and free cloud service called "Dropbox." Dropbox allows you to set up a folder or file directory on your computing device, such as a PC or smart phone, that is sync'd to the cloud (Dropbox server) for backup. When you change or add a file on one computing device Dropbox will automatically sync the change or addition on any other computing device you have Dropbox installed. For security Dropbox is password protected, for more info on Dropbox click here.

For storing, sharing, and viewing test data Dropbox is a great tool for 3 main reasons:

  1. It allows you to securely back up your test data on the cloud 
  2. It allows you to easily share test data among geographically separated teams and companies, such as if you are using a CM that does not have access to your companies intranet.
  3. It allows you to access test data from almost anywhere securely without having to deal with a VPN, such as if you wanted to check the outcome of a test on your smart device at an airport in India.
Now getting the test data to Dropbox is fairly easy since all major software development environments like Labview, Matlab, or Visual Studio have easy to use APIs that allow you to write data to various file types such as an Excel Spreadsheet. The way we incorporate Dropbox into the test mix is by having our test program write to files that are located in a Dropbox folder. Then as long as the computer running your test program is connected to the internet Dropbox will automatically send your test data to the cloud and sync it to other computing devices sharing that same Dropbox account. Now the test data is safely back-upped and securely shared.

We can even go a step further and add certain types of remote control aspects to our test using Dropbox. If instead of just writing data to a file on Dropbox, we have our test program also read from a file we could could control our test from the cloud too! We could do something as simple as use a small section of the test data file for changing basic test settings to something as complex as using a scripting language to change entire test routines. 

As a proof of concept for this post I setup an example cloud test using Agilent's 34972A DAQ / Switch Unit, VEE programming language, and Dropbox. The example cloud test was created to simulate a long term DAQ type testing environment. It makes temperature, voltage, fan rotation, and irradiance measurements on a DUT. I added two simple settings controls to the test data Excel file that allow you to turn on or off a fan and heater on the DUT. The VEE program reads the settings from the Excel file periodically and uses the control features on the 34972A to change the DUT settings. Below is a screen shot of the excel spread sheet from my example cloud test program (click to enlarge). You can also get your own read-only version of my test data file using the Dropbox link I provided below.




To conclude Dropbox provides an easy to use secure way to leverage the power of the cloud to back up, access, and share test data easily and securely. We even looked at a way to use Dropbox and the cloud to control a test remotely from anywhere without the hassle of VPNs. If you have a test example where you use the power of the cloud I would love to hear about please share as a comment or shoot me an email.

11 comments:

  1. شركة نقل اثاث بالدمام التفاؤل شركة نقل اثاث بالخبر كما انها افضل شركة نقل اثاث بالجبيل نقل عفش واثاث بالجبيل والخبر والقطيف والدمام
    شركة نقل اثاث بالدمام
    شركة نقل اثاث بالجبيل
    شركة نقل اثاث بالقطيف

    ReplyDelete
  2. https://www.behance.net/gallery/46472895/_
    https://www.behance.net/gallery/46463613/_
    https://www.behance.net/gallery/46463247/_
    https://www.behance.net/gallery/46451097/_
    https://www.behance.net/gallery/46460639/_
    https://www.behance.net/gallery/46462575/_

    ReplyDelete
  3. https://www.behance.net/gallery/46450923/_
    https://www.behance.net/gallery/46450419/_
    https://www.behance.net/gallery/46430977/-jumperadscom
    https://www.behance.net/gallery/42972037/_
    https://www.behance.net/gallery/40396873/Transfer-and-relocation-and-Furniture-in-Dammam

    ReplyDelete
  4. From this blog you will get all the info you need to write great essay. Only the best students are using this stuff

    ReplyDelete
  5. افضل شركة رش مبيدات بالرياض  الشركة متخصصة في مكافحة الحشرات بطرق حديثة وجودة عالية بشكل لا يضر بأهل المنزل أو يضر الأطفال أو يؤثر عليهم
    الشركة لديها كافة الحلول للقضاء على الحشرات ورشها وإبادتها إبادة تامة ,
    تمتلك الشركة أيضا أفضل الكوادر البشرية الذين يوظفون جُلَ طاقتهم من أجل القضاء على الحشرات وذلك عن طريق الرش والأمصال التي تؤدي للقضاء عليها ,
    لدينا الخبرة لذلك وبأقل الأسعار وأعلى مستوى جودة و أمان بإذن الله تعالى
    اتصل بنا نصلك أينما كنت
    نحن الأفضل في هذا المجال,
    نحن جميعاً نعلم أن السر وراء إبادة الحشرات هي رش المبيدات لذا فكان أول اهتمامات الشركة أن تحرص على استخدام أفضل أنواع المبيدات الحشرية التي تجعلها من أفضل شركات رش مبيدات بالرياض، نظراً لما يملكه المبيد من فعالية قوية و إبادة فورية دون ان يلحق أي أضرار بصحة الموجودين في المنزل ولا يسبب لهم الإزعاج، و كما حرصت الشركة على أن توفر كل ذلك، وكان من ضمن اهتماماتهم أن تقدم خدماتها بأقل الأسعار لكي تناسب كافه فئات العملاء دون أن تسبب لهم أي ضغط مادي.
    الرش يكون بأنواع مجربة وغير ضارة وآمنة على كل من يستخدمها معنا أنتم بأمان وصحتكم بأمان و لا داعي للقلق أو التفكير طويلا فإننا لسنا الوحيدون ولكننا المميزون… اقرأ المزيد

    المصدر: شركة رش مبيدات بالرياض

    شركة مكافحة حشرات بالرياض للحشرات تعاني كل ربات البيوت من مشكلة تكاثر الحشرات ووجودها بشكل مستمر في المنزل، مما يسبب لها الكثير من القلق والإزعاج ويضعها في العديد من المواقف المحرجة أمام ضيوفها فبالرغم من نظافة المنزل ولكن عند وجود الحشرات أمام الضيوف يشعرها بأن المنزل غير نظيف، كما أن الحشرات تحمل الكثير من البكتيريا والجراثيم العدوي الفيروسية التي تسبب الأمراض .
    وتقوم بإبادتها بكل سهولة بين الأشخاص مما ينتج عنها الضرر والأمراض الذي يلحق بصحه الانسان من ما يجعلها تبحث عن الطرق التقليدية التي تساعدها في القضاء نهائيا على الحشرات المزعجة، مثل العته و الفئران والصراصير وأيضاً النمل الابيض وغيرها من الحشرات، التي تسببها الإزعاج مجرد أن تتواجد في المنزل ولكن بعد اليوم لا داعي لكل ذلك يمكنك التخلص من كل هذه الحشرات عند التواصل مع شركة مكافحة حشرات بالرياض ، التي تقوم بالتخلص من كافة أنواع الحشرات ومكافحه الحشرات المنزلية الضارة، عن طريق شركة رش مبيدات بالدمام التي هدفها هو مكافحة الحشرات داخل الدمام وخارجها، كما أن الشركة لديها فريق عمل متميز قادر على إبادة الحشرات نهائياً،
    والعمل على ضمان عدم عودته من مكان مرة أخرى كما أنها تحرص علي أن توفر أفضل أنواع المبيدات الحشرية، المصرح بها من وزارة البيئة والصحة و الأمنة تماماً، على صحه الإنسان وقادرة على إبادة الحشرات من المرة الأولى كل هذا وأكثر، شركة مكافحة حشرات بالدمام على أن تقدم كافة خدماتها لعملائها الكرام بأقل الأسعار الغير قابلة للمنافسة و التي لا تجدها إلا من خلال تعاملك مع شركة مكافحة الحشرات بالرياض تتصل بنا الآن من أجل الحصول على كل ذلك…… اقرأ المزيد

    المصدر: شركة مكافحة حشرات بالرياض

    افضل شركة عزل اسطح بالرياض يتعرض سطح المنزل لعدد من الأسباب التي تؤثر بالسلب على السن الافتراضي لهذا السطح، فالأمطار الكثيفة الموسمية تسقط بكثرة بمدينة الرياض عاصمة المملكة العربية السعودية في فصل الشتاء الأمر الذي يترك تأثيره على سطح المنزل وربما ينشأ تسريب لداخل المنزل من هذا السطح، أما في فصل الصيف فأشعة الشمس المرتفعة تكون السبب في انبعاث موجة حارة داخل البيوت الأمر الذي يدفع اصحاب المنزل لتشغيل المكيفات طوال اليوم فترتفع معها تكليفات كشف حساب وقد يعطل مكيفات المنزل من كثرة التشغيل. … اقرأ المزيد

    المصدر: شركة عزل اسطح بالرياض

    ReplyDelete
  6. Babel account & manag contracting companies
    The program includes 12 specialized systems in contracting field and providing explanation library
    of 145 videos with total of 6 hours of explanation and providing more than 200 questions in the
    field of contracting and group of essays which serve contracting companies.
    برنامج محاسبة مقاولات
    برنامج محاسبة شركات المقاولات
    برنامج مقاولات
    برنامج ادارة شركات المقاولات
    برنامج الاستثمار العقارى
    برنامج استثمار عقارى
    برنامج لشركة استثمار عقارى
    برنامج ادارة محطات الخرسانة
    برنامج محطات خرسانة

    ReplyDelete