Tuesday, June 21, 2011

Making AC Impedance Measurements on Fuel Cells

Making AC impedance measurements on fuel cells can help identify problems with the fuel cell components and help identify deviations in the fuel cell assembly process. Typically when testing fuel cells, multiple impedance measurements are made at various frequencies, the results are then plotted across the frequency band resulting in an Electrochemical Impedance Spectroscopy (EIS) measurement. In this blog post we will cover building a test system for making AC impedance measurements on fuel cells

To make AC impedance measurements on a fuel cell that is producing dc current we first need stimulate the fuel cell output with a load that is varied sinusoidally at a particular frequency and then digitize the cell's output AC current and AC voltage. The digitized signal data would then by fed to a PC where custom software or a math package, such as Matlab or Excel, would be used to perform post processing on the digitized data that includes:


  1. Perform a Fast Fourier Transform on the digitize current and voltage waveform data.
  2. Using complex math functions, divide the transformed voltage by the transformed current to obtain the complex impedance (both magnitude and phase).
  3. Repeat at multiple frequencies to create a full spectrum of impedance measurements on the fuel cell.
The digitized AC current and voltage measurements needed for the impedance calculations can be done with just two pieces of equipment, a high performance electronic load (eload) and a function generation. Below shows the fuel cell impedance measurement set-up (click to enlarge).



By connecting the function generator to the eload's external analog programming input, we can use it to control the eload's load value or input impedance. By setting the function generator output to a sine wave at various frequencies we can create the necessary AC load variations to create the desired output current and voltage waveforms from the fuel cell under test. Agilent's 33210A function generator is a good cost effective fit for this application. For the eload, the reason I underline "high performance" in the above paragraph is because the eload requires some advance features including parallel voltage and current measurement digitizers built-in to capture the input voltage and current simultaniously. Otherwise we would have to add a two channel external digitizers to capture the AC voltage and current (for current we would also need a current shunt) from the fuel cell. The above figure shows Agilent's N3300 eload series. The N3300 series fills the role of a "high performance" eload because it provides simultaneous voltage and current digitization capability. The max. frequency you can make an AC impedance measurement on is going to be limited by the eload's max bandwidth specification, which is the max.rate you can change its input load or impedance setting. For the N3300 eload series the max. sinusoidal bandwidth is 10 KHz. Because of their design, eloads cannot operate at full specifications at low voltages, typically < 3 V. To over come this characteristic of eloads a "boost" power supply can be added to the circuit in series as shown in the figure. For more info on using an eload with a boost supply click here

Unfortunately going into the details of implementing an FFT in software and performing division of complex equations to make AC impedance measurements and creating a Electrochemical Impedance Spectroscopy plot is beyond the scope of this blog post. The good news is there are plenty of information on the internet for performing these calculations (just google it). Also the first link below is to an Agilent app note that provides more detailed information on preforming AC impedance measurements on fuel cells. The second link below takes you to a complete turn-key solution that provides the hardware and software needed to make AC impedance measurements on fuel cells. 



For more info on a turn-key fuel cell test system click here

45 comments:

  1. Very interesting blog. I'm looking for any V-I simple method. Without external devices as Aglient. Because even simple measurements becomes overcomplicated using all this.

    ReplyDelete
  2. Really nice blog, thanks for sharing the valuable information.
    Load cell manufacturers

    ReplyDelete
  3. I admired your helpful words. Top class contribution. I really hope you’ll write more. I'll continue looking for.
    Compression Load Cell | Shear Beam Load Cell

    ReplyDelete
  4. If you set out to make me think today; mission accomplished! I really like your writing style and how you express your ideas. Thank you. electronic components distributor

    ReplyDelete

  5. شركة نقل اثاث بالدمام التفاؤل شركة نقل اثاث بالخبر كما انها افضل شركة نقل اثاث بالجبيل نقل عفش واثاث بالجبيل والخبر والقطيف والدمام
    شركة نقل اثاث بالدمام
    شركة نقل اثاث بالجبيل
    شركة نقل اثاث بالقطيف

    ReplyDelete
  6. I like the post format as you create user engagement in the complete article. It seems round up of all published posts. Thanks for gauging the informative posts.
    cara menggugurkan kandungan

    ReplyDelete
  7. This comment has been removed by the author.

    ReplyDelete
  8. هل تعاني من حشرة البق؟ هل يشكل بق الفراش ازعاج كبير لك؟ هل تشكل حشرة البق خطورة كبيرة عليك وعلى اسرتك واطفالك!؟ هل تريد التخلص من بق الفراش؟ هل تبحث عن الحلول الممكنة للقضاء على البق وتجنب الاصابة ببق الفراش؟ كل هذة الاسئلة سوف يتم الرد عليها من خلال خبراء افضل شركة مكافحة البق بالمدينة المنورة شركة رش حشرات بالمدينة المنورة
    شركة مكافحة حشرات بالمدينة المنورة
    شركة رش مبيدات بالمدينة المنورة
    شركات مكافحة حشرات ورش مبيدات بالمدينة هل تبحث عن شركة مكافحة حشرات بالسعودية هل لديك نمل في المطبخ او حشرة البق في الخشب؟ هل عندك صراصير او نمل او فئران وتفسد عليك حياتك في منزلك او شركتك؟ لا تقلق فهناك العديد من شركات مكافحة الحشرات في السعودية وأيضا يوجد العديد من شركة رش مبيدات ومكافحة الحشرات بالمدينة المنورة شركة مكافحة البق بالمدينة المنورة
    شركة مكافحة فئران بالمدينة المنورة

    ReplyDelete
  9. يقوم العمال لدي شركتنا شركة نظافة بالمدينة وشركة تنظيف خزانات بالمدينة المنورة بالتصوير للخزان من الداخل حتي يتم التعيين و التحديد له من الداخل و معرفة ما يوجد به من الداخل من اوساخ او من اتربة او اي شيئ يمكن ان يكون غير نظيف و يقوموا ايضا بالتحديد اذا تو شركة تنظيف خزانات بالمدينة المنورة
    شركة غسيل خزانات بالمدينة المنورة
    يتم ايضا القضاء علي اي فطريات من الممكن ان تتواجد بداخل الخزانات حيث يقوموا بفك اي فتحات خاصة بالتهوية و يقوم العمال بالفك للفتحات للتبريد التي يقوم الهواء بالخروج منها و عن طريق هذه الفتحات و يقوم العمال بالادخال لجهاز التنظيف و الغسيل للمكيف و يتم العمل للغسيل الشامل للمكيف من الداخل و ستم غسيل شامل للماكينة من الخارج و يتم المسح الجيد للمكيف قبل ان يتم تركيبه و تنظيفه و سحب ماكينة التنظيف الداخلية منه . شركة غسيل خزانات بالمدينة
    شركة تنظيف خزانات بالمدينة

    ReplyDelete
  10. شركة نقل عفش بالدمام
     شركة نقل عفش بالدمام والخبر  بفك العفش حيث يقوم نجارون مدربون على مستوي عالي ومتقدم بفك العفش بطريقة صحيحة. شركة نقل اثاث بالدمام
    الحرص الشديد في التعامل مع قطع العفش وخاصة القطع غالية الثمن أو القطع الحساسة وتقوم شركة نقل اثاث بالدمام والخبر العمالة بترقيم قطع الأثاث التي تتكون من عدة قطع كالدواليب مثلا فان بعض الدواليب يكون مكون من أكثر من قطعة ومن ثم إذا لم يتم ترقيم القطع بعناية سيصعب للغاية تركيبه مرة ثانيه. ارخص شركة نقل اثاث بالدمام
    شركة نقل اثاث بالجبيل

    ReplyDelete

  11. كن علي ثقة كاملة في شركتنا شركة نقل الأثاث بالدمام لأننا سنوفر لك أسعار رائعة وفريدة من نوعها حيث سعر الرد الواحد لنقل العفش ونقل الاثاث بالمنطقة الشرقية شركة نقل عفش بالجبيل
     شركة نقل عفش بالدمام والخبر  بفك العفش حيث يقوم نجارون مدربون على مستوي عالي ومتقدم بفك العفش بطريقة صحيحة. شركة نقل عفش بالقطيف
    لذا فلا تتردد في الاتصال بنا حيث نعتبر افضل شركة نقل عفش بالدمام و السعودية. شركة نقل عفش بالخبر

    ReplyDelete
  12. أكد عزيزي الكريم أنك سوف تحظى بأفضل وأقل سعر بالدمام أو خارجها حيث نعد من افضل شركه نقل عفش بالدمام وتأكد أيضا أنك سوف تحظى بأفضل خدمة نقل عفش بالمنطقة الشرقية وجميع أنحاء المملكة العربية السعودية شركة نقل عفش بالخبر
    نقل عفش بالخبر
    شركة نقل عفش فى بالخبر
    شركة نقل عفش بالدمام شركة نقل اثاث بالقطيف  شركة توصيل الاثاث والعفش للمنزل إذا لم يكن باستطاعتك توصيل الاثاث والعفش بنفسك لا تقلق يمكننا توصيل الاثاث والعفش من خلال خدمة التوصيل لدينا شركات نقل العفش بالخبر

    ReplyDelete
  13. شركة نقل اثاث بالقطيف متخصصين بالخدمات المنزلية وما يهمنا هي مصلحة العميل الذى يريد ان يعتمد على أحد شركات نقل العفش والاثاث بالقطيف او اى مدينة اخرى متواجدين بها فى نقل اثاث سكنه بكل طمأنينة دون اى قلق من شركة نقل الاثاث لما يحتويه من اثاث غالى وثمين وذكريات جميلة من الدرجة الاول وان يحصل علي افضل الخدمات باقل الاسعار و باعلي جوده ونحن في شركتنا شركة نقل اثاث بالقطيف شركة نقل عفش بالخبر
    شركة نقل عفش بالقطيف
    نقدم لسيادتكم شركة نقل عفش بالخبر حيث تقدم لكم أرقى الخدمات في مجال نقل العفش بالدمام لذلك تصنف من افضل شركات نقل العفش بالدمام شركة نقل عفش بالجبيل
    شركة نقل عفش بالاحساء

    ReplyDelete
  14. نحن في شركة تنظيف بالدمام نعد الافضل في مجال تنظيف الشقق لاننا نهتم بادق التفاصيل المهمة التي تعطي انطباع جيد لدي عملائنا لهذا فنحن شركة نظافه بالدمام نستخدم أفضل الادوات التي تستخدم في عملية التنظيف العالمية التي تستخدم في افضل الدول العالمية شركة تنظيف مكيفات بالدمام
    تنظيف مكيفات بالدمام
    فى الدمام او فى المنازل السعوديه يوجد مشكله فى تغير لو ن الكنب مما يؤدى اللى الحاجه اللى عمليات غسيل ونظافه للكنب بالدمام الدينا فريق العمل مخصص فى عملية غسيل الكنب ونظافته بالدمام ليس هذا فقط نقوم عملية غسيل لفرش الكنب بالدمام لاشك ان الكنب له عمليات استخدام ولابد ان يكون منظره رائع دائما لهذا شركة غسيل مكيفات بالدمام
    شركة تنظيف مكيفات بالقطيف
    نحن في شركة تنظيف كنب بالدمام نقوم بغسيل و تنظيف الكنب بأنواعه المصنوع من الأقمشة والجلد وتنظيف المجالس الأرضية بجميع أشكالها.. شركة أحباب طيبة للخدمات المنزلية هي من أقدم و افضل شركة تنظيف كنب بالدمام شركة تنظيف مكيفات بالخبر

    ReplyDelete
  15. لذا لا تتكاسل في إحضار احسن شركة تنظيف كنب بالدمام تكون ذات مصداقية وأمانة في العمل تستخدم المنظفات المستوردة عالية الجودة التي لا تؤثر على صحتك وصحة أسرتك شركة تنظيف كنب بالدمام
    شركة غسيل كنب بالدمام
    تعاني الكثير من السيدات اثناء عملية تنظيف الشقق من شركة تنظيف شقق بالخبر و ذلك لان معظمهم في البداية يحاولون العمل بمفردهم و اتمام عملية التنظيف و الغسيل دون مساعدة ظنا بان ذلك يكون افضل شركة تنظيف شقق بالدمام حيث ان بعض السيدات لا يثقون في الاعتماد علي شركات التنظيف بالقطيف لان كل شركات التنظيف و خدمات تنظيف و النظافة لا تعتبر شركات تنظيف شقق بالدمام شركة تنظيف كنب بالقطيف

    ReplyDelete
  16. شركه مكافحه الحشرات بالدمام هي افضل الشركات في الحلول الاباديه للقضاء علي الحشرات نهائيا تتميز منتجات شركتنا بالجوده والنتائج الفعاله وسرعه التأثير كما يتميز عملائنا في سرعه الوصول لتأديه مهامهم.تستخدم شركة مكافحة حشرات بالدمام خدمات كثيره خاصه للقضاء علي الحشرات بطريقه اباديه بحيث لا تعود مره اخري شركة مكافحة حشرات بالقطيف
    كما أن افضل شركة مكافحة حشرات بالدمام متخصصة أيضاً والوزغ والثعابين والأبراص والناموس وغيرها من الحشرات الأخرى المختلف ونحن شركة رش مبيدات بالدمام والخبر وشركة رش مبيدات بالقطيف نظرا لحاجة المواطنين فى هذه المناطق لمثل هذه الخدمات الملحة والضرورية فقد لبينا رغبتهم وفتحنا لنا فروعا فى كل من الدمام والخبر والقطيف والجبيل لنغطى حاجتهم فى مكافحة الحشرات ورش المبيدات مع افضل شركة مكافحة حشرات بالدمام شركة مكافحة حشرات بالخبر
    شركة مكافحة حشرات بالدمام

    ReplyDelete
  17. تخلص من جمیع أنواع الحشرات الضارة التي تؤذیك وتؤذي عائلتك واتصل بشركة مكافحة النمل الابيض بالقطيف لتحصل على خدمة ممتازة ومعاملة ممتازة، تخلص من الأمراض التي ممكن أن تصیب أفراد عائلتك وتواصل مع شركتنا لتحصل على منزل خالي من الحشرات الضارة التي تؤرق حیاتك وتخرب المنزل، شركة مكافحة النمل الابيض بالقطيف شركة مكافحة البق بالدمام
    شركة مكافحة النمل الابيض بالدمام
    هل يشكل بق الفراش ازعاج كبير لك؟ هل تشكل حشرة البق خطورة كبيرة عليك وعلى اسرتك واطفالك!؟ هل تريد التخلص من بق الفراش؟ هل تبحث عن الحلول الممكنة للقضاء على البق وتجنب الاصابة ببق الفراش؟ كل هذة الاسئلة سوف يتم الرد عليها من خلال خبراء افضل شركة مكافحة البق بالدمام وجميع مدن المنطقة الشرقية شركة مكافحة النمل الابيض بالقطيف
    شركة رش مبيدات بالدمام

    ReplyDelete
  18. يقوم العمال لدي شركتنا شركة نظافة بالمدينة وشركة تنظيف خزانات بالمدينة المنورة بالتصوير للخزان من الداخل حتي يتم التعيين و التحديد له من الداخل و معرفة ما يوجد به من الداخل من اوساخ او من اتربة او اي شيئ يمكن ان يكون غير نظيف و يقوموا ايضا بالتحديد اذا تو شركة تنظيف خزانات بالمدينة المنورة
    شركة غسيل خزانات بالمدينة المنورة
    يتم ايضا القضاء علي اي فطريات من الممكن ان تتواجد بداخل الخزانات حيث يقوموا بفك اي فتحات خاصة بالتهوية و يقوم العمال بالفك للفتحات للتبريد التي يقوم الهواء بالخروج منها و عن طريق هذه الفتحات و يقوم العمال بالادخال لجهاز التنظيف و الغسيل للمكيف و يتم العمل للغسيل الشامل للمكيف من الداخل و ستم غسيل شامل للماكينة من الخارج و يتم المسح الجيد للمكيف قبل ان يتم تركيبه و تنظيفه و سحب ماكينة التنظيف الداخلية منه . شركة غسيل خزانات بالمدينة
    شركة تنظيف خزانات بالمدينة

    ReplyDelete
  19. شركة مكافحة النمل الابيض بالخبر
    شركة مكافحة النمل الابيض بالخبر لاسباب كثيره ومنها التخلص نهائيا من الحشرات الطائره والزاحفه ومكافحة الصراصير والنمل الابيض والفئران وبق الفراش شركة مكافحة النمل الابيض بالقطيف
    شركة مكافحة البق بالقطيف
    شركة مكافحة البق بالدمام تعطي لك ضمان لعدم ظهور البق مرة اخرى بالمنزل لمدة اكثر من سنة وذلك يميزها عن باقي شركات مكافحة الحشرات في الدمام  شركة مكافحة البق بالدمام

    ReplyDelete
  20. شركة مكافحة الحشرات بالدمام
    شركة مكافحة حشرات بالدمام ، إن مشكلة انتشار الحشرات في كل مكان سواء في المنزل أو في العمل أو في الشركة أو في أي مكان يتواجد به الناس  شركة مكافحة الحشرات بالقطيف
    ركة مكافحة الفئران بالقطيف تقدم لجميع عملائها أقوى خدمات المكافحة التي تضمن لكم القضاء التام والنهائي على تواجد الفئران داخل المكان المصاب مهما كانت درجة انتشار  شركة مكافحة النمل الابيض بالدمام
    شركة مكافحة الفئران بالقطيف

    ReplyDelete
  21. شركة تنظيف بالخبر من الشركات التنظيف الضخمة التي صنعت كيان كبير بين الشركات الاخريات، اعتمدت منذ زمن طويل على استخدام اجهزة التعقيم . شركة تنظيف بالخبر
    شركة نظافة بالخبر
    افضل شركة نظافة بالخبر نعمل دائما على تقديم افضل اسعار شركات تنظيف بالخبر تستخدم الشركه افضل مواد التنظيف وافضل المبيدات للقضاء على الحشرات  شركة تنظيف شقق بالخبر

    ReplyDelete
  22. شركة نقل اثاث بالخبر
    شركة نقل اثاث بالقطيف المجهز بأعلى المعدات والاجهزة لنقل اثاث سكنك الى المكان الذى تريده دون احداث اى تلف او كسور فة الاثاث او العفش  كما تقوم شركة نقل اثاث بالقطيف بنقل  الاثاث باستخدام أحدث التقنيات و الآلات الخاصة برفع و تنزيل اثاث لتجنب حدوث أي خدش أو تلف بالأثاث كما تعتمد شركة نقل عفش بالقطيف في كافة أعمال النقل على عمالة مدربة على ايدى ماهرين شركة نقل عفش بالخبر
    شركة نقل اثاث بالقطيف
     شركة نقل عفش بالدمام والخبر  بفك العفش حيث يقوم نجارون مدربون على مستوي عالي ومتقدم بفك العفش بطريقة صحيحة. شركة نقل عفش بالقطيف
    شركة نقل اثاث برأس تنورة

    ReplyDelete
  23. تملك شركة نقل عفش بالظهران الفنين المختصون في فك النجف والأشياء الزجاجية الغالية بطريقة أكثر أمن للحفاظ عليها من الكسر والتلف خلال عملية النقل.يتم فك كل قطعة من الأثاث وتغليفها بشكل كامل وبعناية ودقة كاملة للحفاظ على الأثاث. شركة نقل عفش بالظهران
    شركة نقل اثاث بالظهران
    افضل شركة نقل اثاث بالدمام وشركه نقل عفش بالخبر والقطيف  والامر ليس قاصرا على الدمام  وانما لدينا فروع اخرى بالجبيل والقطيف والاحساء  و نحن من أوائل الناس كــ شركة نقل عفش بالخبر والدمام لدينا خبرة متطورة في خدمات نقل اثاث السكنى والتجاري والفندقي بكل عناية ومهنية لعملائنا الكرام بالاعتماد على تكنولوجيا النقل من الباب إلى الباب باستخدام أحدث الآليات في النقل لضمان أمان خدمة النقل في اقل وقت واقل تكاليف شركة نقل عفش بالدمام
    شركة نقل اثاث بالدمام
    الحرص الشديد في التعامل مع قطع العفش وخاصة القطع غالية الثمن أو القطع الحساسة وتقوم شركة نقل اثاث بالدمام والخبر العمالة بترقيم قطع الأثاث التي تتكون من عدة قطع كالدواليب مثلا فان بعض الدواليب يكون مكون من أكثر من قطعة ومن ثم إذا لم يتم ترقيم القطع بعناية سيصعب للغاية تركيبه مرة ثانيه. أرخص شركة نقل عفش بالدمام

    ReplyDelete
  24. وتعتمد شركتنا فى عمليات النظافة التى تقوم بها على مقومات وعناصر اساسية تساعدها على تقديم الخدمة للعميل بأفضل صورة ممكنة
    شركة تنظيف
    شركة تنظيف بالكويت
    شركة تنظيف منازل بالكويت
    شركة تنظيف شقق بالكويت
    افضل شركة تنظيف منازل بالكويت

    ReplyDelete
  25. To be practical, a cooling unit must have the capacity to keep up an unfaltering temperature. Generally individuals would need to kill their units and on constantly as the temperature turn out to be excessively chilly or hot. furnace repair poughquag

    ReplyDelete
  26. This content is very cool thank you very much for publishing
    شركة رش مبيدات بالدمام

    ReplyDelete
  27. شركة تنظيف بالجبيل بتقديم خدمات النظافة كواحدة من افضل شركات التنظيف بالجبيل لمدينة الجبيل والجبيل الصناعية وذلك لكثرة الطلب من سكان تلك المدينة الجميله على خدماتنا فقد قررنا فتح فرع لنا حتى نقوم بتقديم خدمات النظافة فى اسرع وقت ممكن ولسهوله التواصل مع كل عملاءنا الكرام حيث  ان شركتنا شركة شامكو افضل شركة نظافة فى الجبيل والخبر والدمام تحقق لكم كل ما تحتاجونه فى عمليات الغسيل والنظافة العامة لكل الاشياء التى تخصكم شركة تنظيف بالدمام
    شركة تنظيف بالخبر
    خص شركة تنظيف بالقطيف : حرصاً من شركة تنظيف بالقطيف على اكتساب ثقة عملائها وتقديم مستوى عالي من الرفاهية والراحة لعملائها تقدم شركة تنظيف بالقطيف أرخص الاسعار في عالم النظافة وذلك عن طريق عمل تعاقدات سنوية وتعاقدات نصف سنوية وتقديم العروض والخصومات للعملاء الجدد شركة تنظيف منازل بالقطيف تقدم خدمات النظافة بارخص الاسعار . افضل شركة تنظيف بالقطيف اسرع خدمة تنظيف بالقطيف : اتصل بنا تجد خدماتنا امامك فنحن مميزون بسرعة الوصول للعميل شركة تنظيف بالجبيل
    شركة تنظيف بالقطيف

    ReplyDelete
  28. شركه نقل عفش بالاحساء
    افضل شركة نقل اثاث بالدمام وشركه نقل عفش بالخبر والقطيف  والامر ليس قاصرا على الدمام  وانما لدينا فروع اخرى بالجبيل والقطيف والاحساء  و نحن من أوائل الناس كــ شركة نقل عفش بالخبر والدمام لدينا خبرة متطورة في خدمات نقل اثاث السكنى والتجاري والفندقي بكل عناية ومهنية لعملائنا الكرام بالاعتماد على تكنولوجيا النقل من الباب إلى الباب باستخدام أحدث الآليات في النقل لضمان أمان خدمة النقل في اقل وقت واقل تكاليف شركه نقل عفش بالجبيل
    شركه نقل عفش بالقطيف
    شركة نقل اثاث بالقطيف المجهز بأعلى المعدات والاجهزة لنقل اثاث سكنك الى المكان الذى تريده دون احداث اى تلف او كسور فة الاثاث او العفش  كما تقوم شركة نقل اثاث بالقطيف بنقل  الاثاث باستخدام أحدث التقنيات و الآلات الخاصة برفع و تنزيل اثاث لتجنب حدوث أي خدش أو تلف بالأثاث كما تعتمد شركة نقل عفش بالقطيف في كافة أعمال النقل على عمالة مدربة على ايدى ماهرين شركة نقل عفش بالخبر

    ReplyDelete
  29. شركة نقل اثاث بالدمام
    شركة نقل اثاث بالقطيف متخصصين بالخدمات المنزلية وما يهمنا هي مصلحة العميل الذى يريد ان يعتمد على أحد شركات نقل العفش والاثاث بالقطيف او اى مدينة اخرى متواجدين بها فى نقل اثاث سكنه بكل طمأنينة دون اى قلق من شركة نقل الاثاث لما يحتويه من اثاث غالى وثمين وذكريات جميلة من الدرجة الاول وان يحصل علي افضل الخدمات باقل الاسعار و باعلي جوده ونحن في شركتنا شركة نقل اثاث بالقطيف شركة نقل اثاث بالقطيف
     شركة نقل عفش بالدمام والخبر  بفك العفش حيث يقوم نجارون مدربون على مستوي عالي ومتقدم بفك العفش بطريقة صحيحة. شركة نقل عفش بالدمام
    الحرص الشديد في التعامل مع قطع العفش وخاصة القطع غالية الثمن أو القطع الحساسة وتقوم شركة نقل اثاث بالدمام والخبر العمالة بترقيم قطع الأثاث التي تتكون من عدة قطع كالدواليب مثلا فان بعض الدواليب يكون مكون من أكثر من قطعة ومن ثم إذا لم يتم ترقيم القطع بعناية سيصعب للغاية تركيبه مرة ثانيه. شركة نقل اثاث بالخبر

    ReplyDelete
  30. تعمل شركة اللمسه في مكافحة الحشرات مثل النمل والصراصير وجميع انواع الحشرات بأبها الان ، وتعتبر شركة اللمسه من اشهر شركات مكافحة الحشرات في السعودية , لدينا عمالة مدربة ومتخصصة المواد المستخدمة فى مكافحة الحشرات غير ضارة على الانسان وليس لها روائح نعمل بدون مغادرة المنزل نعمل على راحة عملائنا .
    شركة مكافحة النمل الابيض بنجران
    شركة رش مبيدات بالخرج
    شركة مكافحة حشرات بالخرج
    شركة مكافحة النمل الابيض بالخرج
    شركة رش مبيدات بأبها
    شركة مكافحة حشرات بأبها
    شركة مكافحة النمل الابيض بأبها
    شركة رش مبيدات بنجران
    شركة مكافحة حشرات بنجران
    شركة رش مبيدات بالعينه


    ReplyDelete
  31. هل تبحث عن شركة متخصصة فى خدمات التنظيف بالطائف بافضل المعدات والسوائل وثقة تمة فى العمل ودقة فى النتائج كل هذه المميزت توفرها شركة الخليج الشركة الافضل والامثل فى الخدمات المنزلية بالطائف وبما اننا الشركة الافضل والامثل بدون منافس سوف نسعى لتوفر افضل الخدمات باقل تكلفة وبقدر كبير من الاهتمام والدقة عزيزى اينما كنت فى اى منطقة ا وحى تابع لمدينة الطائف اتصل بنا وسوف نصلك فى الحال شركة الخليج للخدمات المنزلية شركة تنظيف منازل بالطائف
    شركة تنظيف فلل بالطائف
    شركة تنظيف خزانات بالطائف
    شركة تسليك مجارى بالطائف
    شركة رش مبيدات بالطائف
    شركة مكافحة نمل ابيض بالطائف
    شركة مكافحة حشرات بالطائف
    شركة عزل اسطح بالطائف
    شركة عزل خزانات بالطائف

    ReplyDelete
  32. ابعاد درب ضد سرقت
    درب ضد سرقت را در هر ابعادي مي تواند ساخته ! ولي ابعاد استاندارد درب ضد سرقت 105/210 ميباشد.فقط بايد اين نكته را مد نظر داشت كه ابعاد درب ضد سرقت تك لنگه يك محدوديت دارد كه به دليل وجود سازه فلزي داخل درب ضد سرقت نميتوان عرض ان را بيشتر از يك مقداري (يعني يك متر و پانزده سانت )باشد به دليل اينكه در ضد سرقت در اين حدود ابعاد حدودآ يك متر بازشو خواهد داشت و فضاي زيادي از مكان نصب شده را از بين ميبرد

    برگرفته از سایت - reference
    درب ضد سرقت

    ReplyDelete
  33. Babel account & manag contracting companies
    The program includes 12 specialized systems in contracting field and providing explanation library
    of 145 videos with total of 6 hours of explanation and providing more than 200 questions in the
    field of contracting and group of essays which serve contracting companies.
    برنامج محاسبة مقاولات
    برنامج محاسبة شركات المقاولات
    برنامج مقاولات
    برنامج ادارة شركات المقاولات
    برنامج الاستثمار العقارى
    برنامج استثمار عقارى
    برنامج لشركة استثمار عقارى
    برنامج ادارة محطات الخرسانة
    برنامج محطات خرسانة

    ReplyDelete
  34. Nice Blog, thank you so much for sharing such an amazing information with us.
    Mutual Fund Distributor

    ReplyDelete
  35. دانلود آهنگ کاشکی میشد از پرستو در سایت اوری ملودی

    متن آهنگ کاشکی میشد پرستو
    کاشکی میشد دوباره بازببینمت
    بغلم بازبگیرمت
    یه بار دیگه تورو
    کاشکی میشد دوباره باز ببینمت
    بغلم بازبگیرمت
    یه بار دیگه تورو

    ♫ ♫ ♫ ♫

    بم میگن همه
    بین این همه سیاهی ها تصویر منه
    از دید من دیوونه بهتره
    رنگی ندیدم از تو، تو خودم اینم دلیلش
    تویه تاریکیا گم شدم تو خیال خودم
    زمان زودتر میره جلو وقتی نشستم کنارت

    ♫ ♫ ♫ ♫

    ReplyDelete
  36. This ought to be checked with an air conditioning organization, temporary worker, or air conditioning supply organization. Airco

    ReplyDelete
  37. Enjoyed studying this, very good stuff, thanks.

    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete
  38. Here is a good Weblog You might Come across Fascinating that we Encourage Youเว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete