Wednesday, April 27, 2011

Optimizing PXI Modular Test System Throughput Webcast

A super smart colleague of mine just did a great modular test webcast entitled "Optimizing PXI Modular Functional Test System Throughput." Below you will find an overview of the webcast and at the bottom a link to the webcast recording. 

Webcast Overview:
Reducing overall test time in high volume electronic manufacturing sites is critical to meeting manufacturing capacity and cost targets. Optimizing throughput, while not sacrificing test coverage or production yield, is essential to retaining a competitive edge.

Best-in-class manufacturers use statistical methods during test system development to achieve high throughput without compromising test coverage or test yields. During test system development, statistically based Gauge Reliability and Repeatability studies are used to verify the stability of the test methods and test system. After establishing a reliable and repeatable test, methods to optimize throughput can be explored. The statistical methods can be used again to verify test throughput optimization will not impact test yields.

This Webcast will explore these statistical methods used during electronic functional test development and deployment to help the test engineer achieve accurate, reliable results.

Who should view this webcast:
  • Test engineers responsible for automated test
  • Aerospace and Defense
  • Electronic test
  • Communications & Semi-conductor testing
Webcast Link (Hosted by EE Times):

9 comments:

  1. I have read your blog its very attractive and impressive. I like it your blog.

    Java Training in Chennai Core Java Training in Chennai Core Java Training in Chennai

    Java Online Training Java Online Training Core Java 8 Training in Chennai java 8 online training JavaEE Training in Chennai Java EE Training in Chennai

    ReplyDelete
  2. Java Corporate Training Companies in Chennai Corporate Training Companies in India Corporate Training Companies in India

    Corporate Training in Chennai Corporate Training in Chennai

    Corporate Training Companies in India Corporate Training Companies in India

    Java Corporate Training Companies in India Java Corporate Training Companies in India

    Java Corporate Training Companies in Chennai

    ReplyDelete
  3. Java Training Institutes Java Training Institutes Java EE Training in Chennai Java EE Training in Chennai Java Spring Hibernate Training Institutes in Chennai J2EE Training Institutes in Chennai J2EE Training Institutes in Chennai Core Java Training Institutes in Chennai Core Java Training Institutes in Chennai

    Hibernate Online Training Hibernate Online Training Hibernate Training in Chennai Hibernate Training in Chennai Java Online Training Java Online Training Hibernate Training Institutes in ChennaiHibernate Training Institutes in Chennai

    ReplyDelete

  4. http://emcmee.jimdo.com/
    http://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D9%86%D9%82%D9%84-%D8%A7%D8%AB%D8%A7%D8%AB-%D8%A8%D8%A7%D9%84%D8%B1%D9%8A%D8%A7%D8%B6/ شركة نقل عفش بالرياض
    http://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D9%86%D9%82%D9%84-%D8%B9%D9%81%D8%B4-%D8%A8%D8%A7%D9%84%D8%B7%D8%A7%D8%A6%D9%81/ شركة نقل عفش بالطائف
    http://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D9%86%D9%82%D9%84-%D8%B9%D9%81%D8%B4-%D8%A8%D8%A7%D9%84%D8%AF%D9%85%D8%A7%D9%85/ شركة نقل عفش بالدمام
    http://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D9%86%D9%82%D9%84-%D8%A7%D8%AB%D8%A7%D8%AB-%D8%A8%D8%AC%D8%AF%D8%A9/ شركة نقل عفش بجدة
    http://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D9%86%D9%82%D9%84-%D8%B9%D9%81%D8%B4-%D8%A8%D8%A7%D9%84%D9%85%D8%AF%D9%8A%D9%86%D8%A9-%D8%A7%D9%84%D9%85%D9%86%D9%88%D8%B1%D8%A9/ شركة نقل عفش بالمدينة المنورة

    ReplyDelete
  5. http://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D8%AA%D9%86%D8%B8%D9%8A%D9%81-%D8%A8%D8%A7%D9%84%D8%B7%D8%A7%D8%A6%D9%81/ شركة تنظيف بالطائف
    https://emcmee.jimdo.com/%D8%B4%D8%B1%D9%83%D8%A9-%D8%AA%D9%86%D8%B8%D9%8A%D9%81-%D8%AE%D8%B2%D8%A7%D9%86%D8%A7%D8%AA-%D8%A8%D8%A7%D9%84%D9%85%D8%AF%D9%8A%D9%86%D8%A9-%D8%A7%D9%84%D9%85%D9%86%D9%88%D8%B1%D8%A9/ تنظيف خزانات بالمدينة المنورة
    http://emcmee.blogspot.com.eg/2017/02/blog-post.html
    http://emcmee.blogspot.com.eg/2017/02/blog-post_7.html
    http://emcmee.blogspot.com.eg/2017/02/copany-cleaning-tanks-medina.html
    http://emcmee.rebelmouse.com/

    ReplyDelete
  6. This comment has been removed by the author.

    ReplyDelete
  7. If you need to get the highest sat score I recommend that you do it as soon as possible because this could help you and you will definitely get the highest score

    ReplyDelete