Tuesday, April 5, 2011

Ground Loops and Other Spurious Coupling Mechanisms and How to Prevent Them Part 2

This is a two part blog post is based off a great tutorial I read titled “Tutorial on Ground Loops” by P. M. Bellan. A link to the tutorial can be found at the end of the post. The subject of the two part post is something you won’t find in textbooks from your EE courses, spurious coupling mechanisms in circuits and test systems and how to prevent them. A spurious coupling mechanism is any outside unwanted voltage or current source entering a signal path. There are five main spurious coupling mechanisms: direct conduction, capacitive coupling, inductive coupling, radiated electromagnetic field pickup, and ground loops. The part one post focused on the first four types of spurious coupling (click here for part one). In this post we will focus strictly on ground loops.

Ground Loop Theory
Kirchoff's law tells us the total DC voltage in a complete circuit (Vloop) is zero. When considering AC components in a circuit, Kirchoff's law is superseded by Faraday's law. With Faraday's law Vloop = - dF/dt. F is the magnetic flux in the loop. The magnetic flux is given by F = BA. B is the magnetic field linking in the loop and the area of the loop is A. Faraday's law is what makes the basis for Transformers, inductors, and also ground loops. The make up of a ground loop signal depends on linked spurious time-dependent magnetic flux produced by nearby external circuits (fluorescent lighting, switching power supply, motor, computer) as well as the resistance and inductance in the loop.

Ground Loop Examples
The figure below shows and example of a measurement setup where a ground loop is created. The ground loop is formed by the the measurement instrument being connected to ground, the sensor or device under test (DUT) is connected to ground, and both instrument low sides are connected together via the shielding in the coax cable.This creates a loop (shown in green) for spurious time-dependent magnetic flux to enter (shown in blue) and creates unwanted current flow (shown with green arrows).
Used by permission from P. M. Bellan
Eliminating the ground loop in the above example is just a matter of locating and eliminating the inadvertent short (assuming you know it exists). What if we are making a measurement on a DUT that is suppose to be grounded? In this case we can look to our measurement or test instrument to brake the ground loop. For instance most high quality DMMs and power supplies have their low side connector isolated from ground with the option to short it to a ground potential. In this case you would want to ensure the low side connection of the instrument remains isolated from ground to prevent a ground loop from being created.Of course the isolation does have some finite impedance for DC and AC that you may want to check in the instrument's specifications when performing sensitive measurements. Some test and measurement instruments, such as scopes, typically have the low side connector tied to ground. In this case you would need a differential circuit (differential probe for scopes), isolation transformer, or optical isolation to break the ground loop. These types of ground isolation methods introduce their on limitations on the measurement.
The next example involves a multi-channel measurement setup and each channel shares a common low side connection. This setup may be a instrument, such as a digitizer, with multiple channels or a complex test system with switching. This time a loop is created between the low sides of two measurement channels as shown in the figure below. 
Used by permission from P. M. Bellan
One common way ground loops of this type are broken is by disconnecting the shielding or low side return from either the instrument or the DUT. This method will brake the ground loop but it will also degrade the signal since it brakes the signal path return. 
The third example ground loop involves two test and measurement instruments connected together. As shown in the figure below, each instrument is connected to ground and the loop is completed by each instrument's low side being connected together.
Used by permission from P. M. Bellan

This type of ground loop can be broken if one of the instrument's low side is isolated from ground.

Methods for Eliminating and Reducing Ground Loop Error
  • Breaking the loop: As mentioned throughout the post, there are multiple ways to break the loop to eliminate ground loop error including remove an unintentional short, use an instrument with an isolated low side, use a differential circuit / probe, use an isolation transformer, or use optical isolators depending on your application.
  • Increasing inductance of loop path to decrease loop current: By adding inductance, and therefore impedance, into the ground loop you can lower the ground loop current without affecting the desired signal. This can be accomplished by wrapping cabling, whether it be twisted pair or coax cable, around shield beads, a ferrite core, or an iron-core transformer. The more turns the more inductance is added to the loop. For a real world example of this look at the video cord on your computer monitor it will most likely have an iron-core around it. This method is more effective for higher frequency or sudden transient ground loop signals. 
  • Eliminating the area of the ground loop: Make the area of the loop smaller by using shorter signal cabling, shorter power cables, twisting power cables together, and using AC power outlets that are adjacent to each other
  • Removing linked magnetic flux: If possible remove noisy devices out of the test measurement area. This could mean moving a test away from a motor or replacing a switching supply with a linear supply.

Click here to check out the "Tutorial on Ground Loops"

16 comments:

  1. I actually draw my attention so I'd like to know more about this. Keep posting valuable information about this man! Thank you for sharing.
    Regards - www.office.com/setup

    ReplyDelete
  2. If you are looking for some info on how to write good homework you should look at at some blogs, like this one for example. It probably has everything that you need

    ReplyDelete
  3. شركة نقل عفش من الرياض الى الامارات

    شركة نقل اثاث من الرياض الى الامارات
    شركة نقل اثاث من الرياض الى جدة
    شركة نقل عفش من الرياض الى جدة

    شركة نقل Whatever the reasons you wish to store the furniture for it, it is your right to find a service that suits your home and suitable for each piece of furniture that you have to communicate with the numbers of the institution and make sure you get what you want and the completion of the required tasks as hoped and more by the best institution in the inventory Foundation creativity Practical and main instructions before, during and after moving your furniture
    First: Tips during the first round before moving the loaf
    - Arrange as much as possible so that the cuttings do not mix with each other before transferring them.

    - It is preferable to separate the minute or small savings from things that are too great for not losing them.

    Second: Instructions for the second period during the shipment of baggage
    - An empty headquarters should be made available all the way from the halls away from Headquarters so that the working group can move freely.

    - All pieces should be written in detail in a paper or electronic notebook for greater accuracy.

    ReplyDelete
  4. Hey friends if you love to play adventures online game then must try free robux its best adventures game ever.

    ReplyDelete
  5. Thanks for the information. Now I know how to prevent that. Use https://dissertationauthors.com/blog/executive-summary-writing to improve your blogging. Okay?

    ReplyDelete
  6. link
    Would you rather questions are incredibly versatile and it gives your partner a good time and theme to narrate on, from light and funny to deep and sometime might even to disturb. Looks cool right.

    ReplyDelete
  7. click here
    Shadow Fight 2 Mod Apk Download 2019 (Unlimited Money, Gems) ... Or Have you ever played Shadow Fight 2 game? ... Therefore, we bring here a complete guide on Shadow Fight 2 MOD APK with unlimited gold, money, gems & everything and we have also provided a direct link to download the game.

    ReplyDelete
  8. visit post
    Pokemon Go, uses the mobile device GPS to locate, capture, battle, and train the Pokémon for battle, which appear as they are in the player's real-world location. The players can defeat the gym with help of the Pokemon Strength chart.

    ReplyDelete
  9. Pickup lines are short funny lines to say to a women. They are lines to appreciate or gently tease people dirty pickup lines

    ReplyDelete
  10. คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete
  11. http://gpete.blogs.keysight.com/2011/04/ground-loops-and-other-spurious.html?showComment=1559116761548#c4303983929632098242

    I have done multiple research to find which website updated the latest answers for Wordpress. Came across this website called Slant Six games

    ReplyDelete
  12. Wordscapes Solutions
    I have done multiple research to find which website updated the latest answers for Wordpress. Came across this website called Slant Six games

    ReplyDelete
  13. bp visa credit card
    If you are more into using Credit cards, then BP Credit Card will find you easy options to go ahead with your shopping and dining.

    ReplyDelete