Wednesday, March 23, 2011

Creating Arbitrary Waveform Sequences on the 33521A and 33522A

This blog post explains and demonstrates how to create an arbitrary waveform sequence with Agilent's 33522A or 33521A function arbitrary waveform generators. Waveform sequencing is the ability to seamlessly transition (no discontinuities in the output) from one waveform in memory to another waveform somewhere else in memory. Waveform sequencing allows you to create complex easily reconfigurable waveforms by pasting together other simpler waveforms in memory. It is analogous to creating a custom playlist on your MP3 player. Some example sequencing applications include generating serial protocols, simulating the output of environmental sensors over a wide range of conditions, or simulating a biomedical signal such as an ECG signal over a wide range of conditions.
Currently there are two ways to create a arb waveform sequence: using SCPI commands or editing an existing sequence file (.seq file). I will cover both methods in this post. The example sequence we will create consists of three built-in arb waveforms so if you own a 33521A or a 33522A you have these waveforms on your instrument. The three waveforms used are: Negative Ramp, Lorentz, and Sinc. Lets start with the SCPI example. In the following SCPI example, all text preceded by "//" are comments explaining the command and are not part of the command (commands in blue). You can send these commands to the 3352xA either by putting them in your software code, using Agilent Connection Expert interactive IO feature, or using the interactive IO feature on the 3352xA's web interface.
The first four commands reset the 3352xA to a known condition and load an instance each waveform used in the sequence from  non-volatile memory to volatile waveform memory:

*RST //reset the 33522A or 33521A to known state
MMEM:LOAD:DATA "INT:\BUILTIN\NEG_RAMP.arb" //load negative ramp
MMEM:LOAD:DATA "INT:\BUILTIN\LORENTZ.arb"  //load lorentz
MMEM:LOAD:DATA "INT:\BUILTIN\SINC.arb" //load sinc
The following command creates our three waveform sequence. The "DATA:SEQ" part tells the 3352xA that this is a sequence command. The numbers "#3152" tell the 3352xA how long, in ASCII characters, the body of the sequence command is. In our example the "3" tells how long the character count number is ("1", "5", and "2" are three digits). The 152 tells the 3352xA that there are 152 characters in the body of the sequence command. "TESTseq" is the name of the sequence.

DATA:SEQ #3152TESTseq,"INT:\BUILTIN\NEG_RAMP.arb",0,once,lowAtStart,10,"INT:\BUILTIN\LORENTZ.arb",3,repeat,highAtStart,10,"INT:\BUILTIN\SINC.arb",0,once,lowAtStart,10

Lets look at the Lorentz waveform definition in the sequence: "INT:\BUILTIN\LORENTZ.arb",3,repeat,highAtStart,10,
The part in quotes gives the location and name of the waveform being used in the sequence. The "3" tells the 3352xA to play this waveform for 3 cycles. The "repeat" option tells the 33522A that we want to play this waveform more than one time. Notice the other two waveform definitions use the option "once" to play just a single cycle of the waveform. The "highAtStart" option tells the sync output to go high at the start of this waveform. The "10" tells the 3352xA at what point in the waveform to change the sync output (must be at least 4). Refer to the 3352xA Programming Reference guide for a complete list of the settings for defining a sequence. Okay now lets continue on with the rest of the commands we need to output our new sequence:

FUNC ARB  //put the 3352xA into arb waveform mode
FUNC:ARB TEXTseq  //load our sequence into channel 1
SOUR1:FUNC:ARB:SRAT 130e6  //sample rate to 130 MS/s
VOLT 1 VPP  //set the amplitude
OUTP1 ON  //turn on the channel 1 output

Now your 3352xA should be outputting the TESTseq we just created. We still have one more step to go. The sequence is only in volatile memory so if you shut off or reset the 3352xA the sequence will be erased. The following command stores the sequence in internal non-volatile memory. 

MMEM:STOR:DATA "INT:\TESTseq.seq"

Below is a scope screen shot of the sequence we just created. The waveform in green is the sync output of the 3352xA. Notice the Lorentz waveform is played three times and the sync output goes high at the start (point 10) of the Lorentz waveform.

A second way to create a sequence is to modify an existing sequence (.seq file) to create a new one. Whenever you create a new sequence via SCPI commands and store it in non-volatile memory it is stored as a .seq file. To modify it to create a new sequence copy the .seq file from the 3352xA to a USB memory stick.  Transfer it to a computer and open it with a text file editor like Windows Notepad. The .seq file that we just created is below:

File Format:1.10
Sample Rate:130000000.000000
High Level:0.500000
Low Level:-0.500000
Filter:"step"
Header:Arb Name, Repeat Count, Play Control, Marker Mode, Marker Point
INT:\BUILTIN\NEG_RAMP.ARB,1,"once","lowAtStart",10
INT:\BUILTIN\LORENTZ.ARB,3,"repeat","highAtStart",10
INT:\BUILTIN\SINC.ARB,1,"once","lowAtStart",10

Ignore the first line "File Format: 1.10." The next four lines are the amplitude, sample rate, and filter setting for the sequence. This can all be modified if you wanted to change the settings of the sequence. The next line is the header for the waveforms and settings in the sequence. Notice the waveforms and settings are defined the same way they were in the SCPI example. You can modify the waveform names, settings, or add another waveform to create a whole new sequence. You could also copy and paste the sequence text above into a .txt file, modify it, and save it as a .seq file to create a new sequence without any SCPI commands. Whatever you name the .seq file will be the name of the sequence. From there just copy it from the USB memory stick to the 3352xA internal memory and you have a new sequence.

16 comments:

  1. Thank you for sharing excellent informations. Your website is so cool. I am impressed by the details that you have on this website. It reveals how nicely you understand this subject. Bookmarked this website page, will come back for extra articles. You, my friend, ROCK! I found simply the info I already searched everywhere and simply could not come across. What a great web site.
    Regards - www.office.com/setup

    ReplyDelete
  2. If you look at this info you will probably find some tips and hints on how to write good and interesting personal statement. Make sure to do it

    ReplyDelete
  3. I found this post quiet interesting and exciting, and the author of this post has explained everything in detail that is the best thing that i liked about this post. I am looking forward to such great posts.
    office.com/setup | norton.com/setup | mcafee.com/activate

    ReplyDelete
  4. This content is very good, very interesting. Thank you for this great story.

    คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete
  5. Excellent information you have shared, thanks for taking the time to share with us such a great article. I really appreciate your work.
    Office.com/Setup

    ReplyDelete
  6. This is really informative post. Thanks for sharing.
    Office.com/Setup

    ReplyDelete

  7. Microsoft Office Setup is the package of Microsoft limitation programming which

    joins a blend of employments, affiliations, and host like Excel, PowerPoint,

    PowerPoint, Word, OneNote, Distributer and Access. Near to the working structures,

    these employments are Microsoft's key things that are everything seen as used

    programming on Earth. Microsoft Office Setup packages all the absolute best

    programming which Microsoft proceeds onward to the table.
    office.com/setup
    norton.com/setup

    ReplyDelete
  8. So informative,Thanks for sharing this Sobatpoker

    ReplyDelete
  9. If you purchase Office online, then you will get an Office setup product key that will be used during the installation process. How to Install MS Office Setup? After downloading, you have to install office.com/setup
    ..
    www.office.com/setup

    visit office.com/setup and get start with office.

    ReplyDelete
  10. Watch your favorite live sports, news, entertainment, and more. Plus, get unlimited access to the entire Hulu streaming library
    To activate Hulu code go to url
    if you need help to activate Hulu

    Hulu provides the simplest way to stream entertainment to your TV. On your terms. With thousands of available channels. We provide information regarding Hulu Activation Code. Go to Hulu activation
    , and enter the Activation Code

    Hulu activation

    hulu.com/activate

    ReplyDelete
  11. premium-malwarebytes.com is good for Windows PC/Laptop, MAC, Android devices.
    malwarebytes premium crushes the latest scams. It is also protects your cybersecurity. for the installation of the product Go to url : Premium-malwarebytes.com
    install malwarebytes with key code
    Install malwarebytes premium with key
    Install malwarebytes already purchased
    Install malwarebytes to second computer
    Install malwarebytes software

    ReplyDelete

  12. Online Website With reting the highest victory and giving many alternatives so that no one feels difficult to access into the website. And it has been guaranteed with the most wins.

    Link Alternatif | Bandar Terpercaya

    ReplyDelete