Tuesday, February 8, 2011

Scope's Segmented Memory Feature Makes Skipping Points a Good Thing

If you work with signals that have relatively long idle times between low-duty-cycle pulses or bursts of signal activity, then you'll love the segmented memory feature available in today's scopes. Segmented memory allows you to capture more selective signal details with less memory. With segmented memory, the scope’s acquisition memory is divided into multiple smaller memory segments. This enables your scope to capture a whole bunch of successive single-shot waveforms with a very fast re-arm time — without missing any important signal information.  In simpler terms it is a way for you to optimize your scope memory usage by only capturing the signal segments you are interested in. The second advantage segmented memory provides is a user interface that allows you to easily view the signal segments to check overall signal quality or to quickly find that needle in a hay stack bug that you know is out there. After a segmented memory acquisition is performed, you can easily view all captured waveforms overlaid in an infinite-persistence display and quickly scroll through each individual waveform segment. Common applications for this type of oscilloscope acquisition include high-energy physics measurements, laser pulse measurements, radar burst measurements, and packetized serial bus measurements. Below is an example of using segmented memory in a high-energy physics application.


High-energy physics and laser pulse applications 
Segmented memory acquisition in an oscilloscope is commonly used for capturing electrical pulses generated by high-energy physics (HEP) experiments, such as capturing and analyzing laser pulses. With segmented memory acquisition, the scope is able to capture every consecutive laser pulse, even if the pulses are widely separated. the figure below shows the capture of 300 successive laser pulses with a pulse separation time of approximately 12 µs and an approximate pulse width of 3.3 ns. All 300 captured pulses are displayed in the infinite-persistence gray color, while the current selected segment is shown in the channel’s assigned color (yellow for channel 1).

Note that the 300th captured pulse occurred exactly 3.62352380 ms after the first captured pulse, as indicated by the segment time-tag shown in the lower left-hand region of the scope’s display. With the scope sampling at 4 GSa/s, capturing this amount of time would require more than 14 Megapoints of conventional acquisition memory. If these laser pulses were separated by 12 ms, the amount of conventional acquisition memory to capture nearly 4 seconds of continuous acquisition time would be more than 14 Gigapoints. Unfortunately, there are no oscilloscopes on the market today that have this much acquisition memory. But since segmented memory only captures a small and selective segment of time around each pulse while shutting down the scope’s digitizers during signal idle time, scopes can easily capture this much information using just 8 Megapoints of memory

Agilent’s InfiniiVision Series oscilloscopes are the only scopes in the industry that not only provide segmented memory acquisitions simultaneously on all analog channels (up to four analog channels) and logic channels (up to 16 digital channels) of acquisition, but they also are the only scopes that provide hardware based serial decoding on packetized serial data for each captured waveform segment. The InfiniiVision Series includes the scope I have on my bench, the MSO7054A (although now they are on the B model so looks like I need to upgrade).

Click here for more on Agilent's segmented memory feature

Click here for more info on the scope I have on my bench (the B model though)

13 comments:

  1. Very nice article. I recommand it to my friends,I,ll be back here again and again visit here
    ALOKA UST-5286

    ReplyDelete
  2. Very nice article. I recommand it to my friends,I,ll be back here again and again visit here
    ALOKA UST-5286

    ReplyDelete
  3. Great info! I recently came across your blog and have been reading along. I thought I would leave my first comment. I don’t know what to say except that I have PSE-Platform question answer

    ReplyDelete
  4. This is very interesting, You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Regards - www.office.com/setup
    www.office.com/setup

    ReplyDelete

  5. شركة تنظيف مكيفات ببريدة
    شركة تنظيف مكيفات بعنيزة
    شركة تنظيف مكيفات بالبكيرية
    بالاستعانة شركة تنظيف مكيفات بالقصيم
    شركة تنظيف مكيفات ببريدة
    شركة تنظيف مكيفات بعنيزةاصبحت البلاد معرضة لموجات ارتفاع فى درجات الحرارة بشكل شبه مستمر ويعتبر هذا خطر جدا على الانسان وخصوصا كبار السن والاطفال واصحاب الامراض القلبية وامراض المتعلقة بالتنفس ولهذا ينصحهم الاطباء باستخدام المكيف اذا كان مسموح لهم ماديا امتلاكه وءلك لان التكيف هو منقذ لحياتهم حيث قامت دراسات باحصاء عدد حالات الشفاء للمسنين فى البلاد الذين يستخدمون فيها المكيف اكبر من حالات الشفاء فى البلاد التى لا يستخدمون فيها المكيف وكما ينصح الكثير من اطباء الاطفال بضرورة وضع الاطفال الذبن لديهم صعوبات فى تنظيم حرارة اجسامهم فى مكان به مكيف ويعتبر وضع المكيفات فى بيئة العمل تعمل على زيادة الانتاج لديك والمكيف ليس فقط يقوم بتعديل درجة الحرارة عن طريق رفعها او خفضها ولكن يقوم بتنقية الهواء بتقليل الميكروبات والفطريات به مما يجعل مستخدمين المكيف من مصابون بامراض الحساسية نسبة تعرضهم لمشاكل وخطر قليلة
    ماهي فكرة عمل المكيفات
    شركة تنظيف مكيفات بالبكيريةفكرة عمل المكيف هى نفس فكرة عمل ثلاجة وهو الاعتماد على غاز الفريون الذي يعتبر الوسيط لنقل حرارة من الغرفه الى الوسط الخارجي . بسبب اهمية المكيفات الكبيرة وذلك الاحتباس الحرارى الذى جعل فصل الصيف حار جدا ولا تستطيع المراوح تلطيف الجو ونظرا لاهميته يجب المحافظة عليه وتنظيفه بشكل دورى ويوجد العديد من الشركات التى تقوم بتقديم خدمة تنظيف المكيفات بطريقة صحيحة وتعتبر شركة تنظيف مكيفات بالقصيم
    من افضل الشركات التى تقوم بتقديم بتنظيف المكيفات بجودة عالية

    ReplyDelete
  6. I recommend that you need to visit this blog article for some additional info on how to write good essay. Make sure to do it sooner or later

    ReplyDelete
  7. They are good to entertain you when you are looking for the real time entertainment drama wiki

    ReplyDelete
  8. شركة بخ حشرات بالرياض أن تواجد الحشرات في المنزل من الأمور التي تتسبب في ذعر شديد للمواطنين كما تعد من الأشياء التي تتسبب في ضرر كبير من الناحية الصحة

    المصدر: شركة بخ حشرات بالرياض

    شركة تنظيف صالونات بالرياض الصالون جزء لا يتجزأ من أي منزل أو شقة فهو يتواجد بشكل رئيسي لاستقبال الأهل والأصحاب وندفع جميعنا مبالغ مالية كثيرة لشراء صالون

    المصدر: شركة تنظيف صالونات بالرياض

    شركة تنظيف مستشفيات بالرياض اذا كنت تمتلك مستشفى فهذا يعني أنك يجب ان تعطي أهمية كبيرة لعملية تنظيف كل ركن داخل المستشفى لأن المستشفى تكون مكان ملئ بالأمراض
    المصدر: شركة تنظيف مستشفيات بالرياض

    ReplyDelete
  9. Thank you for making me realize this. It's great.
    เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete
  10. This article is great. I like it very much. Thank you.
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete