Tuesday, January 11, 2011

A Low Cost Way to Capture Agile PRFs and PWs in Radar Test

In military radar applications the pulse repetition frequency (PRF) and sometimes pulse width (PW) parameters of a radar's pulsed RF/microwave signal may vary during operation. There is typically two reasons why PRF and PW may be varied:

  1. PRF and PW are tied to a measured target's range and resolution as well as the max range of the radar. A sophisticated radar system that can change modes from searching to tracking or from one search range to another must change its PRF and PW to match the radar's current mode. This is often referred to as mode changes.
  2. Military radars often employ PRF and PW that are constantly changing to help prevent an enemy from "spooking" the radar (creating a false target). These radar's employ complex highly secret algorithms for constantly varying the PRF and PW. This is often referred to as an agile pulse.
In this post I wanted to cover cover a fairly low cost solution for continuously capturing these parameters for verifying an agile PRF/PW algorithm, analyzing pulse noise from one mode to the next, or verifying tolerances from one pulse signal change to another. The solution is made up of a simple RF power detector and one or two gap-free sampling universal counters like the 53230A. The power detector is used to strip off the RF carrier and just output the pulse signal. The gap-free sampling counter or counters are then used to make the needed continuous timing measurements on the pulse signal. Why gap-free sampling counter?
  1. Counters provide high accuracy and high resolution timing measurements.
  2. Gap-free means no pulses will be skipped so you can get a complete and continuous picture of a group of pulses.
  3. Since counters are just making timing measurements with the edge event of a signal, you can capture a large amount of continuous pulse data with less memory and simpler post processing compared to an instrument that is digitizing the entire pulse signal. For instance the 53230A can store up to 1 million readings. There is not many scopes out there that can store 1 million digitized pulses in memory.
  4. Finally counters are low cost compared to RF / high speed digitizing instruments
As I mentioned above you may want to use one or two counters. You only need one if you are just interested in capturing one of the pulse parameters at once. The one counter based solution can be seen below.
The counter in the above figure is set for timestamped measurements which returns the time from positive signal edge to positive signal edge or negative signal edge to negative signal edge. Using the counter for timestamped measurements in this application returns the pulse repetition interval (PRF) from pulse to pulse. The PRF can them be obtained by inverting each reading. Below is an example measurement of an agile PRF signal using the setup above.
The below setup uses two counters to capture both PRF and PW simultaneously. One counter is used in timestamp mode for capturing the PRI and the other is making PW measurements. 
In the above setup, after the pulse parameter measurements are made on the desired set of pulses some simple software can be used to post process and combine the timing measurement data to give you a PRF, PRI, PW, and the duty cycle of each pulse in the set. 
Depending on the gap-free sampling counter you use, it may not measure the first couple of leading pulses from the set. This is because the counter may need to set the right input conditioning and edge leveling before the timing measurements can start. Also if you are using two different measurement modes in the counter, such as timestamps and PW, each mode may skip a different amount of leading pulses which you will need to know when using two counters in parallel to properly align your measurement. Finally, you want to be sure you use a high quality RF power detector for this type of test. Using a low quality detector can lead to carrier noise on the output pulse signal, which can really lower your measurement accuracy. 



20 comments:

  1. شركة نقل اثاث بالرياض افضل شركة نقل اثاث بالرياض
    شركة عزل خزانات بالرياض شركة عزل خزانات بالرياض
    شركة رش مبيدات بالدمام شركة رش مبيدات بالدمام
    شركة تنظيف بالرياض شركة تنظيف بالرياض في تويتر
    شركة تنظيف بالدمام شركة تنظيف منازل بالدمام

    شركة مكافحة حشرات بالمدينة المنورة شركة مكافحة حشرات بالمدينة المنورة
    شركة رش مبيدات بالرياض شركة رش مبيدات بالرياض
    شركة تنظيف خزانات بالمدينة المنورة شركة تنظيف خزانات بالمدينة المنورة
    شركة تنظيف خزانات بمكة شركة تنظيف خزانات بمكة

    ReplyDelete
  2. افضل شركة جلي بلاط بالرياض افضل شركة جلي بلاط بالرياض
    شركة رش مبيدات بالرياض شركة رش مبيدات بالرياض
    شركة شفط بيارات بالرياض شركة شفط بيارات بالرياض
    شركة شراء الاثاث مستعمل بالرياض شركة شراء اثاث مستعمل بالرياض
    شركة تنظيف خزانات بمكة شركة تنظيف خزانات بمكة
    شركة نقل عفش بالخرج شركة نقل عفش بالخرج
    شركة مكافحة حشرات بجدة شركة رش مبيدات بجدة
    شركة تنظيف منازل بالرياض شركة تنظيف منازل بالرياض

    شركة تنظيف منازل شرق الرياض شركة تنظيف منازل شرق الرياض

    ReplyDelete
  3. This is very interesting, You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Regards - www.office.com/setup
    www.office.com/setup

    ReplyDelete
  4. يتوافر لدي شركة دراسة لتقديم خدمات البحث العلمي الكثير من الخدمات البحثية التي تقضي تماما علي جميع العوائق والمشكلات التي يتعرض اليها الباحثين
    http://drasah.com/

    ReplyDelete
  5. يتوافر لدي شبكة المعلومات العربية الكثير من التقنيات الخدمية المتميزة التي يحتاج اليها الباحثين منها الترجمة البحثية التي يحتاج اليها الكثير من الباحثين حتي يتمكنوا من استكمال العديد من المهام في مشوارهم العلمي
    http://www.maktabtk.com/

    ReplyDelete
  6. You need to also examine this blog article for some info on how to write math assignments. Make sure to write it as soon as possible because it will be worth it

    ReplyDelete
  7. يسعي الكثير من الباحثين الي الحصول علي العديد من الانواع المختلفة للخدمات منها خدمة توفير دراسات اجنبية مترجمة في العديد من التخصصات العلمية فيتوافر ذلك لدي موقع مكتبتك لتقديم العديد من الانواع المختلفة للخدمات البحثية

    ReplyDelete
  8. I am searching for many days like this type of blog, today will got it this, am really satisfied with your blog, it’s really helped me a lot, thank you so much for share this wonderful blog, thanks to read my I hope I see your blog soon keep working, if any one searching best website designing company in Delhi please click my website and visit this we are able for you any time and we are made best website for you in cheap rate if are really grow your business so come with me on my website.
    Best Website Designing Company in delhi

    ReplyDelete
  9. Am visit of many blog but not get valuable information, but after seen your blog provide it me a lot of valuable and useful information I really like to thank you so much for share this information with us, if are inserted in grow up your life style and also grow up your looking so please come on my website am put it on many information so and visit again time thank you so much for read my comment I hope your also like my comment and you also go on my web page.
    Lifestyle Magazine

    ReplyDelete
  10. شركة جلي بلاط شمال الرياض تعد مهمة جلي البلاط أحد المهام الشاقة التي تقوم بها ربة المنزل خاصةً في حال تواجده في المطبخ أو غرفة

    المصدر: شركة جلي بلاط شمال الرياض

    تقدم شركة مكافحة النمل الاسود بالرياض خدماتها المتميزة في مجال مكافحة الحشرات عموماً والنمل الأسود على وجه الخصوص، فقد عرف النمل الأسود بعدة أسماء

    المصدر: شركة مكافحة النمل الاسود بالرياض

    شركة طارد الحمام بالرياض حماية المظهر الخارجي للمباني وواجهاتها من التشوهات التي تصيبها جراء الأوساخ التي تخلفها فضلات الحمام من أكثر الأمور المجهدة

    المصدر: شركة طارد الحمام بالرياض

    افضل شركة تنظيف محلات بالرياض تعد اليوم المولات والمحلات من أكثر الأماكن التي تستقبل الكثير من العملاء الوافدين إليها بهدف شراء الأطعمة والمشروبات

    المصدر: شركة تنظيف محلات بالرياض

    شركة تنظيف وجلي بلاط بالرياض أعمال التنظيف للأرضيات لا اختلاف عليها أياً كان نوعها نظراً لما تتعرض له من أوساخ وأتربة التي يتناقلها الهواء أو المحملة

    المصدر: شركة تنظيف وجلي بلاط بالرياض

    شركة مكافحة حمام بالرياض من أصعب العوائق التي قد تواجهها هي ما لا تستطيع التحكم بحدوثها بل تجدها تحدث بشكل مفاجئ لتضطر فيما بعد إلى مواجهة العوائق

    المصدر: شركة مكافحة حمام بالرياض

    ReplyDelete
  11. Excellent Post as always and you have a great post and i like it thank you for sharing

    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete

  12. This is really an amazing blog. Your blog is really good and your article has always good thank you for information.

    เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete