Friday, December 3, 2010

Creating a Differential Signal with a Function / Arbitrary Waveform Generator

Single-ended signals are referenced to a common level, such as ground, that they can share with other signals, so a single-ended signal requires only a single path or wire. Differential signals are made up of a pair of paths that are both dedicated to a single signal at any given time. One path is used at a higher potential than the other. Differential signals do add complexity, since they require two wires instead of just one, but they provide a number of performance advantages over single-ended signals.
Differential signal advantages include better signal-to-noise ratio, fewer timing errors, and less crosstalk. These advantages make differential signals common in applications such as ADC inputs, instrumentation amplifiers, measurement sensors (like accelerometers), and communication signals. When engineers design and test devices that use differential signals, simulating the differential signals for testing can be challenging. These challenges are caused by the fact that most function/arbitrary waveform generators (FAWGs) have single-ended outputs; instruments that can generate differential signals tend to be fairly costly. In this post I will explain two ways to create a low cost differential signal: using a FAWG with some custom hardware and using a 2-channel FAWG
One way to use custom hardware at the output of a single-ended source to create a differential signal is to use a differential amplifier circuit design as shown it the figure.

The resistors in the differential circuit were chosen to achieve a gain value of 1. I set the DC offset to 0 V. When building the circuit, be careful to keep signal paths and wiring as short as possible to keep parasitic reactive affects low for better signal integrity.
FAWG’s with two single-ended channels (isolated from ground) can have their channels combined into a single differential signal channel. To do this, you need to tie together the two "low" or "common" connections of each channel. The "high" of one channel must be used as the high signal path of the differential channel and the "high" of the other channel must be used as the inverse return wire or low signal path, as shown in the figure.

In addition to the two channels, it is also a lot easier to do this on a two-channel FAWG that has channel tracking capability, like Agilent’s 33522A two-channel function/arb waveform generator. This feature gives you the ability to create an inverted mirror image of the output signal from channel one onto channel two, which is exactly what is needed to create a differential signal. Also, this capability means you only have to set up the arb or built-in waveform on one channel and the inverted version of the waveform automatically tracks to the other channel. Without this feature you would have to setup an arb or built-in waveform on both channels and try to output them in sync using triggering.
As an example I measured and captured three signals with a differential input high-resolution digitizer. The example signal we used was a squarewave at 500 KHz. The figure below shows a digitizer screen shot of the signals. The three signals:
  1. Signal in yellow is a differential signal from the output of the differential amplifier connected to the single-ended FAWG
  2. Signal in green is the differential signal output created by the two channels from the 33522A
  3. Signal in purple is the output of the single-ended FAWG before the differential amplifier input


As you can see from the figure there is quite a bit of ringing on the differential signal created with the custom hardware. When I built my diff amp circuit I was careful to keep wiring as short as possible and I provided a large ground plane. Now with further time and engineer effort I could probably further improve the signal integrity of the circuit. But the point of this example is to show you can save test time and achieve better signal quality by using a 2-chan FAWG with tracking to create a differential signal. Also the cost of a 2-chan FAWG is still typically much cheaper than a differential output waveform generator.



28 comments:

  1. شركة رش مبيدات شركة رش مبيدات
    مكافحة الحشرات مكافحة الحشرات
    شركة عزل اسطح بالرياض شركة عزل اسطح بالرياض
    شركة رش مبيدات
    شركة تسليك مجارى بالرياض شركة تسليك مجارى بالرياض
    افضل شركة تنظيف خزانات بالرياض افضل شركة تنظيف خزانات بالرياض

    شركة مكافحة النمل الابيض بالرياض شركة مكافحة النمل الابيض بالرياض
    شركة تخزين اثاث بالرياض شركة تخزين اثاث بالرياض
    شركة تنظيف فلل بالرياض شركة تنظيف فلل بالرياض
    شركة شراء اثاث مستعمل بالرياض شركة شراء اثاث مستعمل بالرياض
    شركة جلي البلاط بالرياض شركة جلي البلاط بالرياض
    شركة تنظيف شقق بالرياض شركة تنظيف شقق بالرياض
    شركة نقل عفش بالرياض شركة نقل عفش بالرياض
    شركة نقل عفش بالرياض شركة نقل عفش بالرياض
    شركة تنظيف موكيت بالرياض شركة تنظيف موكيت بالرياض
    افضل شركة تنظيف مجالس بالرياض افضل شركة تنظيف مجالس بالرياض
    شركة تنظيف مسابح بالرياض شركة تنظيف مسابح بالرياض
    شركة تنظيف منازل بالرياض شركة تنظيف منازل بالرياض
    شركة تنظيف واجهات حجر بالرياض شركة تنظيف فلل بالرياض
    شركة تنظيف قصور بالرياض شركة تنظيف قصور بالرياض
    شركة مكافحة الصراصير بالرياض شركة مكافحة حشرات بالرياض
    شركة رش مبيدات بالرياض شركة رش مبيدات بالرياض
    شركة مكافحة حشرات بالرياض شركة مكافحة حشرات بالرياض

    ReplyDelete
  2. This is very interesting, You’re a very skilled blogger. I have joined your feed and look forward to seeking more of your fantastic post. Also, I have shared your web site in my social networks!
    Regards - www.office.com/setup
    www.office.com/setup

    ReplyDelete
  3. I’m no longer certain where you are getting your information, however great topic.
    I must spend a while studying more or figuring out
    more. Thank you for magnificent info I was searching for this info for my mission.

    www.office.com/setup

    ReplyDelete
  4. Hello everybody, here every person is sharing these kinds of knowledge, therefore it’s good to read this blog, and I used to go to see this webpage daily.
    www.office.com/setup

    ReplyDelete
  5. This comment has been removed by the author.

    ReplyDelete
  6. Cellular phone towers are not always capable to transmit strong signals for cell phones to catch. Frequently , when a phone is located far from the nearest tower system, the signal becomes poor. It's in such instances that a cellphone sign booster becomes very useful. Let's learn something about mobile phone signal booster gadgets. signalbooster.com

    ReplyDelete
  7. www.office.com/setup

    Office Setup, To get started with your Microsoft Office Installation you must need valid product key code & visit Officecom/Setup and we can also help you with your entire process to setup office product online.

    www.office.com/setup

    ReplyDelete
  8. Norton Antivirus for windows can operate with the maximum device of 5 at once. The user can simply create an online account and can add devices to which the user want to add the protection.

    norton.com/setup

    ReplyDelete
  9. McAfee have the complete set of features which can protect your digital online and offline life of the computing devices, and it not only help you to protect it but also it can maintain the stability of your computer, increase the speed with inbuilt PC Optimisation tool.

    mcafee.com/activate

    ReplyDelete
  10. As an example I measured and captured three signals with a differential input high-resolution digitizer. The example signal we used was a squarewave at 500 KHz. The figure below shows a digitizer screen shot of the signals. The three signals:

    1 Signal in yellow is a differential signal from the output of the differential amplifier connected to the single-ended FAWG
    2 Signal in green is the differential signal output created by the two channels from the FAWG
    3 Signal in purple is the output of the single-ended FAWG before the differential amplifier input BK Experience

    ReplyDelete
  11. Microsoft Office is an office suite of applications, which can be downloaded from servers, and services developed by Microsoft.

    www.office.com/setup

    ReplyDelete
  12. Officesetup-install is an independent technical support provider with on-site and On Demand Technical or Information Services for Office related products.

    office.com/setup

    ReplyDelete
  13. A step by step guide to set up Office for installation and activation issues.

    http://www.install-office-setup-com.com

    ReplyDelete
  14. office.com/setup

    office.com/setup

    Start-Office has a best selection of stylish and beautiful furniture and office decors online.

    office.com/setup

    ReplyDelete
  15. I am thankful for the article post.Really great article, looking forward to read more.

    www.office.com/setup

    ReplyDelete
  16. I am thankful for the article post.Really great article, looking forward to read more.

    www.office.com/setup

    ReplyDelete
  17. شركة مكافحة حشرات غرب الرياض اذا كنت تعاني من تواجد حشرات في منزلك او مصنعك أو حديقتك وقمت باستخدام العديد من الطرق للتخلص منها ولكن دون جدوى فالحشرات تعود

    المصدر: شركة مكافحة حشرات غرب الرياض

    شركة مكافحة حشرات شمال الرياض عميلنا الكريم لا قلق ولا خوف من الحشرات بعد اليوم مهما كانت تلك الحشرات وأنواعها المختلفة التي تعكر صفو حياتك وتجعلك لا تستمتع

    المصدر: شركة مكافحة حشرات شمال الرياض

    ارخص شركة مكافحة حشرات بالرياض ان مكافحة الحشرات بالطرق التقليدية أصبحت اليوم لا تجدي نفعًا لذلك يجب الاستعانة بشرة ذو خبرة وكفاءة عالية من أجل التخلص

    المصدر: ارخص شركة مكافحة حشرات بالرياض

    ReplyDelete

  18. Brother Printer Support is active helpline which exclusively support their customers with printer problems. If you face any problem with your printer like cable problem, black print, cartage issue and others then contact at toll free number of Brother Support and get instant help.

    ReplyDelete

  19. Geek Squad Online Support provides online support for your damaged devices. The team of online support is experienced in dealing with tech issues online. In case you're facing issue with your device contact Geek Squad Online Support

    ReplyDelete

  20. Geek Squad Support team is a group of technical experts who deal with damaged devices. They are expert in dealing all sort of issues with your damaged devices and gadgets. Connect with our expert team to get assistance at Geek Squad Support helpline.

    ReplyDelete
  21. Norton is a general respected stamp offering the best of antivirus relationship around the globe. Compelling its structures and sorts, it gives particular changes which meet the certain need of the customers. With Norton Antivirus, you can discharge up as it works an as a shield to your PC. Your PC is completely guaranteed and guaranteed by the world's driving security provider. norton setuphttp://nortoncomnortoncom.com/

    ReplyDelete
  22. Thank you so much for sharing these amazing tips. I must say you are an incredible writer, I love the way that you describe the things. Please keep sharing.

    For more information visit on office.com/setup | office.com/setup | Norton.com/setup | office.com/setup

    ReplyDelete
  23. After purchasing office.com/setupneed to visit office activate online to install and we provide technical services help in office setup on your Computer. http://officecom-officecom.com

    ReplyDelete
  24. Protect your Pc/laptop and other devices with best norton.com/setup Antivirus. Get security against spyware, malware and viruses. http://nrotonsetup.com

    ReplyDelete