Thursday, October 7, 2010

Low-Cost Photovoltaic I-V Curve Measurement System

I have noticed that my posts on photovoltaic test are getting lots of hits so here is another one. Here I am going to present a $3k photovoltaic I-V curve measurement system. The measurement system can be seen in the figure below (click on it to enlarge it).

Here is how it works:

  •  The op amp, FET, and Rsense act like a poor mans programmable electronic load with the PV panel connected across it. The op amp will drive the FET (lower its resistance) until the voltage at the op amps negative input equals the voltage at its positive input. If we can control the voltage at the positive input then we can control the current flowing out of the PV panel into the FET and Rsense just like an eload in consant current mode
  • Setting and stepping the voltage at the positive input of the op amp is done by the 34972A DAQ switch unit. It provides a DAC output from 0 to 15 V. When the DAC is set to 0V the FET is in an open condition and the PV panel is at Voc.
  • Rsense is 100 mOhm precision shunt. If we set the 34972A's DAC output to .5 V the op amp will drive the FET until the voltage drop across Rsense is .5 V. Since Rsense is 100 mOhm we know that 5 A of current is flowing out of the PV panel through Rsense (Ohm's law: .5 V/.1 Ohm = 5 A).
  • The 34972A's built-in 61/2 digit DMM combined with plugin MUX switch cards allow us to measure voltage, current, temperature, and more on a large number of channels. In the figure we use one channel to measure the PV panel's voltage, another channel to measure the panel's current (voltage measurement across Rsense), and two other channels to measure temperature. 
  • Putting it all together the way we get the I-V curve is by stepping the DAC's voltage up from 0 V (panel at Voc) until we reach Isc. At each step we measure the panel's output voltage and current to get our I-V curve. 
  • The way we know we have reached Isc is when further voltage steps from the DAC do not result in the voltage across Rsense increasing. At this point the FET is essentially a short.
This photovoltaic I-V curve measurement system will not work well with low voltage low power PV cells since Rsense and the FET cannot actually become a true short. It is better suited for PV modules and panels. Although the hardware is low cost you do need to wrap some type of software around it to control the DAC and gather the measurements (unless you want to do it manually). The value of Rsense and its power handling capability should be chosen based on your PV device's power range and your measurement accuracy needs. Below is a list of parts I used and their approximate cost. This was just a brief overview of the solution if you need more info just comment or email me.

Part description
Model/part number
Approximate price
Product Web site
DAQ switch measure unit
34972A
$1,850
Agilent.com/find/34972A
20-channel MUX module
34901A
$500
Agilent.com/find/34972A
Multifunction module
34907A
$400
Agilent.com/find/34972A
10-V power supply
B10G50
2 x $120
Acopian.com
Operational amplifier
NE5534AN
$2
Newark.com
Power MOSFET
IRFP150N
$3
Newark.com
0.1-ohm shunt resistor
15FR100E
$1
Newark.com
PCB prototyping board
8015-1
$8
Newark.com
Total
$3,004
Click here for more information on the 34972A DAQ switch unit

24 comments:

  1. One safety concern that I forgot to mention is heat dissipation. The FET is going to have a lot of current running through it so you want to be sure to attach a heat sink to it. Depending on how much current your PV device is putting out you may also want to add some active cooling.

    ReplyDelete
  2. What would you recommend for testing low power PV cells of 1/2 Watt or less? Does it make a difference if the MOSFET is working in the linear region? Would amplifying Vsense with an opamp fix the low power problem?

    ReplyDelete
  3. This solution was intended more for high power test. It would be hard for me to make a recommendation on how to alter the setup without testing. You may want to look at Agilent B2900A family of SMUs (check out blog post on May 18th 2011). They are not too expensive and would offer an excellent solution for 1/2 watt cell testing. Email me if you have any further questions.

    ReplyDelete

  4. Nice post, I bookmark your blog because I found very good information on your blog, Thanks for sharing more information. Three Channel ECG Machine

    ReplyDelete
  5. It is really such a wonderful Idea of using used expensive but essential medical equipment!!!
    Three Channel ECG Machine

    ReplyDelete
  6. Your post will be rather good, and I’m sure some will find it interesting because it’s about a topic that’s as widely

    discussed as others. Some may even find it useful.Thanks so much for your post.

    ALOKA UST-

    5546

    ReplyDelete
  7. I'm impersesd by your writing. Are you a professional or just very knowledgeable.Thanku….ALOKA UST-5546

    ReplyDelete
  8. I think I am going to use a similar blog template to yours. I find it very attractive to the reader.
    ALOKA UST-9130

    ReplyDelete
  9. I am pretty much happy to run into your site on the web and from now on I promise to visit your site every day and enjoy reading it. Seems like a faith.

    ALOKA UST-9130

    ReplyDelete
  10. A wonderful article. In my life, I have never seen a man be so selfless in helping others around him to get along and get working.

    ALOKA UST-9130

    ReplyDelete
  11. Great article, It's one of the best content in your site. I really impressed the post. Good work keep it up. Thanks for sharing the wonderful post.ALOKA UST-9130

    ReplyDelete
  12. Thanks so much for this information. I have to let you know I concur on several of the points you make here and others may require some further review, but I can see your viewpoint. electrical parts

    ReplyDelete
  13. Need a good book critique example? See a great Book Critique example here, my friends!

    ReplyDelete
  14. Awesome article.It is so impressive blog. I really appreciate this post. Thanks for sharing this post with us. Keep posting.
    SSC CONSTABLE RECRUITMENT 2018

    ReplyDelete
  15. The last time you got a new cell phone or laptop, what did you do with the old one? best dashcam

    ReplyDelete
  16. The absolute most crucial statistical connection among voltage, current and immunity at power is traditionally clarified as"Ohm's Law". Ohm's law can be utilised to learn the proper resistor price within a circuit as soon as the voltage is understood and you'd really like to confine the existing to some certain price.Try this ohms law calculator app through which you can easily cames to know about the calculations of voltage,current and resistance.

    ReplyDelete
  17. The absolute most crucial statistical connection among voltage, current and immunity at power is traditionally clarified as"Ohm's Law". Ohm's law can be utilised to learn the proper resistor price within a circuit as soon as the voltage is understood and you'd really like to confine the existing to some certain price.

    ReplyDelete
  18. Nice...!
    This system is very amazing to know the Low-Cost Photo voltaic I-V Curve. Thanks for sharing this information. https://mobdro.ooo

    ReplyDelete
  19. المصدر: شركة تنظيف بيارات بالرياض

    افضل أما الخدمة التي سنتحدث عنها الآن هي من أهم الخدمات التي تتشرف شركة تنظيف قصور بالرياض بتقديمها لعملائها ,وهي تنظيف مجالس سواء في المنازل أو الشقق أو الفلل او القصزر

    لأننا جميعاً نعرف أهمية اجتماعات العائلة في هذه المجالس التي تميز نا عن غيرنا من البلاد والدول ,فلابد أن تكون هذه المنازل على قدر عالي من النظافة والجمال والذي لابد وأن يتناسب مع أهمية المدعوين لهذه المجالس ,حتى يستمتع عملائنا باجتماعاتهم العائلية في جو نظيف وهادئ ومريح يليق بهم… اقرأ المزيد

    المصدر: شركة تنظيف قصور بالرياض

    شركة تنظيف كنب بالرياض عند تجمع الأتربة على أقمشة الكنب أو اتساخها بالبقع التي يصعب إزالتها فإن ذلك يبعث على النفس نوعا من الانزعاج ,و عدم الراحة خاصة مع هبوب العواصف الرملية و تجمع الأتربة الأمر الذي يزيد المشكلة تفاقما ويزيد النتائج سوء .

    من أهم الخدمات التي تقدمها  هي تنظيف السجاد والذي هو من أهم القطع التي يحتوي عليها أي منزل ,وهي ما تقوم بإظهار جمال كل قطع الأثاث في المنزل.

    وفي حالة ما كان هذا السجاد مستخ أو به أي بقع أو شوائب سيفسد كافة المنظر حتى إذا كان المنزل بأكمله نظيف.

    فتقوم شركتنا بتنظيف السجاد باستخدام مجموعة من المساحيق والأدوات العالية الجودة للحفاظ على هذا السجاد من التلف وإعادته نظيفاً وجديداً مره أخرى

    تتخصص  في تنظيف الكنب مع جميع أنواع أقمشته تنظيفا تاما وأرجعاها جديدة كأول مرة قد اشتريته مع الحفاظ على كافة أنواع المنسوجات التي تتخلل الكنبة و ما تحتويه من ألوان و رسومات كل ذلك تقدمه الشركة وبأسعار في متناول يد العميل بإذن الله .

    يمكنك الاعتماد علينا في إتمام عملية التنظيف و على أعلى مستوى ان شاء الله لما تتمتع به الشركة من خبرة طويلة ورضاء لكل عملائها الكرام … اقرأ المزيد

    المصدر: شركة تنظيف كنب بالرياض جميع الاحياء

    ReplyDelete

  20. Amazing post i am pretty much pleased with your good post.You put really very helpful information

    คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete