Monday, September 20, 2010

Sequencing Multiple Power Supply Outputs

Today’s high performance power supplies continue to add more and more capabilities to make the test engineer’s job easier. The capability that I am going to talk about here is sequencing on or off multiple power outputs. This capability allows you to set the order and timing that each power supply output powers on or off. This is useful for designing and testing embedded system designs. Embedded systems can be made up of any combination of microcontrollers, FPGAs, ASICs and memory chips. These individual integrated circuits often have multiple power input requirements that must be properly sequenced on and off to prevent latch-up. Latch-up may cause a wasteful initial surge of current at turn on, or it may be severe enough to inflict permanent damage to the semiconductor device. Ultimately these devices will have a power distribution system with regulators that will ensure the proper sequencing and timing for each power supply turn on and turn off, but during initial design and testing the power distribution system is often not in place yet so test and measurement equipment is used in its place to simulate the proper turn on and off conditions of the design.
In the past power sequencing was typically done in one of two ways: using programmable power supplies with software or using supplies with custom switches. The first way uses programmable supplies and then in software the supplies are properly sequenced on or off. The drawback to this method was unless you were running a real time operating system (windows is not a real time operating system) there was no way to accurately guarantee the timing from one supply output to the next with better than 30 ms of precision. The other method required additional hardware in the form of switch cards and control circuits. A hardware timed control circuit would provide the precision timing that a computer operating system could not. The control circuit would then control the sequencing of the supply output on or off using switches. If you wanted to avoid switch bounce you had to use solid state or mercury switches versus traditional mechanical switches. The problem with this method is complexity it adds to the testing process.
With the capability built into the supply you avoid the complexity of dealing with multiple pieces of hardware and since the timing is done inside the hardware of the supply it is highly accurate. Agilent’s N6700B series of supplies and the N6705B DC Power Analyzer are examples of supplies with built-in power output on / off sequencing. Each one has up to four power supply outputs per mainframe that can be sequenced on or off. Sequencing from one mainframe to another is also possible for applications that require sequencing of more than four power supply outputs. The figure shows a picture of the N6705B DC Power Analyzer being used to test an embedded design that requires turn on power sequencing.


12 comments:

  1. Your website is really cool and this is a great inspiring article.
    hop over to this website

    ReplyDelete
  2. I'm starting to wonder if you've lost your way I've been right here waiting patiently, Your lane should be right here next to me I need you tonight, think of you all of the time. thank you
    super smash flash 2
    bloons tower defense 5

    ReplyDelete
  3. Following Harvard outline format rules to the papers that students write in schools guarantees that they give credit or acknowledgments to all authors. It helps you avoid plagiarism, which is all about academic cheating. Harvard law outlines indicate that you should put enough effort into your chosen topic to come up with a good sentence structure and order. Acknowledging every source that you use in your essay is important. Correct references help you conduct your successful research and demonstrate your integrity.

    ReplyDelete
  4. As I mentioned in a previous post, we have devoted a lot of time writing about protecting your device under test (DUT) from the two main DUT-destroying forces available from a power supply: excessive voltage and excessive current.Mobdro

    ReplyDelete
  5. شركة تنظيف حمامات سباحة بالرياض يرغب الكثير من الأشخاص ممن يمتلكوا بعض الفلل أو القصور ويتواجد بها حمام سباحة في تنظيف تلك الحمامات باستمرار سواء لتطهيرها أو إزالة بعص الرواسب المتواجدة بها، بل وبعض المنازل التي يستغل بها السطح بإنشاء حمام سباحة تحتاج دوماً إلى التعقيم والتطهير.

    المصدر: شركة تنظيف حمامات سباحة بالرياض

    أما عن الخدمات التي تقدمها شركة تنظيف واجهات كلادينج بالرياض فهي كثيرة ومتعددة حيث تمتلك عدد من الأوناش كبيرة الحجم والتي تعمل على الوصول لأعلى نقطة ممكنة في المبنى لكي يتم تغطية الواجهات بالكامل وتنظيفها على أكمل وجه، وبالطبع تمتلك فريق كبير مدرب ومؤهل ويمتلك خبرة واسعة يمكنه التسلق بدون خوف والقيام بتلك المهمة على أكمل وجه لكي يوفر العملاء افضل الخدمات.

    المصدر: شركة تنظيف واجهات كلادينج بالرياض

    شركة تنظيف للبيت بالرياض تبذل الكثير من جهدها لتحقيق النظافة المثالية التي ترغب كل ربة منزل في الحصول عليها؛ فمن الأحلام البعيدة المحافظة على

    المصدر: شركة تنظيف للبيت بالرياض

    شركة تنظيف ثريات بالرياض يعد تنظيف الثريات أو النجف أمر شاق للغاية على الكثير من ربات البيوت بل ويحتاج إلى طرق خاصة في التعامل معه وذلك بسبب تعرضه للكسر

    المصدر: شركة تنظيف ثريات بالرياض

    شركة خدمات نقل عفش بالرياض لكل الباحثين من السادة العملاء عن أيدي العون خلال فترات الانتقال إلى مكان جديد سواء كان الأمر بالنسبة لأثاث المنازل أو لأثاث

    المصدر: شركة خدمات نقل عفش بالرياض

    ReplyDelete
  6. Here is a good Weblog You might Come across Fascinating that we Encourage You
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete
  7. Enjoyed studying this, very good stuff, thanks.
    เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete