Saturday, September 25, 2010

Innovative Way to Interface a Measurement Instrument with a Computer

In this post I am taking a turn from the usual. Typically when I praise a new product it is an Agilent product. Here I am going to lay some praise on an innovative new NI product, USB-TC01 Thermocouple Measurement Device. The innovation in this device is not the measurement technology but the way it interfaces with a computer allowing you to easily retrieve data. Typically interfacing a measurement instrument with a computer and retrieving measurement data from it involves either installing software (that you may have to pay for) or installing drivers and creating your own software. The clever USB_TC01 requires no drivers and no software! The way it works is by connecting to your computer via USB. To Windows the TC01 appears as a mounted disk drive (so no driver). By navigating to the now mounted TC01 “drive” you can launch software that is stored on the TC01. The software allows you to display readings, log readings, and download readings. It also has extras that make it easy to interface with LabView. Pretty cool functionality for a mere $129 price tag.
The technology is similar to the LXI instrument connection standard (to learn more about LXI click here). An LXI compliant instrument acts like a web server so you can connect it to a computer via LAN. The difference between LXI and the TC01 is LXI does require software (web browser which everyone already has), you need to know the instrument’s IP address or host name, and the LXI standard only requires instrument manufacturers to put network setting control in the web interface and not instrument control. Although most LXI instrument manufacturers, like Agilent, allow you to control and retrieve data from the instrument via the web interface.

31 comments:

  1. This is neat! Turning an instrument into a commodity by associating it with a commoditized hard drive.

    ReplyDelete
  2. I know I like it! I am not a fan of installing drivers or software every time I use a different instrument.

    ReplyDelete
  3. The book title is "Hunted" and it's very short book having only one Chapter but i think it's enough to understand the actual facts behind the heartbreak. However, I need paper writing service reviews but yes i must read this book and other important books as well.

    ReplyDelete
  4. And at this portal you will definitely find much more information on this topic, guys.

    ReplyDelete
  5. Very informative! You can get an online degree in Information Technology from the best online colleges and follow your passion in IT.

    ReplyDelete
  6. Are you stuck in your assignment and need help with Assignment? Then do not worry out writing assignment service are here to help you. Myassignment help provides the best assignment help for all students in Australia. Our professional expert writers provide academic assistance services to all students. Students can get help from our online assignment writers 24*7. For more offers visit Myassignment Help now.

    ReplyDelete
  7. This type of planter is very popular with avid gardeners because they provide a healthy environment for an annual’s root system and discourage root rot. They are meant to be used with a liner of some type, grademiners typically a fibrous liner made of compressed fibers called coir. However a new alternative is available called Moisture Mat Liner, made by Braun Manufacturing, a leader in horticulture products. This liner is sold by the foot, in five-foot wide rolls.

    ReplyDelete
  8. The article is very informative. Technology has changed lives to a great extent. I was fascinated with technology since i was 5 years old. After completing high school, I joined Colorado Technical University for information technology program. I learned a lot, got a exposures unimaginable.

    ReplyDelete
  9. Get the global assignment help services by the expert writers at Students Assignment Help. Our experts have earned their degrees from the renowned universities of Singapore. They are fluent in writing assignments without missing the deadlines.

    ReplyDelete
  10. افضل شركة تنظيف موكيت بالرياض هل تغيرت ألوان الموكيت لديك ؟ هل تعانين من بقع في الموكيت أو السجاد ولا تجد الوقت الكافي لإزالتها, أو حالتك الصحية لا تسمح لك بذلك ؟؟ هل لديك بعض أنواع الموكيت أو السجاد باهظة الثمن كالسجاد الإيراني ,أو التركي ونحوه وتخشى إتلافها جراء عملية التنظيف أو بعض المساحيق الخاطئة ؟.
    قدم شركتنا عروض متميزة للغاية لتنظيف الموكيت وكذلك تنظيف شقق في جميع أنحاء مدينة الرياض ,من خلال مجموعة من العاملين الموثوق بهم تماماً وعلى أعلى درجة من الكفاءة والإتقان في عملهم ,حيث يقوم العاملين لدينا بتنظيف المنازل بالكامل سواء الغرف أو المجالس أو المطابخ وكذلك دورات المياه .
    والتي تتطلب قدر عالي من الإتقان لأنها من أهم الأجزاء في أي منزل التي تحتاج قدر عالي من النظافة فهي أساس نظافة المنزل بأكمله وهي من أكثر الأماكن التي تحتوي على ميكروبات وجراثيم قد تؤدي للعديد من الأمراض
    تقدم الشركة خدمات تنظيف وبأفضل مستوى للموكيت و السجاد و بأجود أنواع العمالة المدربة وبأسعار تناسب جميع العملاء.… اقرأ المزيد

    المصدر: شركة تنظيف موكيت بالرياض

    افضل شركة تنظيف مجالس بالرياض هل فقد مجلسك رونقه ؟؟ هل بهتت ألوان أقمشته هل تزعجك تلك البقع التي تعبني من إزالتها ؟
    تقدم الشركة خدمة تنظيف المجالس و بأسعار مميزة تميزنا عن باقي الشركات فتعتمد الشركة على التنظيف الجاف في إتمام عملية التنظيف و أيضا تتعمد إزالة كافة الروائح المتعلقة بها .
    لن تتعرف على مجلسك بعد عملية التنظيف
    وإذا كنت من أصحاب الفلل فتقدم شركتنا العديد من العروض تنظيف فلل على أعلى درجة من الكفاءة والأمانة من خلال مجموعة من العاملين المدربين على أعلى مستوى وباستخدام مجموعة من الخامات العالية المستوى والمنظفات ذات مستويات عالية من الجودة حتى لا تتسبب في أي أضرار صحية لعملائنا

    فيقوم العاملين بتنظيف كل مكان في الفلل سواء الغرف أو الطوابق العليا أو السفلى وكذلك المطابخ والحمامات ودورات المياه لضمان مستوى عالي من النظافة يليق بكافة عملائنا
    عمالة مدربة و على أعلى مستوى من الاحترافية يضمن لك الحصول على أفضل النتائج لإرضائك فرضاؤكم هو هدفنا… اقرأ المزيد

    المصدر: شركة تنظيف مجالس بالرياض

    شركة تنظيف شقق بالرياض التنظيف ليس أمر عابر أو أمر من أمور الرفاهية فهو من أساسيات الحياة وطالما حافظت علي منزلك نظيف خالي من الأتربة والرواسب ستحافظ علي حياتك خالية من كافة الأمراض المختلفة
    متلك اسطول عمالة ذوى خبرة كبيرة حيث يعمل معنا منذ فترة طويلة خبرتة الكبيرة التى اكتسبها والأمانة التى يتصف بها جعلتنا فى صدارة شركات التنظيف.يقوم فريق العمالة بتقسيم نفسة الى اكثر من فريق ليعلم كل واحد منهم مهمتة ويؤديها بإتقان يتحرى الدقة طوال مراحل العمل

    لوجود مشرف يتمم على عملية التنظيف. فريق يقوم بتنظيف غرف النوم وفريق اخر مهمتة تنظيف غرف المعيشة والاخر لتنظيف المطابخ والحمامات

    لن يخرج فريق العمل الا بعد ان يسلمك بيت نظيف خالى تماما من اى اتربة او غبار ومطبخ نظيف تماما خالى من الدهون والزيوت .
    كما ستبقى النظافة سلوك طبيعي دوري بالنسبة إليك ولذلك فشركة دريم هاوس تقدم كل خدماتها الخاصة بالنظافة وذلك حرصا منها علي نظافة وصحة العملاء كما توفر كل هذا من خلال طريقة مميزة ومحترفة جدا في التنظيف بشكل عام .… اقرأ المزيد
    المصدر: شركة تنظيف شقق بالرياض

    ReplyDelete
  11. It is really an innovative way. As a student from computer science this interests me. I'm so happy that I'm studying in one of the top universities across the globe where I got admission through GRE.

    ReplyDelete
  12. Our CPM homework helpers use accurate problem-solving strategies to come up with the right answers to each question in this course. Stuck with the questions in the course 1 of CPM? Get help with CPM homework from us now!

    ReplyDelete
  13. Students Assignment Help serves the best help with essay writing services for the students. We have the best assignment writer who delivers excellent quality assignment writing services to the students. Our professional writers are proficient in writing assignment and timely providing the assignments.

    ReplyDelete
  14. Here is a good Weblog You might Come across Fascinating that we Encourage You
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร Gclub กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> goldenslot
    สนใจร่วมลงทุนกับเรา สมัครเอเย่น Gclub คลิ๊กได้เลย

    ReplyDelete
  15. Enjoyed studying this, very good stuff, thanks.
    เว็บไซต์คาสิโนออนไลน์ที่ได้คุณภาพอับดับ 1 ของประเทศ
    เป็นเว็บไซต์การพนันออนไลน์ที่มีคนมา สมัคร Gclub Royal1688
    และยังมีหวยให้คุณได้เล่น สมัครหวยออนไลน์ ได้เลย
    สมัครสมาชิกที่นี่ >>> Gclub Royal1688
    ร่วมลงทุนสมัครเอเย่นคาสิโนกับทีมงานของเราได้เลย

    ReplyDelete
  16. Watch Hindi serials, Bollywood movies, hindidramas, latest political shows, and all indian tv channels through our indian tv box.

    ReplyDelete
  17. Bananas are also a favorite ingredient for green smoothie recipes. They provide the perfect creamy smoothie base and their flavor complements a variety of fruits such as strawberries, blueberries, pears, apples, pineapple – really any fruit!banana shake

    applications programme suggests that the finished page can demonstrate fully the means wherever it had been organized.Download free software

    ReplyDelete
  18. When you want the best place learning at an affordable price, we are the right choice for you. We charge the lowest reasonable fee for the students from the USA, Canada, UK, Australia, etc Online Quran Academy.

    ReplyDelete
  19. This is a nice and informative post thanks for the information!
    saludpulso.com

    ReplyDelete
  20. This blog is really very nice. Get Essay writing Help Sydney from StudentsAssignmentHelp.com.

    ReplyDelete
  21. The browser also features a built-in ad-blocker and is available for the Windows, MacOS and Linux operating systems blockchain.

    ReplyDelete
  22. We understand students do not have great skills in completing their university task well. That is why the professional writers at Irelandassignmenthelp.com present the best Dissertation writing services services for the scholars at all educational levels.

    ReplyDelete
  23. Check out our TOEFL Preparation blog. I am sure it will help.

    ReplyDelete
  24. banana shake.A banana is an edible fruit. Banana is loaded with fiber, both soluble and insoluble. On the other hand milkis also nutrient-rich. In fact, banana shake is also excellent for workout.

    ReplyDelete
  25. Whether you need screen-printed t-shirts, embroidered workwear, custom sportswear or branded promotional products, we always exceed expectations the north face.

    Schoolwear Centres specialises in supplying school uniforms, with embroidered Logos to schools across UK. Our year –round services saves you time, stress and money school uniform.

    ReplyDelete