Saturday, July 3, 2010

Repeatability Specification in RF / Microwave Switches


High quality RF/microwave switches often have a “repeatability” specification. Repeatability is typically given in dB and is often confused with the insertion loss specification (also given in dB). Insertion loss is a well known spec and can be defined as the loss of signal power due to the “insertion” of the switch into the signal path. Repeatability specification is a little trickier to understand, it can be defined as the variation in insertion loss from one switch closure to the next. You may wonder why does the loss through the switch change at all since it is just two high quality flat conductors making contact? Remember at RF/microwave frequencies we are dealing with wavelengths that about the size of the signal path or shorter. This means the impedance that the signal path presents to the signal is affected by small changes in the signal paths dimensions. When the switch is cycled it never closes exactly the same way it did on the previous closure which results in a slight variation in impedance. This variation in impedance from one closure to the next is represented by the repeatability spec. The repeatability spec is only a small fraction of the switches overall insertion loss, for instance Agilent RF/microwave switches have a repeatability spec of 0.03 dB.

So why do we care about the repeatability spec? The reason we care about the repeatability of a switch is because it is a random error not a systematic error (like insertion loss) and therefore cannot be calibrated out or compensated for in measurements. If you have an RF / microwave signal path that you characterize with a network analyzer and that same path has a switch in it once you cycle that switch the insertion loss or S-parameters you measured with the network analyzer has now changed. So switches add measurement uncertainty to your characterized or calibrated signal paths and that is why it is critical to keep the number of switches in a signal path as low as possible.

Let’s say we have an RF / microwave signal path that we have characterized with two switches in it and these switches have a repeatability spec of 0.03 dB. Does that mean we would spec the signal path with a 0.06 dB uncertainty? The answer is no and the reason is because our repeatability error is random so it takes on a Gaussian distribution like the one shown in the figure.

Since repeatability error takes on this type of distribution we can use the root sum or squares (RSS) method to calculate the measurement uncertainty of the signal path. RSS is calculated using the following formula: sqrt(x1^2+x2^2+....+xn^2). Using RSS means the measurement uncertainty of our signal path with two switches in it is 0.0424 dB instead of 0.06 dB. RSS works because the repeatability is typically calculated out from the Gaussian distribution by 3 sigmas or standard deviations (see figure) so the probability that both switches are at .03 dB deviation (both on the same side of the curve) from the calibrated value is very unlikely (about 1 in 274,000).

For more info on calculating measurement uncertainty check out the NIST page on it here

Now if you’re making high precision measurements in applications where phase accuracy is critical, such as radar test, you may be wondering where the phase repeatability spec is. Unfortunately phase repeatability is not spec’d by RF / microwave switch manufacturers (or at least I have not ever seen it spec’d). This leaves you with two choices if you need to establish phase repeatability for your switches: contact the manufacturer to see if they have data on phase repeatability or calculate it yourself using Gaussian distributions and the principals of probability.

56 comments:

  1. Great!!
    I really like your post!
    It really useful for my thesis writing.
    Thank you so much.
    Students may also searching for Karnataka SSLC PUC Results 2018.
    Can check their results here karresults.nic.in

    ReplyDelete
  2. I think you gonna love this site https://persuasivepapers.com/tips-for-preparing-high-school-persuasive-essay/. Try this once and you will be always return for more writing guides.

    ReplyDelete
  3. Very worthwhile piece of writing, thank you for your article.
    getapk market 1.6.7 download

    ReplyDelete
  4. Selection of multiple signal sources to one output
    • Selection of multiple input signals to one
    measurement instrument
    • Transfer switching to insert or remove a device
    in a signal path
    • Matrix switching of multiple inputs and outputs www.krogerfeedback.com

    ReplyDelete
  5. Such a nice content. today i learned something new from your blog. good job, keep sharing.

    Also checkout my blog discoverers day 2018 and is columbus day a postal holiday.

    ReplyDelete
  6. Report <a href="https://bestwritingservice.com/essay-assignment.html>essay assignment</a> are assigned by professors to see the student's level of preparation. In case if you need any help towards writing, write to https://bestwritingservice.com/

    ReplyDelete
  7. This comment has been removed by the author.

    ReplyDelete
  8. On the off chance that you have a genuine debrid account, CyberFlix APK will give considerably more connections in 720 and 1080p High Definition Cyberflix TV APK

    ReplyDelete
  9. Quite an informative blog. Want to tell something about most Offline games apk that is available online and easy to download and also there is a lot of other different things like apps and games you can download and play after without any internet need.

    ReplyDelete
  10. Hey Thanks for sharing this valuable information with us. I will come back to your site and keep sharing this information with us.krogerfeedback

    ReplyDelete
  11. Hey Your site is awesome and full of information. I have read you posts they are so informative. Keep Posting wonderful content. Visit talktowendys

    ReplyDelete
  12. Your content is indepth and a deep read. Thanks for posting and sharing. blazecc login

    ReplyDelete
  13. Hey Thanks for sharing this valuable information with us. I will come back to your site and keep sharing this information with us. Win Prizes by taking surveys

    ReplyDelete
  14. The students who avail professional writing help look for fast solutions. The fast assessment writing service introduced by Sample assignment by assignment experts. Simply send in the details of your assignment, and we’ll do the rest. Be it providing  a business management assignment help, management assignment help, business plan assessments, business strategy assignments, and more we have you covered.

    ReplyDelete
  15. If you are interested in movies app, then you download showbox apk free for android.

    ReplyDelete
  16. I am a antique ’Article’ collector and I sometimes read some new articles if I find them interesting blackmart. And I found this one pretty fascinating and it should go into my collection. Very good work! blackmart apk

    ReplyDelete
  17. معلومات تفصيليه عن الصراصير ؟

    افضل شركة مكافحة الصراصير بالرياض http://ow.ly/UaRO50owehg تعد الصراصير من الحشرات المنزليه المقززة التى يخشاها الكثير من الأفراد ؛ولها أشكال وأحجام مختلفه ؛فالصراصير لديها ألوان سوداء أو البنى القامت ولديها شعيرات فى الوجه ؛وتتمكن من الوصول الى الأطعمة الخاصه بها عبر مجموعه من قرون الاستشعار التى تساعدها على الاستدلال على أماكن الأطعمة ؛فقط نحن شركة مكافحة حشرات بالرياض .

    تعيش الصراصير فى الجحور أو المستعمرات والمسامات الواسعه التى تتواجد أسفل الحوائط وفى الركنيات ؛وتتمكن الصراصير من نشر الطفيليات والشوائب فى المكان نظرا لأنها تنتج روثا اسود اللون فى أماكن تواجدها ؛وتتغذى على كل ما يقابلها من بقايا أطعمة أو ورق وغيرها من الأمور الأخرى ؛وتخرج من تلك الجحور صيفا للبحث عن الأطعمة وتفضل التواجد فى الأماكن الرطبة التى تمتلأ بالمياه وحول الصنابير ؛ومن المعروف أن هناك أنواعا مختلف من الصراصير لا يمكن القضاء عليها بسهوله سواء الصراصير الألمانيه أو الاستراليه أو الأمريكية أيضا.… اقرأ المزيد

    المصدر: افضل شركة مكافحة الصراصير بالرياض

    افضل شركة رش مبيدات بالرياض http://ow.ly/loyO50owehW الشركة متخصصة في مكافحة الحشرات بطرق حديثة وجودة عالية بشكل لا يضر بأهل المنزل أو يضر الأطفال أو يؤثر عليهم
    الشركة لديها كافة الحلول للقضاء على الحشرات ورشها وإبادتها إبادة تامة ,
    تمتلك الشركة أيضا أفضل الكوادر البشرية الذين يوظفون جُلَ طاقتهم من أجل القضاء على الحشرات وذلك عن طريق الرش والأمصال التي تؤدي للقضاء عليها ,
    لدينا الخبرة لذلك وبأقل الأسعار وأعلى مستوى جودة و أمان بإذن الله تعالى
    اتصل بنا نصلك أينما كنت
    نحن الأفضل في هذا المجال,
    نحن جميعاً نعلم أن السر وراء إبادة الحشرات هي رش المبيدات لذا فكان أول اهتمامات الشركة أن تحرص على استخدام أفضل أنواع المبيدات الحشرية التي تجعلها من أفضل شركات رش مبيدات بالرياض، نظراً لما يملكه المبيد من فعالية قوية و إبادة فورية دون ان يلحق أي أضرار بصحة الموجودين في المنزل ولا يسبب لهم الإزعاج، و كما حرصت الشركة على أن توفر كل ذلك، وكان من ضمن اهتماماتهم أن تقدم خدماتها بأقل الأسعار لكي تناسب كافه فئات العملاء دون أن تسبب لهم أي ضغط مادي.
    الرش يكون بأنواع مجربة وغير ضارة وآمنة على كل من يستخدمها معنا أنتم بأمان وصحتكم بأمان و لا داعي للقلق أو التفكير طويلا فإننا لسنا الوحيدون ولكننا المميزون… اقرأ المزيد

    المصدر: شركة رش مبيدات بالرياض

    ReplyDelete
  18. win free jazz daily call packages now with the mobilepackages.pk and get your free packages now instantly.

    ReplyDelete
  19. Your article is so useful for us,thanks for sharing. Good stuff! Check out my article Taco John’s menu

    ReplyDelete
  20. I can only express a word of thanks. Because with the content on this blog I can add knowledge I, thank has been sharing this information. Do not forget to visit our website to share information hotele

    ReplyDelete
  21. Thanks for sharing this information with us and we will revisit your website also visit www.krogerexperience.com

    ReplyDelete
  22. This article will show you how to jailbreak Firestick. By doing this, you will have access to thousands of free movies, TV shows, sports, live tv.

    ReplyDelete
  23. Excellent article and I think the post that touchs readers's concerns always rock. Roast Borough Market Menu with price

    ReplyDelete
  24. Installing thevideo pair on your computer is a very simple task, just download it to your eztv and double-click on the file you have downloaded to start the installation. Then, all we have to do is follow the instructions that you are giving us to install 123movies correctly on our Windows 7/8/8.1/10 PC.

    covenant kodi is without a doubt one of the best applications that we can use in our daily life. Remind them that in 2015 it was one of the most widely used apps for Android in India. So, we know that if you are here it is because you know the advantages of this app and want to download sportsdevil addon for PC.

    Who doesn’t like sharing files from one device to another at an enormous speed? demonoid proxy was created to make it fast and easy to share any file between mobile devices or computers.

    ReplyDelete
  25. Really I enjoy your site with effective and useful information. It is included very nice post with a lot of our resources.thanks for share. i enjoy this post. Friendly’s Ice Cream Survey

    ReplyDelete
  26. food survey Customer Satisfaction Survey is way to tell your feedback and Participate in food survey on
    Mcdvoice Survey

    ReplyDelete
  27. This comment has been removed by the author.

    ReplyDelete


  28. Nice blog, the article you have shared is good.This article is very useful. My friend suggest me to use this blog.
    tractorshub

    ReplyDelete
  29. This blog very nice and informative. Thanks for sharing this blog.I am waiting for your next articles.Keep it up quickly ............... krogerfeedback fuel points 50 points

    ReplyDelete
  30. Excellent site. Plenty of helpful information here. I am sending it to some buddies ans additionally sharing in delicious.
    centralhours_uk

    ReplyDelete
  31. Customer Satisfaction Survey is way to tell your feedback and Participate in food survey on
    Mcdvoice Survey

    ReplyDelete


  32. Nice blog, the article you have shared is good.This article is very useful. My friend suggest me to use this blog.
    surveydetails

    ReplyDelete
  33. คาสิโนออนไลน์ที่น่าเชื่อถือและมีความเป็นมืออาชีพที่สุดในตอนนี้
    โปรโมชั่นGclub ของทางทีมงานตอนนี้แจกฟรีโบนัส 50%
    เพียงแค่คุณสมัคร สล็อตออนไลน์ กับทางทีมงานของเราเพียงเท่านั้น
    ร่วมมาเป็นส่วนหนึ่งกับเว็บไซต์คาสิโนออนไลน์ของเราได้เลยค่ะ
    สมัครสล็อตออนไลน์ >>> Goldenslot
    สนใจร่วมสนุกกับ คาสิโนออนไลน์ คลิ๊กได้เลย
    มีทั้งคาสิโนออนไลน์ หวยออนไลน์ ฟุตบอลออนไลน์ สล็อตออนไลน์ และอื่นๆอีกมากมาย

    ReplyDelete
  34. Hi your blog is very interesting, You don't need to download Netflix account we provide you free of cost app and watch all free movies and TV shows with this app
    Online Show Box

    ReplyDelete
  35. I have read your excellent post. This is a great job. I have enjoyed reading your post first time.

    surveyexpert

    ReplyDelete
  36. Thanks in favor of sharing such a nice thinking, article is pleasant, thats why i have read it entirely.
    asos complaints email phone number
    borough of poole complaints
    plymouth city council complaints

    ReplyDelete
  37. I have read your excellent post. This is a great job. I have enjoyed reading your post first time.

    pradhanmatri-yogna

    ReplyDelete
  38. Hey i really love the stuff you are sharing with us. Keep on sharing it and i'll keep in touch with your site.
    Sulliden Gold Corp Customer Service Phone Numbers

    ReplyDelete
  39. You highlight some insightful points-however I am concerned you could be skimming details.
    Vodafone Email
    ADT SECURITY PHONE NUMBER

    ReplyDelete
  40. Great Post !! I admire the valuable information you offer in your articles. I will bookmark your blog and refer to my friends.
    homegoodsfeedback
    lennyssurvey lennys subs survey

    ReplyDelete
  41. Awesome post….Thanks for sharing this awesome article
    thestorelocator

    ReplyDelete
  42. Excellent site. Plenty of helpful information here. I am sending it to some buddies ans additionally sharing in delicious.
    Unichem in Waiuku
    McDonald’s in Orewa

    ReplyDelete
  43. Excellent site. Plenty of helpful information here. I am sending it to some buddies ans additionally sharing in delicious.
    http://bit.ly/2HbGWuZ
    http://bit.ly/31G3s72

    ReplyDelete