Friday, July 9, 2010

Easy Instrument Connectivity with Matlab

Matlab is my favorite tool for creating complex arbitrary waveforms since it has a wealth of built-in mathematical capabilities and makes it easy to create and manipulate long floating point matrices. But often when I suggest matlab to colleagues as a tool for creating arbitrary waveforms for test instrumentation they either don't know matlab can connect to instruments or they think they have to sit down and learn how to use some complex driver. This could not be farther from the truth! Matlab makes it easy to connect to instrumentation by providing a graphical user interface instrument control toolbox. Here is a quick summary on how to access and use matlab's instrument control toolbox.
1. Go to matlab's 'Start' menu, select 'Toolboxes', select 'Instrument Control', and 'Test and Measurement Tool' as shown in the top figure.
2. Follow the instructions to establish a connection with the instrument as shown in the middle figure.
3. Go to the 'Session Log' tab and copy the needed connection code from the window and paste it in your script or function.
Now isn't that easy?
For any Matlab experts out there, when I try to build strings that are 1.2 MB long Matlab lab seems to lock up on me (I give it a while to run). Is there a special way to handle strings that long or is that out of matlab's capabilities (which I doubt)?






For more information on Matlab's instrument control toolbox click here

19 comments:

  1. Hey Neil, here's a link to an Agilent Forums post with an example program of how to create and download an arbitrary waveform in Matlab, to your Agilent function generator. The program shows you how to open a visa session and create a very basic pulse waveform. You can create much more complicated waveforms, but here's an example to help you get started.

    https://forums.tm.agilent.com/community/viewtopic.php?f=536&t=24802

    ReplyDelete
  2. Really impressive post. I read it whole and going to share it with my social circules. I enjoyed your article and planning to rewrite it on my own blog.
    pop over to this site

    ReplyDelete
  3. You have a real ability for writing unique content. I like how you think and the way you represent your views in this article. I agree with your way of thinking. Thank you for sharing.
    click to find out more

    ReplyDelete
  4. https://test-dpc.com/
    https://snaptube.vip/
    https://tubemate.vip/ Thanks for sharing.I found a lot of interesting information here. A really good post, very thankful and hopeful that you will write many more posts like this one.

    ReplyDelete
  5. Well Said, you have furnished the right information that will be useful to anyone at all time. Thanks for sharing your Ideas.

    Php course in chennai

    ReplyDelete
  6. I must say that I read this before writing my resume. And it helped me a lot with including relevant coursework on resume.

    ReplyDelete
  7. These are usually not as accurate since the charge may just arc through the upper or lower body and as a result may not give you a complete picture of your overall fat collagen supplements reviews

    ReplyDelete
  8. Regardless of the interface you use, there are common steps that comprise the basic workflow of instrument communication. In all cases, you must examine your hardware resources and create an interface object. Setting properties is optional. Reading and writing depends on the interface you are using. See the section of the documentation for the interface you are using.liteblue usps

    ReplyDelete
  9. it is quite hard to free your self from it. You cannot deny the fact that it has provided you pleasure during some periods of stress and anxiety v2 e cig review

    ReplyDelete
  10. Is it accurate to say that you need some additional cash? You've likely prepared a wellspring of trade out your home, and don't understand it.bobsweep pro

    ReplyDelete
  11. According to a 2007 IBM study, a business technology coach should be "...engaged as a strategic partner for process and culture change." bobsweep pethair

    ReplyDelete
  12. From cell phones to PCs, about every cutting edge contraption are worked by electronics. Ibobsweep pethair plus reviews

    ReplyDelete
  13. It is a University, where a research HOSPITALITY MUT unit is also present apart from being a teaching organization.

    ReplyDelete
  14. Thanks for the information, Get the best RPA Training in Chennai from Hope Tutors at Affordable fees.

    ReplyDelete